Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Pic Microcontrollers Forum can i control 4 dc motor with one pic16f877a
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 235 subscribers
  • Views 480 views
  • Users 0 members are here
Related

can i control 4 dc motor with one pic16f877a

aml
aml over 14 years ago

i want to control four wheel for my robot to control speed and direction

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    To control the dc motors the simplest option is to use a couple of so called H-bridges. These allow your microcontroller to control both the speed and the direction of dc motors.

    You can simply use pwm to control the speed, looking at the datasheet of the 16f877 it seems that it only has 2 hardware pwm outputs. This means that if you want to control each motor sepperatly you will have to implement 2 software pwm ports, besides using the 2 hardware pwm ports.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 14 years ago

    AML,

     

    You could try to use an external breakoutboad for driving several motors from a single port.

     

    What that really amounts to is using another microcontroller with more motor control ports, or several small motor controllers in a row. This new system would interpret the singal coming in from the PIC 16F877a and control the motors according to how you design the software. This would be a good option if the motors are high powered and needed a separate driver circuit anyway.

     

    For ease, I recommend getting a PIC with more control ports, if you want to bypass additional boards.

     

    Cabe