Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Pic Microcontrollers Forum PIC 16f887 UART to PC
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 236 subscribers
  • Views 691 views
  • Users 0 members are here
  • uart
  • rs232
  • serial
  • pic
Related

PIC 16f887 UART to PC

e14 Contributor
e14 Contributor over 11 years ago

Hello,

 

I am trying to send what I am calling a "device ID" to my PIC and have the PIC store it. The other half of this issue is that I am also writing a program in C that runs on on my PC that will accomplish this transaction. My expected results are I send an ID from the PC software and the PIC replies with the ID that it has received ("ID set to: 77). It does work perfectly the first time, however if I try to send a new ID, the PIC does not reply with ID only with "ID set to:". If I reset the PIC I can send in a new ID again, but only once.

 

Using the terminal application in Mikro C, I can send the ID, and resend the ID as much as I want without resetting the PIC.

 

My question for this discussion is should I be looking for problems in the code on the PC side or PIC side? Both are written in C, and my gut feeling is that its on the PC side since the terminal works, but why would resetting the PIC allow me to send a new ID Properly?

 

I can provide code if you like, but wont paste it now since this is more of a "where should I start" type of question.

 

I appreciate any thoughts and constructive advice.

 

Thanks,

George

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Problemchild +1
    I have tried using Putty, and It worked fine as well. Here is the PIC C Code: char myidd[10]; void newline(){ UART1_write(13); UART1_write(10); } void main() { UART1_init(9600); ANSEL = ANSELH = 0; TRISA…
  • Problemchild
    0 Problemchild over 11 years ago

    I think most folk would be as confused as you as the answer is yeah both...ish probably!

    Obviously that's not the answer you want image !

     

    Please can you post the code or at least the section in question so that those who have the skills to help can take a look and offer some advice.

     

    BTW have you tried any other terminal software ?

    Any pictures or diagrams would be good as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Problemchild

    I have tried using Putty, and It worked fine as well.

    Here is the PIC C Code:

     

    char myidd[10];

      

    void newline(){

      UART1_write(13);

      UART1_write(10);

    }

     

     

    void main() {

      UART1_init(9600);

      ANSEL = ANSELH = 0;

      TRISA = 255;

      TRISB = 255;

      TRISD = 0;

      PORTD = 0;

      for(;;){

      if (rb7_bit == 1){

          PORTD = 0b00000000;

        }

        if (rb0_bit == 1) {

          PORTD = 0b00000111;

          //delay_ms(3);

        

          if (UART1_data_ready){

            memset(myidd, 0, strlen(myidd));

            UART1_read_text(myidd, "id", 10);

            UART1_write_text("ID set to: ");

            UART1_write_text(myidd);

            newline();

          }

        }

      }

    }

     

     

    Here is the section of my program that should be relevant:

     

    void pgm_dev(){

        char com_port[7] = "COM";

      

        char dev_id[12];

        memset(dev_id, 0, sizeof(dev_id));

      

        char pic_input[256];

        memset(pic_input, 0, sizeof(pic_input));

      

        char dumberr[256];

        memset(dumberr, 0, sizeof(dumberr));

     

        system("cls");

        printf("Please enter the number of your Com Port: ");

        fgets (com_portpick, 4, stdin);

        strcat(com_port, com_portpick);

        str_length = strlen(com_port);

      

        if (com_port[str_length - 1] == '\n'){

            com_port[str_length - 1] = NULL;

        }

     

        DWORD  accessdirection =GENERIC_READ | GENERIC_WRITE;

        HANDLE hSerial = CreateFile(com_port, accessdirection, 0, 0, OPEN_EXISTING, 0, 0);

     

        if (hSerial == INVALID_HANDLE_VALUE) {

            FormatMessage(FORMAT_MESSAGE_FROM_SYSTEM, NULL, GetLastError(), MAKELANGID(LANG_NEUTRAL, SUBLANG_DEFAULT), dumberr, 256, NULL);

                printf("Could not open selected COM port! (%s)\n", com_port);

                strcpy(com_port, "COM");

                printf("Press Enter to continue");

                getch();

                pgm_dev();

        }

     

        DCB dcbSerialParams = {0};

        dcbSerialParams.DCBlength=sizeof(dcbSerialParams);

     

        if (!GetCommState(hSerial, &dcbSerialParams)) {

               FormatMessage(FORMAT_MESSAGE_FROM_SYSTEM, NULL, GetLastError(), MAKELANGID(LANG_NEUTRAL, SUBLANG_DEFAULT), dumberr, 256, NULL);

                printf("%s", dumberr);

        }

     

        dcbSerialParams.BaudRate=9600;

        dcbSerialParams.ByteSize=8;

        dcbSerialParams.StopBits=ONESTOPBIT;

        dcbSerialParams.Parity=NOPARITY;

     

        if(!SetCommState(hSerial, &dcbSerialParams)){

            FormatMessage(FORMAT_MESSAGE_FROM_SYSTEM, NULL, GetLastError(), MAKELANGID(LANG_NEUTRAL, SUBLANG_DEFAULT), dumberr, 256, NULL);

                printf("%s", dumberr);

        }

     

        COMMTIMEOUTS timeouts={0};

        timeouts.ReadIntervalTimeout=50;

        timeouts.ReadTotalTimeoutConstant=50;

        timeouts.ReadTotalTimeoutMultiplier=10;

        timeouts.WriteTotalTimeoutConstant=50;

        timeouts.WriteTotalTimeoutMultiplier=10;

     

        if(!SetCommTimeouts(hSerial, &timeouts)){

            FormatMessage(FORMAT_MESSAGE_FROM_SYSTEM, NULL, GetLastError(), MAKELANGID(LANG_NEUTRAL, SUBLANG_DEFAULT), dumberr, 256, NULL);

               printf("%s", dumberr);

        }

     

        printf("You have selected %s press Enter\n", com_port);

        getch();

        system("cls");

        printf("Please connect the device and press the PROGRAM button.\n");

        printf("Press ENTER when ready.\n");

        getch();

        system("cls");

        devid:

        printf("Enter desired device ID Up to 8 letters and numbers no special characters followed by \"id\": ");

        fgets (dev_id, 12, stdin);

      

        str_length = strlen(dev_id);

        if (dev_id[str_length - 3] != 'i' || dev_id[str_length - 2] != 'd'){

            if(dev_id[str_length -3] == 'I' || dev_id[str_length] == 'D'){

                printf("Must be lowercase!\n");

                printf("Press any key to try again\n");

                getch();

                system("cls");

                goto devid;

            }

            printf("You must folow with \"id\"\n");

            printf("Press any key to try again\n");

            getch();

            system("cls");

            goto devid;

        }

        system("cls");

                  

        // Write device ID

        DWORD dwBytesWrote = 0;

        !WriteFile(hSerial, dev_id, 12, &dwBytesWrote, NULL);

          

     

     

        //if (!WriteFile(hSerial, dev_id, 12, &dwBytesWrote, NULL)){

        //    FormatMessage(FORMAT_MESSAGE_FROM_SYSTEM, NULL, GetLastError(), MAKELANGID(LANG_NEUTRAL, SUBLANG_DEFAULT), dumberr, 256, NULL);

           //    printf("%s", dumberr);  

        // }

          

        // Read device ID from Device

        DWORD dwBytesRead = 0;

          

        //    if(!ReadFile(hSerial, pic_input, 256, &dwBytesRead, NULL)){

        //        FormatMessage(FORMAT_MESSAGE_FROM_SYSTEM, NULL, GetLastError(), MAKELANGID(LANG_NEUTRAL, SUBLANG_DEFAULT), dumberr, 256, NULL);

        //        printf("%s", dumberr);

        //    }

        !ReadFile(hSerial, pic_input, 256, &dwBytesRead, NULL);      

        //pic_input[dwBytesRead] = '\0';

           printf("%s", pic_input);

         

        //!ReadFile(hSerial, pic_input, 256, &dwBytesRead, NULL);

        //pic_input[dwBytesRead] = '\0';

        //printf("%s", pic_input);

        //!ReadFile(hSerial, pic_input, 256, &dwBytesRead, NULL);

        //pic_input[dwBytesRead] = '\0';

        //printf("%s", pic_input);

         

        printf("Press the clear button on the device, and press ENTER when ready.");

        getch();

        start_232f = 0;

        CloseHandle(hSerial);

        menurtn();

      

    }

     

     

    Thanks,

    George