Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Pic Microcontrollers Forum 8 bit PIC with RTC chip.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 232 subscribers
  • Views 3424 views
  • Users 0 members are here
Related

8 bit PIC with RTC chip.

asanyi
asanyi over 3 years ago

Hi, my circuit is composed from a PIC16F15345 microcontroller and a MCP79411 RTC chip, connected with i2c, it has an own 32.768 crystal. The 16F15345 also drives deprez meters and LEDs with PWM signals. While the power of the main circuit is switched off, the RTC runs correctly (precise timing) from its backup 3V battery. But activating the power of the PIC and the PWM driving, the RTC has lost its correct operation, delaying 30 minutes per 12 hour! Any idea to fix is accepted...

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago in reply to asanyi +2
    You will have far more success if you learn to plan and draw schematics. Even if freehand in your notebook they can be copied. What is a "deprez solenoids" MK
  • asanyi
    asanyi over 3 years ago in reply to ggabe +2
    Main power at normal operation, 5V: supplied the PIC VDD pin, supplied the MCP79411 RTC on pin8 VDD, supplied the anods of the LEDs. The deprez coil are drived from PWM pins of the PIC VIA NPN transistors…
  • michaelkellett
    michaelkellett over 3 years ago +1
    You need to show us the circuit diagram and ideally some pictures of the hardware. The kind of problem you describe is often caused by bad layout, inadequate power supply decoupling or ciruit errors…
Parents
  • michaelkellett
    michaelkellett over 3 years ago

    You need to show us the circuit diagram and ideally some pictures of the hardware.

    The kind of problem you describe is often caused by bad layout, inadequate power supply decoupling or ciruit errors.

    Without more information it is not possible to tell which, if any, is the cause here.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • asanyi
    asanyi over 3 years ago in reply to michaelkellett

    Michael, thanks for the fast response. Well, the project was quite simple with fast building, so there is only a handmade schematic and the circuit is soldered to a prototype PCB. But I try by words... Power supply, step by step the components: and old NOKIA cell phone charger with 6...8V DC output, 1000uF/16V electrolit + 100nF ceramic capacitor, L4941 low drop 5V regulator, 1uF tantalium capacitor on output. PIC: 100nF ceramic closest to its pin1/pin20 power connections. PIC works with internal osc, 32MHz. RTC: 100nF ceramic closest to its pin4/pin8 connections. RTC osc: 32.768 crystal on pin1 and pin2 (closest), 2x22pF ceramic. Remark: the MCP79411 datasheet offers 6pF capacitors, but trying these, not working. The rest of the circuit (2 LEDs and 2 deprez solenoids from 4 PWM output) has all together 15mA current consumption with 100 duty. Thats all. Maybe the problem is caused around the RTC crystal/capacitor fail fitting. But it is clear, only at activated PWM signals detected. Anyway, similar issue was detected at my earlier project, a vintage Nixie-tube clock. When I tried to regulate the light of the nixies by switching PWM the 170V DC nixie power, the RTC went to fail timing. With different PIC, but with the same RTC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago in reply to asanyi

    You will have far more success if you learn to plan and draw schematics. Even if freehand in your notebook they can be copied.

    What is a "deprez solenoids"

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 3 years ago in reply to asanyi

    You will have far more success if you learn to plan and draw schematics. Even if freehand in your notebook they can be copied.

    What is a "deprez solenoids"

    MK