Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Pic Microcontrollers Forum PIC 10F222 based signal conditioner.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 232 subscribers
  • Views 993 views
  • Users 0 members are here
  • 8_bit
  • microchip
  • embedded
  • Design
  • development
Related

PIC 10F222 based signal conditioner.

Catwell
Catwell over 5 years ago
Description of the problem:
 
Hall effect sensor was positioned so as to detect a shaft mounted “steal flag”.
 
The flag would pass the sensor once per revolution of the shaft. The sensor worked perfectly, however, the slower the shaft rotated, the more time it took for the flag to sweep by the sensor. At lower shaft speeds, the output pulse from the sensor was long enough to confuse the motion control computer.
 
The computer needed sensor feedback for positioning and it thought the shaft was rotating at 900 RPM instead of 40 RPM. You can imagine the potential for catastrophe.
 
The solution? Program a PIC 10F222 to perform as a one-shot. Now regardless of the length of the input pulse, the positioning computer receives a perfect, bounce-less, 5uS pulse. And the best part is that the10F series has an internal oscillator and no need for any ancillary components. All the chip needs is ~5V.
  • Sign in to reply
  • Cancel
  • Thomas
    Thomas over 16 years ago

    Hi Catwell,

     

    You have posted a problem, and also the solution for others.

    I feel using a cheap timer IC (555) as one-shot, would be a cost-effective solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Catwell
    Catwell over 16 years ago in reply to Thomas

    True, about the 555 timer, but I want to share the versatility of the 10F. Plus, the 10F needs no support components.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 16 years ago in reply to Catwell

    Hi,

     

    1/ The PIC10F222 requires absolutely no external components (internal oscillator & powerup).

    ==> The 555 DOES need a few external components (caps, resistors,...

     

    2/ The PIC10F222 includes FLASH & RAM. Therefore it's operation can be changed by simply reprogramming the internal FLASH.

    ==> The 555 operation can only be altered by changing external components (desoldering/soldering)...

     

    You can even use a cheaper microcontroller than PIC10F222 : PIC10F200 (6 pins SOT)

     

    regards