Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Documents Embedded Linux Development Platform
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: squadMCU
  • Date Created: 9 Jun 2011 3:38 PM Date Created
  • Last Updated Last Updated: 7 Oct 2021 10:03 AM
  • Views 953 views
  • Likes 0 likes
  • Comments 1 comment
Related
Recommended

Embedded Linux Development Platform

Eric started building robots at eight, and continues his passion/obsession today as the Embedded Firmware Product Specialist at Freescale Semiconductors. Because Freescale is into selling silicon and Eric is into robotics, it seems as though he’s one of the lucky few people that get paid for what they would otherwise do for free.
Eric’s latest project is extending his RobotSee software platform (http://www.EMGRobotics.com) to work with the new robot from Freescale: the Freescale Tower Mechatronic Robot. RobotSee is a free, open source robotics toolkit that works with Windows, the Chumby, Android tablets, and phones, and Linux. As you might expect, RobotSee provides a vision toolkit that includes features such as face recognition. Moreover, the toolkit — which uses an easy-to-use language with similarities to both C and Basic — supports voice recognition, speech synthesis, GPS navigation, and even an interface to those affordable brain-machine interfaces that are on the market.
The Freescale Tower Mechatronic Robot (which I’ll refer to as simply ‘Mech’) is Freescale’s first entry in the market targeting robotics enthusiasts. At $199, Freescale is positioning the robot as the next step up from robots based on the Stamp or Arduino. The basic board — which goes for $99 — uses a MC52259 32-bit microcontroller with 64K RAM and 512K Flash. It has space for two plug-in daughter boards, including a $25 magnetometer or compass and a $99 three-axis accelerometer. There’s also a pair of USB connectors, analog and digital I/O, I2C, SPI, and even a legacy RS-232 port. Development software includes free versions of CodeWarrior and RobotSee. In terms of difficulty, RobotSee is just a bit more challenging than, say, programming the BASIC Stamp. CodeWarrior, on the other hand, requires modest familiarity with C/C++ programming, and doesn’t come with built-in libraries for vision, speech, voice, and the rest.

Eric Gregori started building robots at eight, and continues his passion/obsession today as the Embedded Firmware Product Specialist at Freescale Semiconductors. Because Freescale is into selling silicon and Eric is into robotics, it seems as though he’s one of the lucky few people that get paid for what they would otherwise do for free.

 

Eric’s latest project is extending his RobotSee software platform to work with the new robot from Freescale: the Freescale Tower Mechatronic Robot. RobotSee is a free, open source robotics toolkit that works with Windows, the Chumby, Android tablets, and phones, and Linux. As you might expect, RobotSee provides a vision toolkit that includes features such as face recognition. Moreover, the toolkit — which uses an easy-to-use language with similarities to both C and Basic — supports voice recognition, speech synthesis, GPS navigation, and even an interface to those affordable brain-machine interfaces that are on the market.

 

The Freescale Tower Mechatronic Robot (which I’ll refer to as simply ‘Mech’) is Freescale’s first entry in the market targeting robotics enthusiasts. At $199, Freescale is positioning the robot as the next step up from robots based on the Stamp or Arduino. The basic board — which goes for $99 — uses a MC52259 32-bit microcontroller with 64K RAM and 512K Flash. It has space for two plug-in daughter boards, including a $25 magnetometer or compass and a $99 three-axis accelerometer. There’s also a pair of USB connectors, analog and digital I/O, I2C, SPI, and even a legacy RS-232 port. Development software includes free versions of CodeWarrior and RobotSee. In terms of difficulty, RobotSee is just a bit more challenging than, say, programming the BASIC Stamp. CodeWarrior, on the other hand, requires modest familiarity with C/C++ programming, and doesn’t come with built-in libraries for vision, speech, voice, and the rest.

 

 

Read the complete post from Bryan Bergeron on Servo Magazine

  • mc52259
  • freescale
  • robot
  • usb
  • accelerometer
  • embedded
  • development
  • magnetometer
  • platform
  • microcontroller
  • 32-bit
  • electronics
  • mechatronic_robot
  • linux
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
Parents
  • squadMCU
    squadMCU over 15 years ago

    Freescale Tower Mechatronics Robot

     

    This video is unavailable.
    You don't have permission to edit metadata of this video.

     

     

    Freescale's Mechatronics Robot, board and software allow users to experiment with acceleration, magnetic, pressure and touch sensors and microcontrollers as well as electromechanical control for industrial and consumer applications. Simple application development can be achieved in a completely programmable integrated development environment (IDE). No prior programming knowledge is needed to create embedded applications.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • squadMCU
    squadMCU over 15 years ago

    Freescale Tower Mechatronics Robot

     

    This video is unavailable.
    You don't have permission to edit metadata of this video.

     

     

    Freescale's Mechatronics Robot, board and software allow users to experiment with acceleration, magnetic, pressure and touch sensors and microcontrollers as well as electromechanical control for industrial and consumer applications. Simple application development can be achieved in a completely programmable integrated development environment (IDE). No prior programming knowledge is needed to create embedded applications.