Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Polls Will Edge Computing Transform IoT as Cloud Computing Transformed Enterprise IT?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 19 Sep 2018 9:02 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:58 PM
  • Views 2149 views
  • Likes 1 like
  • Comments 9 comments
Related
Recommended

Will Edge Computing Transform IoT as Cloud Computing Transformed Enterprise IT?

Edge computing works by selectively moving cloud-compute processing from cloud data centers to edge and end node processing platforms. Edge computing also helps to guarantee user’s privacy and security by sanitizing traffic to the Cloud, filtering personally identifiable information where necessary.

 

Edge computing systems often operate over public networks, consequently they require integration of both wired and wireless network connectivity and importantly, they require being built with a hardware root of trust. Hardware root of trust is an approach to computing where the processing of security algorithms as well as key and certificate storage are performed in trusted hardware. Hardware-based trust systems are much more robust than software-based systems against cyber-attacks seeking to compromise software-based systems.

 

So, what do you think: Will Edge Computing Transform IoT as Cloud Computing Transformed Enterprise IT?

 

(If you aren't sure, then please join me as I host our first (of many) edge computing webinars: IoT Webinar: Computing at the Edge - When, Why and How )

 

 

  • scasny_web
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dougw
    dougw over 7 years ago +8
    It is a cycle... First there were mainframes and terminals - central control Then there were PCs - decentralization Then there were severs and nodes - centralization Then there were smart phones and tablets…
  • shabaz
    shabaz over 7 years ago +5
    After the recent Edge computing webinar, I thought this was interesting : ) Using multiple cameras and heavy processing to work out distances. www.youtube.com/watch It's a very broad definition of edge…
  • mcb1
    mcb1 over 7 years ago in reply to dougw +4
    We have cloud based computing at work, where the email is held somewhere in Australia. It's a right PITA as the connection to the server will stop, take ages to connect, and is just not worth it. I fully…
Parents
  • dougw
    dougw over 7 years ago

    It is a cycle...

    First there were mainframes and terminals - central control

    Then there were PCs - decentralization

    Then there were severs and nodes - centralization

    Then there were smart phones and tablets - decentralization

    Then there was cloud computing - centralization

    Now there is edge computing - decentralization

    It seems there will always be new technology that power brokers develop and exploit to control centrally and then the technology gets cheap enough and public enough that they lose control to individuals who always want their own control. Then the cycle repeats.

    Probably the next wave will have big data swing it back to central control for a while.

    I don't know if I prefer the cycle to continue or the two phases to coalesce, but I think it would be bad if either phase dominates. (the matrix or anarchy)

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 7 years ago in reply to dougw

    We have cloud based computing at work, where the email is held somewhere in Australia.

    It's a right PITA as the connection to the server will stop, take ages to connect, and is just not worth it.

     

    I fully understand having redundancy in times of emergency, but surely this can be done in parallel with a localised server doing the delivering and mirroring the content.

     

    Mainframes and terminals were because the horsepower to drive the programs just wasn't there, and it was not as GUI intensive as it is now.

    Data transmission wasn't available like it is now ... when I first started at NZ Post Office we had 960 voice channels (with some data on top) or the entire country, but it stopped and started at 4 or 6 major centres so in theory you could handle more.

    It was an unbelievable upgrade to double that with an overlay and then fibre came along ....

     

    Mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 7 years ago in reply to dougw

    We have cloud based computing at work, where the email is held somewhere in Australia.

    It's a right PITA as the connection to the server will stop, take ages to connect, and is just not worth it.

     

    I fully understand having redundancy in times of emergency, but surely this can be done in parallel with a localised server doing the delivering and mirroring the content.

     

    Mainframes and terminals were because the horsepower to drive the programs just wasn't there, and it was not as GUI intensive as it is now.

    Data transmission wasn't available like it is now ... when I first started at NZ Post Office we had 960 voice channels (with some data on top) or the entire country, but it stopped and started at 4 or 6 major centres so in theory you could handle more.

    It was an unbelievable upgrade to double that with an overlay and then fibre came along ....

     

    Mark

    • Cancel
    • Vote Up +4 Vote Down