Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Polls Favorite microcontroller language?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: neuromodulator
  • Date Created: 20 Oct 2018 7:22 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:58 PM
  • Views 2464 views
  • Likes 1 like
  • Comments 12 comments
Related
Recommended

Favorite microcontroller language?

I like C++ a lot, specifically I love OOP and the STL. If I had to write everything in plain C I would end up writing a lot of boilerplate code ('\0' supporting strings structures and functions; and container-alike structures and functions), time I would rather like to spend on the system functionality. Still, C++ is not well supported on microcontroller, as plain C has been the defacto for a long time.

 

What is your favourite language when programming microcontrollers and why?

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 7 years ago +7
    Hi! I think for most people the beginner language might still be C with just a bit of C++ (i.e. just classes), since this is what the Arduino IDE and many example programs for Arduino use far as I can…
  • genebren
    genebren over 7 years ago +6
    I mostly use C, but I will drop down to assembly for critical timing needs.
  • glennvanderveer
    glennvanderveer over 7 years ago +6
    I am also an old school programmer from a time when RAM/ROM were at a premium and C and assembly were the only way to make programs fit and run with the limited resources...
Parents
  • johnbeetem
    johnbeetem over 7 years ago

    I use the term "microcontroller" to mean a single chip with a fairly weak CPU, a moderate amount of non-volatile memory (usually Flash or FRAM), and a small amount of RAM (usually SRAM).  Since the MCU has limited processing power and memory, it's important to use those resources efficiently.  Thus I prefer to program it in C, which is essentially a portable assembly language that uses high-level language notations.  C and ASM make it a lot easier to keep track of low-level resources and use them efficiently.  With a good compiler, C is usually as efficient as ASM these days so there's rarely a need to program in ASM.  Plus C source code is more compact than ASM and is (mostly) portable so you can use the same source code if you switch processors.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • johnbeetem
    johnbeetem over 7 years ago

    I use the term "microcontroller" to mean a single chip with a fairly weak CPU, a moderate amount of non-volatile memory (usually Flash or FRAM), and a small amount of RAM (usually SRAM).  Since the MCU has limited processing power and memory, it's important to use those resources efficiently.  Thus I prefer to program it in C, which is essentially a portable assembly language that uses high-level language notations.  C and ASM make it a lot easier to keep track of low-level resources and use them efficiently.  With a good compiler, C is usually as efficient as ASM these days so there's rarely a need to program in ASM.  Plus C source code is more compact than ASM and is (mostly) portable so you can use the same source code if you switch processors.

    • Cancel
    • Vote Up +5 Vote Down