Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Help selecting an amplifier IC
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 340 subscribers
  • Views 5014 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Help selecting an amplifier IC

jimmy5893
jimmy5893 over 5 years ago

I am working on a project with 2 other classmates of mine. We are using the analog devices ADAU1701 DSP to process audio from a device using a 3.5 mm jack. We are not using the development board, so we need to find an amplifier IC. I am looking for an IC that can provide enough power for most headphones. I have seen all sorts of numbers floating around so I am confused about what would be appropriate. The supply voltage to the IC is 8V DC max. It also can't be too hard to solder on to a PCB. I could use some help.

 

I initially was looking at TI for chips and I noticed that a lot of their "hi-fi" chips only output 0.1w or less at 16 or 32 ohms. This confused me because I have a dedicated amp (liquid spark) for my planar magnetic headphones which is a Fostex T60rp (modded), and it outputs 1.3W at 50 ohms. Some other forums said that 1 to 2 milliwatts are enough because most headphones have a sensitivity of 90-115 dB/mW. 

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 5 years ago +4
    Hi Jimmy, I recently ordered in a couple of these and found them to work pretty good: https://www.ebay.com/itm/LM386-MINI-Mono-Amplifier-Module-3V-12V-US-Seller-Fast-Shipping/111745624072?ssPageName=STRK…
  • shabaz
    shabaz over 5 years ago +4
    Hi Jimmy, A few milliwatts or low tens of milliwatts is sufficient for typical headphones or earphones. Mobile phones only output a few tens of mW to the headphone socket, and that's good enough for typical…
  • jimmy5893
    jimmy5893 over 5 years ago in reply to jw0752 +2
    Thank you, I will look into it. From the data sheet of the LM386, it can provide 325mW at 6V. So is an amplifier chip that has between 100mW and 500mW adequate for most headphones? One other thing is that…
Parents
  • aswinvenu
    aswinvenu over 5 years ago

    Hi Jimmy,

     

       Why don't you build a stereo amplifier using two LM386 on a prototyping board and test it with your headphone. If you are satisfied with the result then use it for the project.

    It won't take much time to build one from scratch.

     

    Regards,

    Aswin

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jimmy5893
    jimmy5893 over 5 years ago in reply to aswinvenu

    I heard that the LM386 is okay enough, but my friend wants a stereo IC so he doesn't have to solder two chips. Is there another option that comes to mind?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jimmy5893
    jimmy5893 over 5 years ago in reply to aswinvenu

    I heard that the LM386 is okay enough, but my friend wants a stereo IC so he doesn't have to solder two chips. Is there another option that comes to mind?