Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Help selecting an amplifier IC
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 340 subscribers
  • Views 5043 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Help selecting an amplifier IC

jimmy5893
jimmy5893 over 5 years ago

I am working on a project with 2 other classmates of mine. We are using the analog devices ADAU1701 DSP to process audio from a device using a 3.5 mm jack. We are not using the development board, so we need to find an amplifier IC. I am looking for an IC that can provide enough power for most headphones. I have seen all sorts of numbers floating around so I am confused about what would be appropriate. The supply voltage to the IC is 8V DC max. It also can't be too hard to solder on to a PCB. I could use some help.

 

I initially was looking at TI for chips and I noticed that a lot of their "hi-fi" chips only output 0.1w or less at 16 or 32 ohms. This confused me because I have a dedicated amp (liquid spark) for my planar magnetic headphones which is a Fostex T60rp (modded), and it outputs 1.3W at 50 ohms. Some other forums said that 1 to 2 milliwatts are enough because most headphones have a sensitivity of 90-115 dB/mW. 

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 5 years ago +4
    Hi Jimmy, I recently ordered in a couple of these and found them to work pretty good: https://www.ebay.com/itm/LM386-MINI-Mono-Amplifier-Module-3V-12V-US-Seller-Fast-Shipping/111745624072?ssPageName=STRK…
  • shabaz
    shabaz over 5 years ago +4
    Hi Jimmy, A few milliwatts or low tens of milliwatts is sufficient for typical headphones or earphones. Mobile phones only output a few tens of mW to the headphone socket, and that's good enough for typical…
  • jimmy5893
    jimmy5893 over 5 years ago in reply to jw0752 +2
    Thank you, I will look into it. From the data sheet of the LM386, it can provide 325mW at 6V. So is an amplifier chip that has between 100mW and 500mW adequate for most headphones? One other thing is that…
Parents
  • jc2048
    jc2048 over 5 years ago

    Rohm have a reasonable range of audio parts. I can't see anything there that would give you everything you want, though.

     

    https://www.rohm.com/products/audio-video/audio-amplifiers

     

    On Semi is another manufacturer you could look at, though again it doesn't look like they have anything that would meet all your criteria.

     

    https://www.onsemi.com/products/amplifiers-comparators/audio-power-amplifiers

     

    I can't recommend any of these. Not the kind of design I've ever done.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 5 years ago in reply to jc2048

    The Sennheiser HD 600 phones need 1V rms for 102db, a typical small power amp running off a 5V supply will just about do this. The power (to the headphones) will be about 3mW.

    Many headphones are lower impedance and will need less voltage for the same power.

    I don't think you'll easily find a very low distortion headphone amp that will work from a single 5 - 8V supply.

    The LM4880 would be a good sensible bet, distortion about 0.1% at 200mW, 2 channels, can manage about 1V RMS output, easy to use 20 pin DIP packaging. It can drive 200mW into 8ohm speakers.

     

    THe MAX13331 comes closer to your ideal in performance but is in a more difficult to solder package. It can't drive an 8 ohm speaker load so well.

     

    If you want loud into the Sennheiser phones and the abilty to drive speakers with a watt or more then you'll need more power supply volts, becaue you will need about 5V RMS which means a 20V power suppply span.

     

    If I were you I'd go for the LM4880, cheap and easy to use, if you want to drive speakers then use powered speakers.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 5 years ago in reply to jc2048

    The Sennheiser HD 600 phones need 1V rms for 102db, a typical small power amp running off a 5V supply will just about do this. The power (to the headphones) will be about 3mW.

    Many headphones are lower impedance and will need less voltage for the same power.

    I don't think you'll easily find a very low distortion headphone amp that will work from a single 5 - 8V supply.

    The LM4880 would be a good sensible bet, distortion about 0.1% at 200mW, 2 channels, can manage about 1V RMS output, easy to use 20 pin DIP packaging. It can drive 200mW into 8ohm speakers.

     

    THe MAX13331 comes closer to your ideal in performance but is in a more difficult to solder package. It can't drive an 8 ohm speaker load so well.

     

    If you want loud into the Sennheiser phones and the abilty to drive speakers with a watt or more then you'll need more power supply volts, becaue you will need about 5V RMS which means a 20V power suppply span.

     

    If I were you I'd go for the LM4880, cheap and easy to use, if you want to drive speakers then use powered speakers.

     

    MK