Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum What is your must have 3D printer option?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 303 subscribers
  • Views 855 views
  • Users 0 members are here
  • 3d pinting
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

What is your must have 3D printer option?

colporteur
colporteur over 5 years ago

Can you provide a list of three options that must be included, if you are going to purchase of a 3D printer?

 

I have been asked to provide a list of options for evaluating the selecting of a 3D printer. A friend of mine is considering making a purchase.  He has no experience with 3D printers. He is looking for some insight before making the purchase. The only experience I have with 3D printers is, having attended a few of the sessions of 3D Printing For Makers: Free 4 Part Webinar Series . After reviewing my notes I came up with the following list.

 

  • Number of extruders
  • Type of polymer supported
  • Closed or open case
  • Heated deck
  • Software

 

The list is pretty short. I am unable to rank importance. I'm looking for input from the Experts or rather those people that have or have used a 3D printer. These people from experience have insight into the printing. I'm thinking they can provide a recommendation on options they feel can make or break a 3D printer. If you are aware of a gotchas to avoid that would be appreciated.

 

The printer purchase is for a resident of Canada. The budget for the project is less than thousand in Canadian dollars. I would speculate the printer will be used to support primarily designs within a model railroad environment. The user is not experienced and has basis computer user skills.

 

If you were looking to purchase a 3D printer, what would be your must have options?

  • Sign in to reply
  • Cancel

Top Replies

  • Sean_Miller
    Sean_Miller over 5 years ago +3
    For a filament printer: Open source filament. (meaning, you don't have to buy their cartridges like XYZ Printing) Software that allows full control of settings throughout the process like Repetier Aluminum…
  • dixonselvan
    dixonselvan over 5 years ago +3
    Let me tell you this first I am not an expert in 3D printing or printers but a few years back I had a similar question while choosing which 3D printer to buy. So I am sharing my experience with you here…
  • dougw
    dougw over 5 years ago +2
    Number one feature needed is the ability to change filament in the middle of a print - so you don't need to worry if there is enough to complete the print and you can use spools all the way to the end…
Parents
  • dougw
    dougw over 5 years ago

    Number one feature needed is the ability to change filament in the middle of a print - so you don't need to worry if there is enough to complete the print and you can use spools all the way to the end.

    Number two is a heated bed with auto-release surface - hot plastic sticks to it but when it cools, the part is no longer stuck.

    Number three is an open chassis that allows easy access to all parts - some closed chassis machines are extremely difficult to service and maintain.

    Number four is a quiet machine, but it doesn't trump easy access.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 5 years ago in reply to dougw

    DW, you indicate close chassis. I read a review where the case being closed reduces problems with the model during cooling (i.e.no drafts in a closed case.) Care to comment?

     

    Break...Break...

    What printer are you currently using? Are you satisfied with it performance?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 5 years ago in reply to colporteur

    Enclosed cases do seem to maintain warmer ambient air and contain noise better but the printer I use most (Anycubic I3 Mega) is open and it has no problems with delamination or other thermal issues. I have used it for several years and hundreds of prints and never even had to relevel it.

    Before this printer, I would have rated automatic bed levelling as a pretty important feature, so that is probably still useful if bed leveling performance is unknown.

    I have a larger printer that had some issues keeping the large bed uniformly hot so I built an insulated thermal enclosure and monitored the temperature at various locations inside. I also used a heat gun to try and ensure the temperature was what I wanted at all locations. It was a lot of work throughout the print but it did help. For that printer, and printing large objects, just the enclosure was not helping enough to be a useful feature. The heat gun without the enclosure was far more effective in achieving desired temperatures - mainly it was needed during the first 15 minutes of a print job.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 5 years ago in reply to colporteur

    Enclosed cases do seem to maintain warmer ambient air and contain noise better but the printer I use most (Anycubic I3 Mega) is open and it has no problems with delamination or other thermal issues. I have used it for several years and hundreds of prints and never even had to relevel it.

    Before this printer, I would have rated automatic bed levelling as a pretty important feature, so that is probably still useful if bed leveling performance is unknown.

    I have a larger printer that had some issues keeping the large bed uniformly hot so I built an insulated thermal enclosure and monitored the temperature at various locations inside. I also used a heat gun to try and ensure the temperature was what I wanted at all locations. It was a lot of work throughout the print but it did help. For that printer, and printing large objects, just the enclosure was not helping enough to be a useful feature. The heat gun without the enclosure was far more effective in achieving desired temperatures - mainly it was needed during the first 15 minutes of a print job.