Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Need some help choosing a 0.96" OLED and a connector
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 339 subscribers
  • Views 5824 views
  • Users 0 members are here
  • oled
  • ssd1306
  • ffc_cable
  • display
  • ffc/fpc_connector
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Need some help choosing a 0.96" OLED and a connector

starfox5194
starfox5194 over 5 years ago

image

I am trying to fit this 0.96" SPI OLED SSD1306 screen into my dash cluster. Although the screen fits, the controller board must be relocated.

I want to use SPI, not I2C for the draw speed.

image

Problem is, I damaged the screen when I used a heat gun to de-solder the screen from the control-board. Screen still kind of works, but I would like to re-do this with less soldering down the road.

 

This SPI display does not come with a controller board, and the connection is a 30-pin 0.7mm pitch. 0.7mm is non-standard, so I can't find a connector to make a solder-free extension.

https://www.buydisplay.com/datasheet-128x64-oled-module-spi-0-96-inch-graphic-displays-white-on-black

 

This I2C display uses a 0.5 mm pitch. But I don't know if there is a controller board that I can connect this to that is cheap and affordable.

https://www.buydisplay.com/128x64-oled-i2c-0-96-display-white-color-connector-fpc-ssd1306

 

Does anyone have any suggestions for me? I really need to keep the 0.96" dimension, I just need a way to relocate the breakout board with ease!

 

Thanks,
Alex

  • Sign in to reply
  • Cancel

Top Replies

  • Fred27
    Fred27 over 5 years ago +2
    Redesigning the PCB might be the easiest. Your other option would be to design a longer flex PCB to replace the existing one. That would be interesting to do, but likely to be more expensive - and quite…
  • Fred27
    Fred27 over 5 years ago +1
    I seem to be having permission problems seeing the photos you've attached.
  • starfox5194
    starfox5194 over 5 years ago in reply to shabaz +1
    Sorry the photos were not working. I tried uploading them to imgur this time. https://imgur.com/a/peHIm8c The controller board I am referring to is the OLED controller board, not the microcontroller board…
Parents
  • shabaz
    shabaz over 5 years ago

    I cannot see the photos either, but the 0.7mm pitch one is designed for soldering on a PCB, so there will be no connector for that.

    I didn't understand the requirement, by controller board do you mean an adapter board to go from 0.7mm to 0.5 mm? or to translate from one protocol to another?

    Do you mean a microcontroller board? Any microcontroller can communicate to the display, provided you can supply the voltages needed by the OLED module (usually they need one unusual voltage but if you already have a board for the 0.7mm pitch part, then it will already have such a supply).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 5 years ago

    I cannot see the photos either, but the 0.7mm pitch one is designed for soldering on a PCB, so there will be no connector for that.

    I didn't understand the requirement, by controller board do you mean an adapter board to go from 0.7mm to 0.5 mm? or to translate from one protocol to another?

    Do you mean a microcontroller board? Any microcontroller can communicate to the display, provided you can supply the voltages needed by the OLED module (usually they need one unusual voltage but if you already have a board for the 0.7mm pitch part, then it will already have such a supply).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • starfox5194
    starfox5194 over 5 years ago in reply to shabaz

    Sorry the photos were not working. I tried uploading them to imgur this time.

    https://imgur.com/a/peHIm8c

     

    The controller board I am referring to is the OLED controller board, not the microcontroller board (ESP32)

     

    I am trying to figure out the simplest way install the screen without using the 30 wires you can see I added in the photos.

     

    I think my best option now is to download Adafruit's eagle schematic and redesign the PCB to be a slightly different shape to fit my needs. I've never used eagle before, so this is going to be interesting.

    https://github.com/adafruit/Adafruit-128x64-Monochrome-OLED-PCB

     

    Still, if there is a better way to do this, please let me know!

    image

     

    image

     

    image

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 5 years ago in reply to starfox5194

    As Fred says would be the cleanest option. Another option could be to use flat flex cable, and two PCBs created, one either end (and fold the flat flex at 45 degrees to make a 90 degree turn, if you see what I mean).

    It's all a complication though! The wires can be reliable too, (or use ribbon cable) but perhaps with a PCB if possible, rather than directly onto the display (i.e. have a small PCB where the display is, where you can solder in the display, and run your wires, either soldered to the PCB and then secured, or using a connector, if you have space).