Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Any beginner tips for Nvidia Jetson?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 305 subscribers
  • Views 3193 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Any beginner tips for Nvidia Jetson?

lorrainbow
lorrainbow over 4 years ago

Hi,

I'm using a Nvidia Jetson board, the 2gb for now moving onto the 4gb later, to track people. I tried setting it up and installing a demo project but ran into lots of errors - a common one was running out of memory and the whole thing freezing on me.

I'm thinking I missed a setup step where I needed to partition the memory??

 

Does anyone know of any setup guides for this board? If it works for what I need to do I might need between 6 and 12 of them! So would like a nice easy setup routine that just works.

 

Thanks!

Lorraine

  • Sign in to reply
  • Cancel

Top Replies

  • yosoufe
    yosoufe over 4 years ago +2
    If it freezes and it does not unfreeze, you may increase the swap size. https://www.jetsonhacks.com/2019/11/28/jetson-nano-even-more-swap/ and also running headless should help.
  • mp2100
    mp2100 over 4 years ago +1
    lorrainbow I just got my own Jetson Nano 2 GB, so I'm a beginner too. I have not run any of the demos yet, and of course the demos were probably created for the 4GB model. (but microcenter in the US had…
  • lorrainbow
    lorrainbow over 4 years ago in reply to mp2100 +1
    Thanks Allen, yeah I'm guessing the demos are for the 4gb model too! I've got that on order as it was out of stock. I did stick with the default 2gb swap, then had to change it cause it kept freezing.…
  • mp2100
    mp2100 over 4 years ago

    lorrainbow  I just got my own Jetson Nano 2 GB, so I'm a beginner too.  I have not run any of the demos yet, and of course the demos were probably created for the 4GB model.  (but microcenter in the US had the 2GB on sale for $50, couldn't pass that up. )

     

    I downloaded the new operating system "Jetpack 4.5", new version from January 2021.  How much swap do you have? On mine, by default it set swap to 2.5 GB.  You could try setting it higher. Here's an example for a raspberry pi that I have used successfully: https://pimylifeup.com/raspberry-pi-swap-file/

     

    I do have to say, the jetson nano 2Gb is fast, faster than my Pi 4.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • lorrainbow
    lorrainbow over 4 years ago in reply to mp2100

    Thanks Allen, yeah I'm guessing the demos are for the 4gb model too! I've got that on order as it was out of stock.

     

    I did stick with the default 2gb swap, then had to change it cause it kept freezing.

     

    Thanks for the guide.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mp2100
    mp2100 over 4 years ago in reply to mp2100

    My skill level on the Jetson:

    image

     

    But I am really looking forward to running the demos.  Here's hoping they will run.  Some of the instructions say, "run it overnight".  I do plan to increase my swap to, say, 4 GB, if it lets me, to move memory up to near the jetson nano 4GB model, even at the cost of slow swapping.

     

    Also, I see new to Jetpack 4.5, they do have a way to boot from USB, so changing from an SD card boot to a nice USB SSD drive will be nice, especially for swappiness.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • yosoufe
    yosoufe over 4 years ago

    If it freezes and it does not unfreeze,

    • you may increase the swap size. https://www.jetsonhacks.com/2019/11/28/jetson-nano-even-more-swap/
    • and also running headless should help.
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 4 years ago in reply to mp2100

    Operating system swap partitions/files are typically 2.5* the amount of RAM you have available, that way it can 'swap' out the entire amount of RAM, and a bit extra.

     

    If it's running linux you can also setup swap as a file (Increasing Linux Swap with a File - instructions may vary depending on linux version) as opposed to a partition, and locate it on say, a USB stick, but obviously that'll be even slower.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mp2100
    mp2100 over 4 years ago in reply to mp2100

    Sorry, bad answer about swap.  That Pi link definitely did NOT work.  (note to self: don't assume raspbian is the same as debian )

     

    The nano is running ubuntu 18.04, I'm going to try this next:

    https://askubuntu.com/questions/1075505/how-do-i-increase-swapfile-in-ubuntu-18-04

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mp2100
    mp2100 over 4 years ago in reply to yosoufe

    Thanks Yousof, I will try that link, specific to the nano.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • yosoufe
    yosoufe over 4 years ago in reply to mp2100

    np. by the way this YouTube channel becomes your good friend when working with jetson https://www.youtube.com/channel/UCQs0lwV6E4p7LQaGJ6fgy5Q