Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Looking for support resources for GNURadio
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 338 subscribers
  • Views 3926 views
  • Users 0 members are here
  • gnuradio
  • troubleshooting gnuradio
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Looking for support resources for GNURadio

colporteur
colporteur over 5 years ago

Can you share resources you have used or are aware of for troubleshooting issues with GNURadio software installation on Ubuntu?

 

I am receiving error messages when I try to use a Audio Source or Audio Sink block? My goal was to test the GNURadio installation using a audio source and audio sink block and/or Signal Source and Audio sink blocks and have it play a tone from the computer speaker. I have followed the suggested fixes in the following link because they make some reference to Audio. It didn't resolve my issue.

https://wiki.gnuradio.org/index.php/ALSAPulseAudio

https://wiki.gnuradio.org/index.php/Audio_Source

https://wiki.gnuradio.org/index.php/Audio_Sink

 

The environment:

tried

GNURadio version 3.8.1.0 (Python 3.8.5): Ubuntu package install

tried

GNURadio version 3.9 Ubuntu package install

Ubuntu 20.04.2 LTS

uname -r 5.8.0-43-generic

 

I have been unsuccessful in getting a response from the mailing GNURadio list https://lists.gnu.org/mailman/listinfo/discuss-gnuradio so I can post a question. IT appears to be active but I get no response from my subscription attempts. I had hoped someone has experienced a similar problem and can offer advice.

 

I'm looking for your go-to resource for troubleshooting GNURadio issues. Can you help?

 

Error Messages:

Audio Source error

Generating: '/home/user/Documents/GNURadio/audio.py'

 

Executing: /usr/bin/python3 -u /home/user/Documents/GNURadio/audio.py

 

Warning: failed to XInitThreads()

Traceback (most recent call last):

File "/home/user/Documents/GNURadio/audio.py", line 128, in <module>

main()

File "/home/user/Documents/GNURadio/audio.py", line 106, in main

tb = top_block_cls()

File "/home/user/Documents/GNURadio/audio.py", line 76, in __init__

self.audio_source_0 = audio.source(samp_rate, 'pulse_monitor', True)

AttributeError: type object 'audio' has no attribute 'source'

>>> Done (return code 1)

 

Audio Sink error

Generating: '/home/user/Documents/GNURadio/audio.py'

 

Executing: /usr/bin/python3 -u /home/user/Documents/GNURadio/audio.py

 

Warning: failed to XInitThreads()

Traceback (most recent call last):

File "/home/user/Documents/GNURadio/audio.py", line 130, in <module>

main()

File "/home/user/Documents/GNURadio/audio.py", line 108, in main

tb = top_block_cls()

File "/home/user/Documents/GNURadio/audio.py", line 77, in __init__

self.audio_sink_0 = audio.sink(samp_rate, 'hw:0,0', True)

AttributeError: type object 'audio' has no attribute 'sink'

 

>>> Done (return code 1)

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 5 years ago +3
    I found a solution but have gained little knowledge of the root cause of the issue. With a complete fresh install of Ubuntu 20.02.2 LTS and using the resident software manager to install GNURadio 3.8.1…
  • cstanton
    cstanton over 5 years ago +1
    At a glance this looks like an outdated library, or a missing library ('audio' , since from "gnuradio import audio"). The type 'audio' not having an attribute 'sink' would mean that the code either couldn…
Parents
  • cstanton
    cstanton over 5 years ago

    At a glance this looks like an outdated library, or a missing library ('audio' , since from "gnuradio import audio"). The type 'audio' not having an attribute 'sink' would mean that the code either couldn't interrogate and create an 'instance' of the audio object to refer to, or it isn't defined in the library for 'audio' that 'sink' even exists in it.

     

    Updating from an older version of the libraries to a newer one, and thus creating the dependencies would explain why GNURadio, when using or compiling the same version, would then work.

     

    Either it was interrogating a more localised python library install for GNURadio or the system wide python library install and somewhere along the line realised the dependencies it needed and installed the right ones.

     

    Other typical explanations for these are often down to permissions and having the correct access to folders.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cstanton
    cstanton over 5 years ago

    At a glance this looks like an outdated library, or a missing library ('audio' , since from "gnuradio import audio"). The type 'audio' not having an attribute 'sink' would mean that the code either couldn't interrogate and create an 'instance' of the audio object to refer to, or it isn't defined in the library for 'audio' that 'sink' even exists in it.

     

    Updating from an older version of the libraries to a newer one, and thus creating the dependencies would explain why GNURadio, when using or compiling the same version, would then work.

     

    Either it was interrogating a more localised python library install for GNURadio or the system wide python library install and somewhere along the line realised the dependencies it needed and installed the right ones.

     

    Other typical explanations for these are often down to permissions and having the correct access to folders.