Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Using transformer secondary windings
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 302 subscribers
  • Views 2097 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Using transformer secondary windings

colporteur
colporteur over 4 years ago

image

Can I use both secondary windings to power separate loads?

 

I have a need for two 4.5VAC power supplies.

I have a transformer that is 9VAC with a center tap. I would like to connect one load to one 4.5VAC O/P and the other load to the other 4.5VAC. I'm assuming I can do this, provided I don't exceed the max current rating. It has been a long time since I have dabbled this low in analogue. I was looking for some reassurance or refresher.

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 4 years ago in reply to Jan Cumps +3
    Thanks JC for the reply. The AC loads are two small model railroad buildings that require 4.5VAC. It looks like they have some internal electronics to generate power for the few LEDS scatter around. It…
  • gdstew
    gdstew over 4 years ago +1
    As far as I can remember you can use a half wave rectifier on both output taps and the share the center tap as ground there is no problem with the circuits connecting to each other. Using half wave rectification…
  • colporteur
    colporteur over 4 years ago in reply to gdstew +1
    Only need the AC. I have no need for the rectifier stuff.
Parents
  • Jan Cumps
    Jan Cumps over 4 years ago

    Yes if they power two separate circuits that don't share any DC nodes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 4 years ago

    Yes if they power two separate circuits that don't share any DC nodes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • colporteur
    colporteur over 4 years ago in reply to Jan Cumps

    Thanks JC for the reply. The AC loads are two small model railroad buildings that require 4.5VAC. It looks like they have some internal electronics to generate power for the few LEDS scatter around.

     

    It is hard enough to find an AC output adaptor but to find one with that small a voltage was difficult. My electronics training from 40 years ago suggested, why not take apart a DC wall wart and just use the transformer. Some na-sayers on the floor said, "you can't do that!" so I began to have second doubts.

     

    It too me a few tries to find a suitable DC adaptor at the thrift store. After getting at the guts of the adapater and measuring the windings, I still had my doubts. I do more digital electronics than analogue with my legacy knowledge so it tends to be a bit rusty. I got lazy and didn't want to dig out my text books to find the answers. I figured one of the smart peoples that hang out here would respond.

    • Cancel
    • Vote Up +3 Vote Down