Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Have a question about multimedia or audio? Ask our Expert, Ken Boyce
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 97 replies
  • Subscribers 312 subscribers
  • Views 7824 views
  • Users 0 members are here
  • communications
  • audio
  • expert
  • multimedia
  • ken_boyce
  • consumer_electronics
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Have a question about multimedia or audio? Ask our Expert, Ken Boyce

nlarson
nlarson over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Communications in the element14 Community Wireless Communications Technology group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

KenBoyce

 

Ken Boyce

Ken has 40 years of experience and his expertise spans the multimedia, communications and consumer electronics industries.  He has a personal interest in audio and multimedia related subjects.

 

  • Sign in to reply
  • Cancel
Parents
  • mberman
    mberman over 15 years ago

    Hi Ken,

    I liked your comprehensive response to the questions about LCD and Plasma HDTVs.  I have a Lenovo laptop that only has a 9-pin VGA monitor output and my Sharp HDTV does not have this type of input.  Have you used any of the laptop to HDTV "wireless" transmitters available today to view A/V material (e.g., YouTube, online TV shows) from the web on your HDTV?  I have a Wi-Fi set-up at home that works well.  In fact, streaming Netflix video via the Roku receiver I have looks great and has 720p resolution without interruptions. Any suggestions for a good laptop VGA or "USB 2.0" to HDTV wireless transceiver?

    Many Thanks, Mel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mberman
    mberman over 15 years ago

    Hi Ken,

    I liked your comprehensive response to the questions about LCD and Plasma HDTVs.  I have a Lenovo laptop that only has a 9-pin VGA monitor output and my Sharp HDTV does not have this type of input.  Have you used any of the laptop to HDTV "wireless" transmitters available today to view A/V material (e.g., YouTube, online TV shows) from the web on your HDTV?  I have a Wi-Fi set-up at home that works well.  In fact, streaming Netflix video via the Roku receiver I have looks great and has 720p resolution without interruptions. Any suggestions for a good laptop VGA or "USB 2.0" to HDTV wireless transceiver?

    Many Thanks, Mel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 15 years ago in reply to mberman

    Hi Mel,

     

    I am sorry, but I have not tried any laptop to HDTV connections.  It should be very similar to connecting a laptop to an outboard projector.  A cable is run from the laptop to the projector, then at the computer you can use ALT-F7 (I forget which exactly) and choose the display mode for 2 monitors.  One will be the laptop screen itself, and the other should then be the HDTV (provided it has an PC input mode).  I am sure you know this already.  However, I would have thought you could get a 9-pin to 15-pin adapter cable somewhere without having to go a "wireless" direction.  I never ran into the problem before.   I have no experience with any product for this purpose other than a cable interconnect.

     

    If I get a chance, I may try this over the weekend as I need to take my laptop to a location where there is a small isolated HDTV that does have PC input. But if my memory is correct, everything is 15 pin interconnects.

     

    Ken

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to mberman

    Mel,

     

    I did not find any 9-15 pin cables locally, but check out this link for how to make one.  Good luck.

     

    http://www.hardwarebook.info/9_to_15_pin_VGA

     

    Ken

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mberman
    mberman over 15 years ago in reply to Former Member

    Hi Ken,  Many Thanks for your kind research and the info you provided.

    Turns out that the VGA output from computers is analog in nature and not directly compatible with the digital HDMI input of HDTVs.

    And, since I want a "wireless" connection, I found that there are a few VGA to HDMI transceivers available, but I was wondering if you had any experience with them (and you did not not---no problem).  All the Best, Mel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ksmith
    ksmith over 15 years ago in reply to mberman

    Mel,

     

    It may be worth checking into different set top boxes that will take streaming video from a computer and display it on your TV. This works great for things like videos and such you have on your computer. Not so sure it would work all that well if you want to display your actual computer screen onto the TV and operate the computer from there.

     

    Many of the major game consoles (PS3, XBox, etc) will allow this either natively or with some "tweaking" done. And I know there are a few other types of devices that do it, but I'm not really up on the subject.

     

    But I think you're looking for more of a pure adapter cable type of thing and for that I'm not really sure. The issue of the analog vs digital is probably going to be the big issue with finding such a device that would work well.

     

    If you do come up with something please post it hear as I wouldn't mind having that as well. Could certainly come up with some nice uses for some older computers if there's an easy (and not expensive) way of doing it.

     

    -Kent

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mberman
    mberman over 15 years ago in reply to ksmith

    Hi Kent,

    Yes, I heard of the PS3 and XBox working as laptop interfaces to an HDTV, but I don't own either of those gaming consoles.  However, there are a couple USB 2.0 to HDMI "wireless" transceivers on the market today.  They seem to have mixed reviews however.  Below are the weblinks for your info and/or investigation.  Please let me know if you find a good solution.  In my case I have a Lenovo laptop running Windows XP 2nd Ed with VGA and USB 2.0 ports.

    Thanks, Mel

    http://reviews.costco.com/2070/11515142/reviews.htm?pageNumber=2

    http://www.amazon.com/Warpia-Wireless-Projector-Display-Converter/dp/B002XISRJS