Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Have a question about multimedia or audio? Ask our Expert, Ken Boyce
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 97 replies
  • Subscribers 312 subscribers
  • Views 7820 views
  • Users 0 members are here
  • communications
  • audio
  • expert
  • multimedia
  • ken_boyce
  • consumer_electronics
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Have a question about multimedia or audio? Ask our Expert, Ken Boyce

nlarson
nlarson over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Communications in the element14 Community Wireless Communications Technology group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

KenBoyce

 

Ken Boyce

Ken has 40 years of experience and his expertise spans the multimedia, communications and consumer electronics industries.  He has a personal interest in audio and multimedia related subjects.

 

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 15 years ago
    Hi do you have any information about any product based on BU9458 or BU9457. This is very interesting chips for MP3 decoding controlled by I2C from Romh. I need information if any succesfull product is based on this chip but I need independant opinion (not from Romh) about these chips. Best Regards Alex
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    Hello Alex,

     

    Unfortunately I do not have any product based experience with the BU9458 or BU9457 devices from Rohm.  Nor do I know of a commercial product on the market that uses them.

     

    Also, it appears that the datasheets for those devices do not offer much info on any application circuit.  So I can't really judge very well a potential product design based on them.

     

    However, the basic idea of the parts is good in that you have both SD card and USB (flash memory drive) as input sources for the formatted audio material.  Also, a key advantage is that the part can operate self contained as a decoder or can be controlled via an external processor/micro-controller.

     

    My direct experience with an MP3 player design was one involving a PIC microcontroller + an MP3 decoder which in turn was controlled by a larger CPU running a complex system that happened to need audio at various operations.  That design used a standard SD card with very simple file naming structure which may not meet your needs.  If you want more info on this, let me know.

     

    Ken

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member
    Thank you very much.
    I find solution thanks to Element14 PDF files on the server which are not has been available on any other place (even I could find that kind documentation on Rohm site) and later I got help from Anglia by providing to me Demo board and more info, but essentially this is the same information found on Element 14 for BU9458. There has been problem with information about "access code" as that part of information has not being 100% documented ( This is not so obvious until you try to finish product by using available information form PDF). After solving that problems chip is so easy to use and work perfectly. Really nice things are, that firmware inside the chip do all for you and find out about what kind a memory you are using (FAT32, 16, sectors, organizations etc). Even it is possible to read data from USB or SD not necessary MP3. Thanks to BU9458, Microcontroller can use large SD and USB not just to control music. It is possible to Read USB or SD and use this information to flash micro controller or just to use data for some other useful purpose to microcontroller as configurations files for example.
    Thank you very much again and best regards
    Alex
     
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    Hi Alex,

     

    Thank you for updating me on your project.  I am glad it has worked out well for you.  It would be great if Rohm improved their data sheet content.

     

    Kind regards,

    Ken

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • davidefa
    davidefa over 15 years ago in reply to Former Member

    Hi Aleksandar, I'm trying to understand the "access data" too.

    Chould you kindly specify the sequence of commands to extract directory/files names ( in mode3 )?

    For example:


    - how to read the name of the first folder (It shold be the root folder)?

    - how to read the name of the first file in the first folder?

    - how to read the name of the second file in the first folder?

    ...

     

    - how to read the name of the second folder ( I mean the first folder in the root folder)?

    - how to read the name of the first file in the second folder?

    - how to read the name of the second file in the second folder?

    ...

    - how to read names of subfolders too?

     

    Regards

     

    Davide Fabbri

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to davidefa

    Ha-ha... those are exactly questions which I had before I find the solution. And this just proves that definitely there is a need for more information to be added to PDF files about BU9457X.
    I will not surprise if you all ready find one for yourself. But if you did not I will provide you more information.

     

    I am working on MP3 player with microchip graphic TFT solutions and PIC 32. I also using mod 3 for BU9458 (BU9457 and BU9458 are equally good and no software need to be changed, hardware is the same as well).

    What I will explain here I do not claim that this is the very best solution (as there is not documented that this is the right way how need to be done but its work perfectly and I strongly suspect that this is idea of designers of BU9457x how to control BU9457X in order to play right MP3 file.

    If you find better solution please let me know although as I say this solution working perfectly well for me.

     

    1. Very first you need to use command SET DIRECT and access code, should be 0, 0, 0, 0, 0, 0.
    (All binary zeros not ASCII).

    2. Then use GET DIRECT

    3. Then use READ FILE INFO command

    4. Then use READ BUFFER from 20 (think as memory location 20 hex and it is called COMAREA)

    Now use access code which you get from process in steps 3. and 4.. You can find access code information from buffer comarea and use this access code to SET DIRECT in next step.

    5.SET DIRECT ( StatusOutputOffset[25hex}, ...24,23,22,21…;StatusOutputOffset[20hex])

    You are ready for first MP3 to play, by setting command PLAY DIRECT.

    6. PLAY DIRECT  this will start the music (if you all ready have your SD or USB files with MP3)

    That command will play very first MP3, but what if  you don’t want to play very first song?


    Then you need to repeat steps 3. Then 4. N times in case that your song is song number N.

     

    But how to be sure that song number N is the right one?

     

    Just repeat 3. (Read file info) and after 4. ( Read buffer comarea from 20 hex)


    You have information in comarea about name of the song (MP3 file). If this is right one just set command play if not continue to repeat steps 3. and step 4 read until you get right one.

     

     

    Now there is more then that. For example you need to wait that BU9458 is available by checking status 1 , 2, 3 etc to confirm that BU945X is analyzed all and is not busy, that BU945X has recognized USB or SD but I recommend at first stage to simplified all by using loops of 10 ms so you can avoid to read STATUS 1,2,3 etc between each steps.  When you have mastered control over BU945X then you can add more improvement (for start use even more then 10 ms, 100 ms will ensure that between each step (commands) are more then enough time and is definitely long enough for all internal processes inside BU9457X so you can use what I explain and without checking STATUS 1,2…


    If all of that is not working for you probably you having problems with I2C communication.


    Any way I can send you my C code (give me your e mail), if you promise that you will not laugh on my code, but don’t forget…. my code works image

     

    Best Regards Alex

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to davidefa

    Just to add on my previous e mail as a replay to you.

    Try first to take control over BU9457X as I describe to you, play little bit with chip and then use PDF file to understand how to get names of files and folders (you get names and folders by repeating steps 3 and 4 and reading from COMAREA).

    Although document is not specific for repeating steps 3 and 4 the rest of the document is good.

    So you can use existing Rohm PDF files to get to the bottom of all problems.

    Everything is easy if you manage to do what I explain to you.

    The moment when you do, Rohm document suddenly has a sense… or document is fine but we just can not find sense in the document for that part.

    Whatever is the case I am sure after trying mu suggestion everything will work fine for you…

    Best Regards Alex

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • davidefa
    davidefa over 15 years ago in reply to Former Member

    Thank you very much Alex.

    Your description is crystal clear. After the call to SET DIRECT 000000, GET DIRECT, need call READ FILE INFO repeatedly to scroll all files.

    It would be great if you could send me your C code at: element14 at davidefabbri dot net ( No laugh, I swear )

     

    Davide Fabbri

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to davidefa
    Yes that is exactly the case and I cannot believe… you explain same thing in just one sentence!

     

    Definitely I should be politicians!

     

    Later one I will send you source code.

     

         Best Regards Alex

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • davidefa
    davidefa over 15 years ago in reply to Former Member

    !!!!!!!!!!!!!!!!!!!!!!!!

    !                      !

    !  Alex for President  !

    !                      !

    !!!!!!!!!!!!!!!!!!!!!!!!

     

    Thank you for sharing your code ( and your schematic ), now I have a good ( and working ) starting point.

    The project is an 'mp3 player for armchairs': a client of us produces relaxing/massaging armchairs, and he want to add this function to his armchairs.

    The player should have an usb input ( so each one with an usb memory could listen to his favorite music ).

    Two versions are planned: a 'dumb version' ( with no display ) and a 'smart version' ( with grafical display ) and bu9457/8 addresses both versions.

     

    P.S. oddly enough rohm applications for bu9457/8 already knows of this strange use ( as an mp3 player for armchairs ), the image is from rohm site

     

    http://www.rohm.com/ad/usb_audio/images/pic_05.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • davidefa
    davidefa over 15 years ago in reply to Former Member

    !!!!!!!!!!!!!!!!!!!!!!!!

    !                      !

    !  Alex for President  !

    !                      !

    !!!!!!!!!!!!!!!!!!!!!!!!

     

    Thank you for sharing your code ( and your schematic ), now I have a good ( and working ) starting point.

    The project is an 'mp3 player for armchairs': a client of us produces relaxing/massaging armchairs, and he want to add this function to his armchairs.

    The player should have an usb input ( so each one with an usb memory could listen to his favorite music ).

    Two versions are planned: a 'dumb version' ( with no display ) and a 'smart version' ( with grafical display ) and bu9457/8 addresses both versions.

     

    P.S. oddly enough rohm applications for bu9457/8 already knows of this strange use ( as an mp3 player for armchairs ), the image is from rohm site

     

    http://www.rohm.com/ad/usb_audio/images/pic_05.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 15 years ago in reply to davidefa
    That’s it! …this is second time that I have been suggested for President and I will go for it!
    Use of MP3 player in armchair is quite good idea.
     
    I like option where you do not need to put headphones on your head and yet music can be loud because speakers proximity to user head at the same time you not distract any body and yet not bother with headphones…just one touch of the button and relax… much more then armchair…not odd at all…
    Best Regards Alex