Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Have a question about ADCs or DACs? Ask our Expert, Nick Gray
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 118 replies
  • Subscribers 345 subscribers
  • Views 17419 views
  • Users 0 members are here
  • expert
  • nick_gray
  • power
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Have a question about ADCs or DACs? Ask our Expert, Nick Gray

ChristyZ
ChristyZ over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Communications in the element14 Community Wireless Communications Technology group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


Nick Gray

 

Nicholas Gray

Nicholas has worked in the Semiconductor industry for over 30 years and has authored a number of published articles about data converters (ADCs and DACs) and signal integrity issues.

 

  • Sign in to reply
  • Cancel

Top Replies

  • nickgray
    nickgray over 14 years ago in reply to e14 Contributor +1
    Hi, Ben, A couple of ADCs that should do well in your application with Hall Effect sensors are the ADS1146 and the ADS1255, both from Texas Instruments. I am sure that other suppliers probably have suitable…
  • nickgray
    nickgray over 14 years ago in reply to YT2095 +1
    The reason that you picked up radio signals when connecting a long wire antenna to the input is because the ADC had an input bandwidth that could pick up those signals. The sampling action of the ADC then…
Parents
  • YT2095
    YT2095 over 14 years ago

    Hi,

    I`m after an 8 bit A to D converter that will run up to a couple of MHz (but nothing past 4Mhz as it would be a waste).

    I`v already got the Audio A to Ds working well for my computer, but whilst experimenting with them to get it running smoothly, I couldn`t help but wonder what would happen if I attatched my Long-Wire antenna to the input, and surprisingly there Was radio of sorts present.

    needless to say that prompted a few ideas image

    my D to A is near infinate speed as it`s a homemade R2R, so that side is fine, but now I want something that`s a Single channel, 8 bit, really fast conversion time, A to D.

    the voltage rails aren`t a problem as I`v been forced to use a PC PSU for 5V current reasons, so have all the available +/- 12 and 5v stuff ready and waiting.

    I have a ZN425E-8 here, but feel certain there are likely to be Other chips out there that will out perform this, so to save me reading Tons of data sheets, does any particular chip spring to mind?

     

    Cheers image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • YT2095
    YT2095 over 14 years ago

    Hi,

    I`m after an 8 bit A to D converter that will run up to a couple of MHz (but nothing past 4Mhz as it would be a waste).

    I`v already got the Audio A to Ds working well for my computer, but whilst experimenting with them to get it running smoothly, I couldn`t help but wonder what would happen if I attatched my Long-Wire antenna to the input, and surprisingly there Was radio of sorts present.

    needless to say that prompted a few ideas image

    my D to A is near infinate speed as it`s a homemade R2R, so that side is fine, but now I want something that`s a Single channel, 8 bit, really fast conversion time, A to D.

    the voltage rails aren`t a problem as I`v been forced to use a PC PSU for 5V current reasons, so have all the available +/- 12 and 5v stuff ready and waiting.

    I have a ZN425E-8 here, but feel certain there are likely to be Other chips out there that will out perform this, so to save me reading Tons of data sheets, does any particular chip spring to mind?

     

    Cheers image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • nickgray
    nickgray over 14 years ago in reply to YT2095

    The reason that you picked up radio signals when connecting a long wire antenna to the input is because the ADC had an input bandwidth that could pick up those signals. The sampling action of the ADC then aliased the input signal, converting the RF signal to the audio band as the signal was digitized. You can “tune” in different stations by adjusting the ADC clock frequency. If the ADC input bandwidth is too high, you may sometimes pick up two adjacent radio stations at the same time, although one or both of them may be a little distorted.

     

    Most ADCs today have a serial output. This allows them to be in a much smaller package with fewer pins, reducing their cost. Because you have used the ZN425E8, I am assuming that you want the ease of use of a parallel output ADC and will not consider serial output devices.

     

    There seems to be a gap in ADC speeds between 1 Msps (megasamples per second) and 10 Msps, with not many products available in that range. However, all ADCs can operate a little faster than their specified maximum speed, but their performance may suffer if you try to operate them too much faster than their rated speed. On the other hand, high speed converters may not work well at very low speeds. The general solution to this type of problem is to use a high speed converter and just lot look at all the samples if you do not want data a high rates. For example, If you want data at 2 Msps and can not find a suitable converter at that speed, get a converter specified at 15 or 20 Msps, operate it at 16 Msps and look at every 8th output. This gives you a used data rate of 16 Msps / 8 = 2 Msps. Don’t consider the use of a super fast ADC as a waste. The prices of these things are about the same as slower devices. Here are some suggested ADCs The first is from Analog Devices, the others are from TI / National Semiconductor.

     

    AD7822, 2 Msps
    ADC1173CIMTC/NOPBADC1173CIMTC/NOPB, 15 Msps
    ADC1175, 20 Msps
    ADC08351, 42 Msps
    TLV5535, 35 Msps
    TLC5540, 40 Msps
    ADS830EADS830E, 60 Msps

     

    Nick Gray

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • YT2095
    YT2095 over 14 years ago in reply to nickgray

    That`s fantastic, Thanks!

    currently I`m using a Z80 at 8.192 MHz, but hope to upgrade to a 10 MHz version soon, so any even multiple of that would be great, and who knows, since the entire CPU card is replacable, using a Fast A to D would make it somewhat "Future proof".

    Cheers image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 14 years ago in reply to YT2095

    I am happy that I could help. My best to you.

     

    Nick Gray

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • YT2095
    YT2095 over 14 years ago in reply to nickgray

    just a quicky to let you know that I just bought 7x AD7822s`, all the others were SMD devices (Useless to me).

    they only cost £2 each from a fella in Israel.

    these should be sufficient for now as back-ups are always handy, and may even lead to some single use stand-alone devices later.

    Again, thank you for your help image

     

    edited to update: Scratch that, turns out the AD7822 were SMD devices also, so I canceled that and bought 4X ADC1175s` instead, I figure if I`m forced to go the SMD route I may as well have something I want and hopefully get a breakout bourd for it and solder it up without wrecking too many of them in the process.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 14 years ago in reply to YT2095

    You are most welcome. I am glad that I could help.image

     

    Nick Gray