Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Have a question about radio or wireless communication?  Ask me!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 84 replies
  • Subscribers 347 subscribers
  • Views 9786 views
  • Users 0 members are here
  • communications
  • pinter_electronics_consultants
  • expert
  • radio
  • wireless
  • chris_pinter
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Have a question about radio or wireless communication?  Ask me!

Chris_Pinter
Chris_Pinter over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Questionabout Communications in the element14 Community Wireless Communications Technology group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


image

 

Christopher Pinter

As the founder and President of Pinter Electronics Consultants Chris has been instrumental in developing the business from its inception in 2005 to its current status.  He has over 15 years of experience in radio and wireless communication hardware design and product development. Chris graduated from the Okanagan University with a diploma in Electronic Engineering Technology and the British Columbia Institute of Technology with a Bachelor of Technology in Electronics.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hi Chris,

     

    Want to create a wireless- remote control switch for a 115v winch motor that will function over 500 ft, obstructed line-of-sight. The motor is currently controlled by a DPDT momentary switch to engage forward and reverse. A 800 ft, 4-wires cable is currently used to connect power to the motor and switch to control the motor. I want to create a wireless switch control (Tx/Rx) units to untether the winch motor from the truck. A portable generator will be used to provide power directly to the winch and the wireless receiver. I want to use once channel for forward and separate channel for reverse. Reverse is accomplished by a relay within the winch motor.   I'm thinking of something in the 27Mhz  or 433Mhz band, around 1W to achieve this distance.

     

    I want to try and build this as a DIY project to learn about wireless controls.

     

    It seems simple in the idea, but struggling with where to start... Tx/Rx components needed, relays, etc.

    I have schematics for the motor wiring and the switch control box. Just want to replace the wire connecting them with a wireless connection.

    I can send them to you if that would help.

     

    Can you direct me some companies that can provide the components needed to build such a beast?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hi Chris,

     

    Want to create a wireless- remote control switch for a 115v winch motor that will function over 500 ft, obstructed line-of-sight. The motor is currently controlled by a DPDT momentary switch to engage forward and reverse. A 800 ft, 4-wires cable is currently used to connect power to the motor and switch to control the motor. I want to create a wireless switch control (Tx/Rx) units to untether the winch motor from the truck. A portable generator will be used to provide power directly to the winch and the wireless receiver. I want to use once channel for forward and separate channel for reverse. Reverse is accomplished by a relay within the winch motor.   I'm thinking of something in the 27Mhz  or 433Mhz band, around 1W to achieve this distance.

     

    I want to try and build this as a DIY project to learn about wireless controls.

     

    It seems simple in the idea, but struggling with where to start... Tx/Rx components needed, relays, etc.

    I have schematics for the motor wiring and the switch control box. Just want to replace the wire connecting them with a wireless connection.

    I can send them to you if that would help.

     

    Can you direct me some companies that can provide the components needed to build such a beast?