Does anyone know what kind of data does this Wifi module transmit?
http://www.microchip.com/wwwproducts/Devices.aspx?dDocName=en547511
Be sure to click 'more' and select 'suggest as answer'!
If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!
Does anyone know what kind of data does this Wifi module transmit?
http://www.microchip.com/wwwproducts/Devices.aspx?dDocName=en547511
Mr. Koh,
This module, plus a newer recommended one - the MRF24WB0MA - is an IEEE802.11 protocol compliant WI-FI device. However the data that you can send/receive is via the supported Serial Peripheral Interface Bus (SPI Bus). The data can be any digital data formatted and transmitted to/from the host microcontroller or processor. You can look up the SPI bus specifications, or get a quick look at http://en.wikipedia.org/wiki/Serial_Peripheral_Interface_Bus. Usually data is sent as 8 bits, but can be any organization since when the last bit (LSB) is sent, the controller stops toggling the clock on the SPI bus. Common data organizations are 8-bit (general data), 12-bit ot 14-bit for high quality voice data such as phone links, etc, or 16-bit to 24-bit for high quality audio (music) data. Tailor the data organization to your application need.
Good Luck,
Ken