Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Have a question about ADCs or DACs? Ask our Expert, Nick Gray
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 320 subscribers
  • Views 2600 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Have a question about ADCs or DACs? Ask our Expert, Nick Gray

bluescreen
bluescreen over 15 years ago

Don't forget to sign up for email notifications under the "Actions" box so you'll see when Nick answers your question.

 

image

 

Nicholas Gray

Nicholas has worked in the Semiconductor industry for over 30 years and has authored a number of published articles about data converters (ADCs and DACs) and signal integrity issues.

 

If not already, you'll need to

image or image

 


to ask your question.

Otherwise, click reply below.

  • Sign in to reply
  • Cancel
Parents
  • Catwell
    Catwell over 15 years ago

    Nicholas,

     

    I have been looking for an ADC for quite some time. Read here.

     

    Can you recommend some data acquisition systems that come with easy to use software? I don't want to spend a lof of time developing the backbone software or the GUI, so quick setup is key.

     

    Currently, my only option is the Picologger software and hardware. The software is fine, but it has a couple bugs and is complicated to use. However, the software is free, another deciding factor for me.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 15 years ago in reply to Catwell
    Hello, Cabe:

    It seems you are not looking for an ADC, but a complete data logging solution.

    The problem you are having finding the software you need is that every application is different and requires different software. It is not feasible for anyone to try to provide universal software that will work for every application, so manufacturers leave it to the user to provide his or her own software. Sometimes people contract this out to a software developer and there are many of those. If the system pointed out to you by Kris Demets seems to suit your needs, it may be quicker to wait for that system than to design, build, test and debug your own. Certainly being a Beta tester for Kris’ company, as you suggested, is a good idea, if they are open to it.

    The software that was pointed out to you that drives an LCD, which you can not use, could work if you modified the software to remove the LCD drive coding.

    Since the Picotech solution seems to be what you need, but with better software, you could try contact them and letting them know what bugs you found in the software and ask if there are any fixes or if revisions are planned to improve performance. You might find that they are working to fix the software. Go to the user forum as suggested by Kenny Millar. A more likely cause of the bugs is that a summer college intern who has little or no real software experience outside of school did the software and tested it in a single environment. He or she probably was never taught how to test everything in to coding and did not realize that some parts of the code were not tested. When he or she demonstrated it to the engineer mentoring him or her, the mentor did not think to enquire whether every part of the code was tested and what assurances were there that everything was properly tested. This is a common problem with work done by summer college interns as the person assigned to mentor the intern has his or her own job to do and is given the mentorship as extra work on top of what is normally required. A sad situation, but realistic in that this is what too often happens.

    It seems you have pretty much decided on using the PicoLog, but are not satisfied with the ease of use of the software. This makes me think that you may not be familiar with programming at all. If this is the case, I suggest contracting out software modification or development. I know of an excellent software guy in Roseville, California who almost definitely could do this, but I do not know if he has the time to do it as quickly as you need, or if he has the time to take on more work.

    I wish you every succes. Let me know if there is anything else I can do to help.

    - Nick Gray
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Catwell
    Catwell over 15 years ago in reply to nickgray

    Nicholas,

     

    Thank you for the advice. I am going to contact Picotech and see if they can correct the bugs.

     

    As for programming, I could do it, but I want to finish this project and get it to market quickly. Writing a GUI and backend would take longer than I want to spend. If you could connect me with your friend in California, I would greatly appreciate it.

     


    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 15 years ago in reply to Catwell
    Send me a private message with yout contact information and I will get you in touch with a programmer.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bnuthakki
    bnuthakki over 15 years ago in reply to nickgray

    Hello Nick,

    I have to monitor voltage of each battery in the battery stack of 150 lead acid batteries. Each battery have voltage range from 1.5V to 3V. Can you suggest me the best method.

     

    Balakrishna Nuthakki.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Catwell
    Catwell over 15 years ago in reply to nickgray

    Mr Gray,


    I contacted Picotech, and they said that the software, "Picolog," is at the end of its lifespan. Only critical patches will be applied. And apparently, my concerns are not that.


    So, my search continues, and I need to deliver my product ASAP.


    Can you suggest another product like Picolog?


    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 15 years ago in reply to Catwell

    I am sorry that Picotech will not support their software. Unfortunately, I know of no one who is doing something similar. Hopefully, you and Rob can work something out. I sent him your email address. He is quite busy, but might be able to help you if the task is not too large.

     

    - Nick Gray

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 15 years ago in reply to bnuthakki

    I am not really an expert in voltage monitoring, but I may still be able to help. What you do not indicate is just what level of monitoring do you need. Do you need to continually know the voltage level of each individual battery, or whether any battery in the stack is above or below a certain level.

     

    Monitoring each and every resistor is quite a task. The voltages of all but the one or two cells nearest ground will have to be divided down with a couple of resistors, then these voltages connected to an array of analog multiplexers before being presented to an ADC input. When cascading multiplexers, it is important to include a resistor to ground at the connection of the output of one multiplexer to the input of another multiplexer.

     

    If you only want to know if any voltage is above or below a certain level, the voltages will again have to be divided down, then use voltage comparators to determine if the voltages are above or below a threshold. You can use some OR gates after the comparators to present a single node to a processor or controller, perhaps to an interrupt pin. After an interrupt is generated, you could scan the entire array for the problem cell with a series of multiplexers.

     

    Any way you look at it, the circuit is going to be quite large if you must look at each cell separately.

     

    I do hope this helps. If not, please give me more detail as to what you are trying to do and I will try to help further.


    - Nick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • nickgray
    nickgray over 15 years ago in reply to bnuthakki

    I am not really an expert in voltage monitoring, but I may still be able to help. What you do not indicate is just what level of monitoring do you need. Do you need to continually know the voltage level of each individual battery, or whether any battery in the stack is above or below a certain level.

     

    Monitoring each and every resistor is quite a task. The voltages of all but the one or two cells nearest ground will have to be divided down with a couple of resistors, then these voltages connected to an array of analog multiplexers before being presented to an ADC input. When cascading multiplexers, it is important to include a resistor to ground at the connection of the output of one multiplexer to the input of another multiplexer.

     

    If you only want to know if any voltage is above or below a certain level, the voltages will again have to be divided down, then use voltage comparators to determine if the voltages are above or below a threshold. You can use some OR gates after the comparators to present a single node to a processor or controller, perhaps to an interrupt pin. After an interrupt is generated, you could scan the entire array for the problem cell with a series of multiplexers.

     

    Any way you look at it, the circuit is going to be quite large if you must look at each cell separately.

     

    I do hope this helps. If not, please give me more detail as to what you are trying to do and I will try to help further.


    - Nick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • bnuthakki
    bnuthakki over 15 years ago in reply to nickgray

    Dear Sir,

    Thanks for the reply. I would like to measure the voltage of each cell continuously. I have found some ICs like LTC6802 and equivalent but they only support for Lead acid. I have to now design new circuit for this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 15 years ago in reply to bnuthakki

    Hello, Balakrishna -

     

    I have studied the LTC6802-1 and the LTC6802-2 data sheets and find no reason to believe that these devices are only for lead acid batteries. There is mention of "primary cell" but the data sheet also says that the cell voltage can be anywhere between zero and 5V, with specified performance for cell voltages up to 4.2V. It seems to me that the LTC6802 is well-suited to your application. I called Linear Technology [ (408)432-1900 ] and was told that this device is just a battery monitor and does not care about the battery chemistry (type of battery) and their customers are using it for all types of batteries, including super caps. I would try to get some samples and try it out. the LTC6802-1 is for daisy chaining the SPI communications, requiring fewer I/O lines on a processor than the LTC6802-2, which uses individual SPI lines so are individually addressable. the LTC6802-1 is the more popular version.

     

    - Nick Gray