Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Looking for some help on picking a microcontroller.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 335 subscribers
  • Views 1669 views
  • Users 0 members are here
  • avr
  • microcontrollers
  • pic32
  • arduino
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Looking for some help on picking a microcontroller.

Former Member
Former Member over 10 years ago

So, I am working on a project that runs 100-120 LEDs in parallel. I would like to be able to use a little programming to add effects. For example, i would like to use pwm to make them fade on, when i power on the device. I tried doing this with an attiny85, but that maxes out at 40ma of current. so even a test string of 10 LEDs was way too dim. I need a microcontroller that is programmable and can handle 2 amps of current. I have an arduino uno and am familiar with a few different attiny chips. But, i'm not afraid to pickup a different development board. I'd also like the microcontroller to be able to comfortably fit inside of a round tube with an internal diameter of .75" to 1". all suggestions, or microcontrollers to read up on are welcomed.

Thanks, Derek

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 10 years ago in reply to artful_bodger +1
    Thank you. i actually had a 10 year old emachine running linux die the other day. it was a weak computer i used only for coding arduino. I actually planned on taking it apart for the psu today. I'll look…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    You need something like this to help with how to drive the LEDs

     

    Driving BIG loads with your micro controller - no isolation

    Drive BIG things with added safety. OPTO Isolators

    Sense BIG things with your Launchpad or Arduino, OPTO Isolated inputs.

     

     

    You can get cheep boost cnvertors that will up the voltage to a sufficient level to drive the led strings

     

    You say you dont have the room but as 10 strings of 10, you only needing to add 10 resistors

     

    If you want to control the LEDs individually or as groups then you will have to do something like this anyway or use NeoPixels (To use the Adafruit name for them) which are 5V multicolour (RGB) leds that are serially adddressable, you hook them all up in series for the power and one data line to the AT Tiny

     

    What supply are you using

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Robert Peter Oakes

    for prototyping i'm using the 5v line of an arduino uno. but i plan to use a 3.7 lipo battery in the final product. and all the LED's are soldered into one long string. they look kind of like a ladder. they are going into a tube just a little bit wider than the LED ladder. I could add 10 resistors. but there is no way to separate the LED string and make it look nice. I want one solid structure going up the tube. So i'm doing 1 chain of 100 LED's in parallel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • peterjcs23
    peterjcs23 over 10 years ago in reply to Former Member

    an interesting bit of product design, the circuit has to fit your requirement! Use an overrated insulated mosfet to switch with PWM and if the handle can be metal use it as the heat sink. Let us know how you get on!

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to Former Member

    100 LEDs in parallel is not a good plan ! You may get away with it but they will draw different currents and unless the wires are very thick the ones furthest from the supply will get less volts.

     

    In series you will need 400V (not ideal - part way to a real weapon ! - but possible for a one off).

     

    How about one really bright LED at one end and fibre optics or carefully sculpted light guides ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<