Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Power Supply for Home lab?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 136 replies
  • Subscribers 345 subscribers
  • Views 20568 views
  • Users 0 members are here
  • diy_power_supply
  • function_generator
  • power_supplies
  • diy
  • voltage/current
  • power_supply
  • power_meter
  • variable_power_supply
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Power Supply for Home lab?

mudz
mudz over 10 years ago

Hi,
I am starting this year with different projects. Indeed, I need a power supply which I felt for so long is the main missing component in my small home lab. Currently, I am using PC SMPS, Transformers, and different adaptors to power up different projects and kits.
Many times I felt need of a variable power source but I did that with two different power supplies, but it is time consuming. And many more things to say but its just a waste of time to write and for yourself to read...... Now Its too much and I'm going to build one good power supply. Previously I'm fulfilling my power supply needs by using a adaptor and then using a voltage regulator(7805, 7809, 7812, LM317..) afterward for my projects.
So, what do you suggest?

Also I'm going to include few more additions to it like function generator, power consumption meter.
So what do you suggest what will be the best thing to make a good power supply?

An IC?

A Microcontroller? like PIC

Just build a box consisting a transformer/adaptor with voltage regulator and few pots?

Do tell me which will be better to use? A microcontroller or IC available in market for specific task for example Function generator IC? I'm confused should I go with a microcontroller and make my own program to do these tasks or should I buy an IC for individual task and then using a controller to control all?

 

 

mudz

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    I know this is self promoting but I am in the middle of a set of tutorials on building a LAB / Bench power supply and accessories I start with the basic building blocks, explaining in practical terms what…
  • michaelkellett
    michaelkellett over 10 years ago +2
    There is no best - it depends what you are doing - I have loads of different power supplies (it's my work not just a hobby so they can be paid for if needed.) My favorite general purpose supply is a rather…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to mudz +2
    I would suggest starting with a basic naalog design (As I have shown in my series), understand its operation, then it should be a simple extension to add DAC and ADC monitoring this way it seperates the…
Parents
  • dougw
    dougw over 10 years ago

    This supply by JSPAYNE seems to be pretty capable without getting too complex:

    Variable Voltage, Variable Current Power Supply

    The main challenges would be to get an appropriate transformer and big enough heat sinks.

    I would add a couple of low cost modules to display current and voltage.

    Just look for "3 wire voltmeter" on your favourite shopping source.

     

    Doug

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to dougw

    Basic RAW power could be from even a re-purposed Laptop power supply, easy to use, safe to use and typically upto or in excess of 20V at several amps

     

    I agree that the heat sink will be the issue, or atleast the limiting factor, if your outputting 1V at 5A and your raw power is 35V then your output stage will have to be dissipating 170W or so, thats alot of heat

     

    there are online heatsink calculators that may help, you will need to read a few data sheets though to get the required parameters :-  here is an example   http://mustcalculate.com/electronics/heatsink.php

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to dougw

    Basic RAW power could be from even a re-purposed Laptop power supply, easy to use, safe to use and typically upto or in excess of 20V at several amps

     

    I agree that the heat sink will be the issue, or atleast the limiting factor, if your outputting 1V at 5A and your raw power is 35V then your output stage will have to be dissipating 170W or so, thats alot of heat

     

    there are online heatsink calculators that may help, you will need to read a few data sheets though to get the required parameters :-  here is an example   http://mustcalculate.com/electronics/heatsink.php