Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Power Supply for Home lab?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 136 replies
  • Subscribers 345 subscribers
  • Views 20713 views
  • Users 0 members are here
  • diy_power_supply
  • function_generator
  • power_supplies
  • diy
  • voltage/current
  • power_supply
  • power_meter
  • variable_power_supply
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Power Supply for Home lab?

mudz
mudz over 10 years ago

Hi,
I am starting this year with different projects. Indeed, I need a power supply which I felt for so long is the main missing component in my small home lab. Currently, I am using PC SMPS, Transformers, and different adaptors to power up different projects and kits.
Many times I felt need of a variable power source but I did that with two different power supplies, but it is time consuming. And many more things to say but its just a waste of time to write and for yourself to read...... Now Its too much and I'm going to build one good power supply. Previously I'm fulfilling my power supply needs by using a adaptor and then using a voltage regulator(7805, 7809, 7812, LM317..) afterward for my projects.
So, what do you suggest?

Also I'm going to include few more additions to it like function generator, power consumption meter.
So what do you suggest what will be the best thing to make a good power supply?

An IC?

A Microcontroller? like PIC

Just build a box consisting a transformer/adaptor with voltage regulator and few pots?

Do tell me which will be better to use? A microcontroller or IC available in market for specific task for example Function generator IC? I'm confused should I go with a microcontroller and make my own program to do these tasks or should I buy an IC for individual task and then using a controller to control all?

 

 

mudz

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    I know this is self promoting but I am in the middle of a set of tutorials on building a LAB / Bench power supply and accessories I start with the basic building blocks, explaining in practical terms what…
  • michaelkellett
    michaelkellett over 10 years ago +2
    There is no best - it depends what you are doing - I have loads of different power supplies (it's my work not just a hobby so they can be paid for if needed.) My favorite general purpose supply is a rather…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to mudz +2
    I would suggest starting with a basic naalog design (As I have shown in my series), understand its operation, then it should be a simple extension to add DAC and ADC monitoring this way it seperates the…
Parents
  • jonivanart
    jonivanart over 10 years ago

    This may have been mentioned and it may not be what your trying to accomplish as an end result but... The current project I am working on 1870's Programmable Clock Project... requires 3 power sources 24v, 12v, and 5v DC. I simply found some laptop power supplies. One had the 12 and 5 v and the other 24v. They have the built in regulators and have a great amperage rating for most all electronics projects. I'm basically wiring the 120vac wires together to the power supply chord to power them all up at the same time. You could do this in a project box, wire the grounds together and create an external ground post along with the 3 different posts for the 3 different power sources. I'm thinking about building one and also adding a step up transformer to also include 120vac and 240vac for powering vacuum or Nixie tubes. ;-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 10 years ago in reply to jonivanart

    Your project looks fantastic.

    Are you using harmonically related cables? The seem to be striking a power chord!

    You should be able to derive the Nixie voltage quite easily from the AC not dissimilarly to how many CFLs operate from light sockets.

    In the land of Oz I think it was 360VDC.

     

    Just make sure you keep all of the wiring safe!

     

    SAFETY FIRST!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • COMPACT
    COMPACT over 10 years ago in reply to jonivanart

    Your project looks fantastic.

    Are you using harmonically related cables? The seem to be striking a power chord!

    You should be able to derive the Nixie voltage quite easily from the AC not dissimilarly to how many CFLs operate from light sockets.

    In the land of Oz I think it was 360VDC.

     

    Just make sure you keep all of the wiring safe!

     

    SAFETY FIRST!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to COMPACT

    To Dab:

    DAB wrote>>...

    my idea that there are no electron particles and that the electron cloud around all atoms is a collection of captured photons...

    ...I am very confident that my use of a single elemental particle and two well known and documented forces can account for everything in the universe...

    ELY Reply>>No electrons? just captured photons? Are these captured photons captured RANDOMLY? Or part of some design or plan? Please name the two forces that you believe are at work here

    To Peter Oakes :

    WRT "Intro to Power Electronics" MOOC, are in? or are you out?

    Same to Compact:

    are in? or are you out?

    -USCDADNYC

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jonivanart
    jonivanart over 10 years ago in reply to COMPACT

    Thanks for the compliment!

    In this project the vacuum tubes will simply be illuminated by LED'S so no high voltage requirements here. ;-) But I will be doing some work with Nixie's in the following project. I believe they are 360VDC. I already have the transformers for that. I have found vacuum tubes that operate on 240 and 120VAC also. I will be using some of the 120VAC ones in this project with the LED's. I think there was a progression in that era to eliminate the extra transformer by creating 120VAC tubes and get away from 240VAC ones. Not exactly sure on that research yet tho. I love the history I'm learning through these projects...