Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Power Supply for Home lab?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 136 replies
  • Subscribers 345 subscribers
  • Views 20946 views
  • Users 0 members are here
  • diy_power_supply
  • function_generator
  • power_supplies
  • diy
  • voltage/current
  • power_supply
  • power_meter
  • variable_power_supply
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Power Supply for Home lab?

mudz
mudz over 10 years ago

Hi,
I am starting this year with different projects. Indeed, I need a power supply which I felt for so long is the main missing component in my small home lab. Currently, I am using PC SMPS, Transformers, and different adaptors to power up different projects and kits.
Many times I felt need of a variable power source but I did that with two different power supplies, but it is time consuming. And many more things to say but its just a waste of time to write and for yourself to read...... Now Its too much and I'm going to build one good power supply. Previously I'm fulfilling my power supply needs by using a adaptor and then using a voltage regulator(7805, 7809, 7812, LM317..) afterward for my projects.
So, what do you suggest?

Also I'm going to include few more additions to it like function generator, power consumption meter.
So what do you suggest what will be the best thing to make a good power supply?

An IC?

A Microcontroller? like PIC

Just build a box consisting a transformer/adaptor with voltage regulator and few pots?

Do tell me which will be better to use? A microcontroller or IC available in market for specific task for example Function generator IC? I'm confused should I go with a microcontroller and make my own program to do these tasks or should I buy an IC for individual task and then using a controller to control all?

 

 

mudz

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    I know this is self promoting but I am in the middle of a set of tutorials on building a LAB / Bench power supply and accessories I start with the basic building blocks, explaining in practical terms what…
  • michaelkellett
    michaelkellett over 10 years ago +2
    There is no best - it depends what you are doing - I have loads of different power supplies (it's my work not just a hobby so they can be paid for if needed.) My favorite general purpose supply is a rather…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to mudz +2
    I would suggest starting with a basic naalog design (As I have shown in my series), understand its operation, then it should be a simple extension to add DAC and ADC monitoring this way it seperates the…
Parents
  • COMPACT
    COMPACT over 10 years ago

    I've designed and built many power supplies in my lifetime and if you want something simple that's premade then e14 has reasonably priced adjustable and programmable power supplies.

    The Tenma  72-253572-2535 is a good start with both Constant Voltage and Constant Current modes

    With both modes available it is very easy to use it to test LEDs.

     

    Another handy tool to have is an accompanying DC load unit as this will enable you to properly test power supplies and batteries)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 10 years ago in reply to COMPACT


    LOOkatu .. I'm going to build it myself.. MAKE IT MYSELF.. image
    Thanks COMPACTimage

     

    mudz

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 10 years ago in reply to michaelkellett

    Hey michaelkellett
    Thanks for the heads up.. This is what I was really looking for an Experience, I'm definitely not going with the old age things. I know those are masterpiece of their time and some are still believed to be still in phase but I am going to make an advanced version of that. I might fail over few things but hey I'm building this up for the most important thing "Experience" then comes my power supply requirements.
    Well I'm still figuring out what will be the best to build with.. I will come up with a solution within this week..
    I can get my hands on those op ams.. bdw I have never worked on OP ams before.. So I am considering it straight away. image
    Thanks a lot !

     

    mudz

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to mudz

    Nothing like jumping in at the deep end !

     

    I can't post the complete design for the tester I mentioned  but it has a pair of interesting power supplies (tracking, +/- 0-12V, with current limiting) and I 'll post an extract showing that part of the design in a few days.

     

    It uses OPA192s.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 10 years ago in reply to michaelkellett

    Looking forward to it..
    Thanks!

     

    mudz

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to michaelkellett

    My comments here is Not to be taken as Legal Advice. It is just an Simplified Overview of the US Patent Process as recently modified by the 2011 AIA (America Invents Act)  NOT ACA (ObamaCare). AAR. Do post your designs if you do not believe they are Patentable. If you believe the Designs are Patentable (over the Prior Art) then keep them secret and seek further Legal Advice for Patent Protection. By posting your (possibly Unpatentable) designs, you are contributing to the Prior Art.

    To which other people's designs will be judged against. i.e. they will not be able to Patent what you designed. In "closely similar" inventions (designs) your Prior Art will help to exclude any later Designer from "exclusively benefiting' from your design (b/c your design is now Prior Art)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to uscdadnyc

    Dear Edward - thanks for your comment.

     

    My own, admittedly unusual, opinion is that patents are a bad thing for society in general and that they usually benefit those with power and resources at the expense of everyone else. Sometimes my customers insist on patenting stuff -  I can't stop them !

     

    I am always delighted to put my own tiny spanners into other peoples patenting works - and in this case it might even have the spin off effect of being helpful to someone as well.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 10 years ago in reply to michaelkellett

    Great looking op-amps Michael - they also have pretty good output drive current capability.

    Doug

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to michaelkellett

    Hi Michael,

     

    I'm new to this blog, but I've been in engineering for many years, mostly test equipment and microwave communication equipment. Microwaves requires lots of good analog and digital control so I've done a lot of that too. My interest in your blog on a lab power supply fits into my latest project that I thought you might find interesting. That is to create a platform of control, display, packaging, cooling, and power management that would allow engineers to build specialized equipment that they would need for whatever their specialty was. Examples of what I know everyone needs is of course, lab power supplies, so this would be my first product. Next would be a programmable load, several varieties of microwave frequency synthesizers, microwave power detectors, block converters for extending the range of radios, and spectrum analyzers. Because you have a lab power supply designed, it seemed to me that you might be interested in participation in creating a product on this platform that would be remotely controlled, have a display of the voltage and current, a single knob control that would allow setting the output very precisely and stepping or scanning over a predetermined range with variable size steps. I am well on the way of completing the housing, control, display, etc.

     

    These would have a standard interface so that they could easily be integrated into an automated test system.

     

    I strongly believe that in order to sell test equipment one needs to be able to provide many different solutions in a multitude of areas so that a catalog would be extensive, and one would go to it for a solution of whatever their problem is. Hewlett Packard used to do this when Dave and Bill were around, but the new company has moved into bigger and more complex systems meant for volume manufacturers. (For example, a top of the line spectrum analyzer and now run several hundred thousand dollars.) They have also split off various companies that Dave Packard spent his lifetime collecting. I want to provide an alternative for consultants and engineers that have small labs and smaller budgets, In order to quickly generate a multitude of test equipment many different engineering talents would be required, so I plan to make the platform open source with standard interface so that engineers could easily create what they needed, but not have to worry about all the details of making a salable product, and marketing it. My role in this is to create the system for this to happen, define interfaces, create the market, and communicate with the participants.

     

    Would you have an interest in participating in this?

     

    Fred Storke

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 10 years ago in reply to e14 Contributor

    Hi Fred,

     

    What is your opinion of the Red Pitaya?

     

    Compact

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to COMPACT

    My 2c worth... its awsome, I have one and am currently performing a review of it

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 10 years ago in reply to Robert Peter Oakes

    It seems a bit too expensive to me.

    Does it have an electrically isolated USB connection to its host PC?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • COMPACT
    COMPACT over 10 years ago in reply to Robert Peter Oakes

    It seems a bit too expensive to me.

    Does it have an electrically isolated USB connection to its host PC?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to COMPACT

    you connect mainly  through ethernet to the host, all the apps are web based so in that regard it is isolated due to the transformer in the ethernet physical layer connector circuit

     

    there are a couple of USB ports too but they are not isolated and not normally used for the apps like Scope, Spectrum and LCR

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to Robert Peter Oakes

    Thx for the pre-evaluation of the Red Pitaya. It looks Great. I have a few Simply Q's if you can indulge me:

    Q1; For 3X the price of a BitScope, this provides more than 3X the Options/ Capability(es) . Do you agree?

    Q2. The Red Pitaya is Linux-based, while the User Interface is Web-Based, so the "Controlling-function-(virtual)-Knobs/Display" can be on (let's say) a Windows PC/Laptop?

    Q3. The uSD Card on the Red Pitaya (RedP) Determines the Functionality of the RedP, much like the uSD card in a RaspPi? Debian O/S  for a RaspP PC. Minibian for a RaspPi Controller (using GPIO Pins)

    Q4. Is the RedP available in the USA? Somebody said "470" Dollars?

    Q5. Is the USB Port on the RedP a USB-"B"  Female Receptacle? Another words in original USB parlance: PC/Laptop = Computer;; RedP = Device.

     

    Thx.

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to uscdadnyc

    To Peter Oakes:

    Updated Q5: Saw a few youtube videos on the Red Pitaya (Acronym "RedP" OK?. What acronym does the community use?). Saw that the Full-Size USB Connector(on RedP)  is a Full Size Female Receptacle -A..

    Q5A. This being the case, Maybe? IF you connect both PC/Laptop to a USB Hub then you can use (2) Male-Female USB-A Cables? Possible to do it this way?

    Q5B: What about a Full Size -A Male-to-Male Cable, connecting PC/Laptop to RedP? BUT don't you need to cross-over D+ and D-? {Analogous to RJ-45 Cross-over when you are going device-to-device. In the YouTube video By Elektor.tv "Red Pitaya: One Instrument to Replace Them All" the presenter (Speaker) said "...change  Adapter Settings..."

    What? in a PC/Laptop? Don't you need a X-over? IDK (I Don't Know) of ANY PC/Laptop that allows an changing of wires. Do you know what the story is.?

    Q6: Did you buy a Bare-Bones RedP or an RedP Development Kit?

    Q7; Are You USA or Abroad? Did you buy local (to me: USA) or Foreign?

    Q8: Do you think www.element14.com  might sell this RedP?

     

    Thx

    uscdadnyc (ny ny usa)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to uscdadnyc

    To Peter Oakes:

    IDK I was blogging w/ a YouTube Star (you, Peter Oakes). AAR I am looking forward to your Youtube (follow-up) videos mentioned in your DEC 2015 "What's new". My previous Q5B is still Open. I know it was Not your video (it was elektor.com) but you are the Man! Thx.

    I still have my old Textronix Oscilloscope Probes (X10, I remember), So Q9: I don't need the RedP Development Kit b/c the Kit comes w/ Probes? (which I already have). And the S/W load is analogous to getting RaspPi S/W, Correct?

    Q10: I think I can run the RedP off my Android (Cyanogen Mod 11) rooted B&N Nook HD+ (via WiFi). But I guess it is time to spring for a new Laptop/Tablet. What types of options should I look for in a Laptop/Tablet? Options that are desirable when communicating/logging Data from the RedP?( a) SSD/HDD?, but the RedP has SATA connections(?)? (b) Optical Drive?, but Optical Drives have all but Vanished from Portables these Days. (c) USB ports ?(USB 3.0, most desirable) and lots of them.

    BTW I recently bought a Student Edition of MatLab w/ simulink, and I believe there is C/C++ support (linkages) to/from RedP.? As there exists between MatLab and RaspPi.

    Thx Again

    -USCDADNYC

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to uscdadnyc

    To Michael Kellett:

    Pls elaborate on your comment below:

    --------

    Created 2 years ago by michaelkellett in Open Source Hardware

    The issues in making  a decent oscilloscope go way beyond a micro. The Red Pitaya thing is an attempt at this but compared with a real scope it's just a joke. First you need the front end, input impedance 1M, variable (switcahble) gain from perhaps 100 to 0.01 in 1,2,5 steps with a flat frequency

    ______

    Was this comment about the (current [timestamp 07FEB16]) Red Pitaya? Or was there a previous Incarnation? I appreciate that a low Impedance on Part of the measuring Instrument WILL affect the Readings (Think Heisenburg's Uncertainty Principle). But at a bandwidth of just 50MHz, are the implications that onerous? Sorry,

    I did not do the Math yet.

    BTW what about Bitscope? Same low Input Impedence?

    -USCDADNYC (NY NY USA)

    0 1 464

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to uscdadnyc

    I was going to keep out of the RedP aspects of this thread but now that I've been asked ........

     

    The RedP is an interesting attempt at a low cost instrument based on the Xilinx Zynq chip. It was massively over-hyped on it's launch with claims that it could replace instruments costing 10s of k$. The current web site is a bit more restrained  but still sadly lacking in detailed specs.

    To take the inputs : a real scope has a wide bandwidth amplifier and either a switch or other means of selecting a wide range of gains so that the sensitivity can be set between a few mV per vertical division to perhaps 20V. As you pay more the ranges extend a bit and the precision and bandwidth improve. The other key feature they offer is some kind of DC offset control before the ADC - this is really useful. The RedP offers 20V or 1V, jumper selectable, and I'm not sure if its 1M impedance on both ranges. This will be so inconvenient that you will very quickly get totally fed up with it and either try to build an input amplifier/attenuator (which is very difficult) or give up and buy a real scope.

     

    The RedP samples at  14 bits at 125MHz -  this is very slow - the cheapest Rigol samples 8 bits at 1GHz which is a much better compromise for a general purpose scope.

    Try comparing the published data sheets of Pico, Rigol, Kesysight, Tektronix and LeCroy scopes with the RedP data - it's quite instructive - worry about the bits that don't get mentioned (and assume the worst).

    The closest almost real scope to the RedP would be one of the Pico offerings (they do have proper switching ranges and input amps).

     

    Remember that for useful work you need to be sampling at 10x the working frequency, so the RedP is good for up 12.5MHz.

    I don't know anything in detail about the Bitscope - it's pretty cheap but I wouldn't want have to use one.

     

    My advice is always to buy a real scope - if you can't afford  a new one then buy a second hand one.

     

    I practice what I preach - my main scope cost more than my car - but I couldn't do my work without it.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to michaelkellett

    To MK,

    Thx for your Candid Assessment on the RedP as opposed to Real Oscilloscope(s). Truth be told I am somewhat of Techie (having a BSEE from 1973) but I am looking for a "overview" Product. Not to get into the Nitty-Gritty of Designing/Testing, but some product that has the Basic Functions that show (maybe in a Limited way) Electronic Instrumentation. An Analog in Chemistry would be "Qualitative Analysis" Rather than "Quantitative Analysis". I am a USPTO Registered Patent Attorney, so my interest in what is available at any given Time/Place will (hopefully) constitute Prior Art. You have given me info about specs & capabilities that Must be considered (taken into account) when I evaluate the RedP to my (uncertain) Needs. Thx Again.

    BTW I do have an actual CRT Oscilloscope. It is a Sony/Tektronix Dual Channel "Portable", circa early 1980's. It is under 30 years of Dust.

     

    -USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to uscdadnyc

    Red Pitaya's main user interface is via the Ethernet port and is presented as a set of WEB pages, not X Windows or anything.

    It does have SSH etc available to it and can have additional apps installed / compiled on it

     

    Most of the Pitays analogue/signal processing functionality is handled by the FPGA, this is how it gets its great speed in processing of the inputs and outputs, the price of this is it runs very hot (Over 60deg C)

     

    Right now, the Pitaya has the following main apps available (Some have multiple options and some you have to pay an additional fee for so it may not be as cheap as it appears

     

    2 Channel Scope with the limitations michaelkellett has mentioned ( IE, 12Mhz ish true bandwidth assuming a 10X sample rate)

    2 Channel Spectrum Analyzer

    2 Channel Signal generator / Arbitary Waveform Generator upto the 125Mhz sample rate again but limited to less than a volt output (TBC)

    LCR/reactance meter

    Software defined Radio (New and I have not tested this yet)

     

    you can run the ARB and Scope at the same time as there available in the same app, you cant run more than one app at a time on the main WEB pages due to locking of the IO devices like ADC etc I guess

     

    The ADC and DACs are 14bits which is way better than most scopes these days (There all typically 8 bit), one benefit of this is that you get extra resolution out of a range compared to a reg digital 8 bit scope so this can in a limited fashon make up for no sub 1V range for instance as at 1V there is a 1/16384 V resolution... 61uV, this is way better than most scopes and is close to comparable with a 10 - 15mV range on a scope (15mV range would equate to a resolution of 61uV too) so perhaps to be fare we would round that up to a 20mV range. The point here is that any 8bit scope is not that accurate as it only resolves to 256 levels of a signal, scopes are primararly used to Look at the signal and get an idea of what it is doing

     

    If your going to always or mostly be looking at logic level type signals or atleast limited to low voltages then 20V is not too bad but this is the base range, add a 10X probe and guess what, thats 200V. The input t the Pitaya is 1Mohm as mike sait which makes it ideal for adding a 10X probe if needed

     

    Other features are DUAL SATA ports, a full set of GPIO so you could use it as a logic analyzer or control, Matlab / LabView capability, Scratch pogramming, and you could add your own custom apps too if needed, with our without leveraging the FPGA

     

    Ill have more once I have done the review but thatshould help fo now

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to Robert Peter Oakes

    Oh, forgot to mention, Mine came from RS-Components for me to review so I did not have to buy it.  but you can get from Mouser, Direct from RedPitaya, from Eletor and a few other places. Oh and of course RS-Components. I did not find it on Newark though... sorry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to uscdadnyc

    WRT to my Q5 and collateral Q5A,5B, etc. I think I have an answer to my own Q's

    The Wiki on Red Pitaya has a table of Ports, (partial listing here)

    "

    EthernetFull-duplexRJ451000Base-T Ethernet connection

    USBFull-duplexA USB Used for standard USB devices

    Micro USB (Console)Full-duplexMicro B USB Used for console connection

    Micro USB (Power)InputMicro B USB 5 V / 2 A power supply

    Micro SDFull-duplexMicro SD slot Micro SD memory card                         "

     

    The "Micro USB (Console)Full-duplexMicro B USB Used for console connection" is the One USB

    port to use (for a wired connection from PC/Laptop to RedP) No settings to change OR Cross-over

    needed. Just a Male-full-size A -to- Male-micro-size B Cable.

     

    Sorry about the confusion

     

    USCDADNYC (NY NY USA)