Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Power Supply for Home lab?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 136 replies
  • Subscribers 345 subscribers
  • Views 20961 views
  • Users 0 members are here
  • diy_power_supply
  • function_generator
  • power_supplies
  • diy
  • voltage/current
  • power_supply
  • power_meter
  • variable_power_supply
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Power Supply for Home lab?

mudz
mudz over 10 years ago

Hi,
I am starting this year with different projects. Indeed, I need a power supply which I felt for so long is the main missing component in my small home lab. Currently, I am using PC SMPS, Transformers, and different adaptors to power up different projects and kits.
Many times I felt need of a variable power source but I did that with two different power supplies, but it is time consuming. And many more things to say but its just a waste of time to write and for yourself to read...... Now Its too much and I'm going to build one good power supply. Previously I'm fulfilling my power supply needs by using a adaptor and then using a voltage regulator(7805, 7809, 7812, LM317..) afterward for my projects.
So, what do you suggest?

Also I'm going to include few more additions to it like function generator, power consumption meter.
So what do you suggest what will be the best thing to make a good power supply?

An IC?

A Microcontroller? like PIC

Just build a box consisting a transformer/adaptor with voltage regulator and few pots?

Do tell me which will be better to use? A microcontroller or IC available in market for specific task for example Function generator IC? I'm confused should I go with a microcontroller and make my own program to do these tasks or should I buy an IC for individual task and then using a controller to control all?

 

 

mudz

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    I know this is self promoting but I am in the middle of a set of tutorials on building a LAB / Bench power supply and accessories I start with the basic building blocks, explaining in practical terms what…
  • michaelkellett
    michaelkellett over 10 years ago +2
    There is no best - it depends what you are doing - I have loads of different power supplies (it's my work not just a hobby so they can be paid for if needed.) My favorite general purpose supply is a rather…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to mudz +2
    I would suggest starting with a basic naalog design (As I have shown in my series), understand its operation, then it should be a simple extension to add DAC and ADC monitoring this way it seperates the…
Parents
  • COMPACT
    COMPACT over 10 years ago

    I've designed and built many power supplies in my lifetime and if you want something simple that's premade then e14 has reasonably priced adjustable and programmable power supplies.

    The Tenma  72-253572-2535 is a good start with both Constant Voltage and Constant Current modes

    With both modes available it is very easy to use it to test LEDs.

     

    Another handy tool to have is an accompanying DC load unit as this will enable you to properly test power supplies and batteries)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 10 years ago in reply to COMPACT


    LOOkatu .. I'm going to build it myself.. MAKE IT MYSELF.. image
    Thanks COMPACTimage

     

    mudz

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to uscdadnyc

    WRT to my Q5 and collateral Q5A,5B, etc. I think I have an answer to my own Q's

    The Wiki on Red Pitaya has a table of Ports, (partial listing here)

    "

    EthernetFull-duplexRJ451000Base-T Ethernet connection

    USBFull-duplexA USB Used for standard USB devices

    Micro USB (Console)Full-duplexMicro B USB Used for console connection

    Micro USB (Power)InputMicro B USB 5 V / 2 A power supply

    Micro SDFull-duplexMicro SD slot Micro SD memory card                         "

     

    The "Micro USB (Console)Full-duplexMicro B USB Used for console connection" is the One USB

    port to use (for a wired connection from PC/Laptop to RedP) No settings to change OR Cross-over

    needed. Just a Male-full-size A -to- Male-micro-size B Cable.

     

    Sorry about the confusion

     

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 10 years ago in reply to uscdadnyc

    Hi Edward,

     

    Many thanks for you wealth of information.

    As you are a registered Patent Attorney are you able to give our members some guidance of the Patent process?

    I think it would be very much appreciated.

     

    Compact

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to Robert Peter Oakes

    Kudos to Both PO & MK. You guys are the BEST. You guys cut down to the Chase w/o hyperbole. W/ the info gotten from you two, I can get a PhD in Oscilloscope (and wannabe's) Technology.

    To PO:

    PO wrote>>... [RedP has ]a full set of GPIO so you could use it as a logic analyzer or control...

    ELY reply>> You just brought to Memory Lane again. In the 1970's, I had built a "Kit" Logic Analyzer. It was Only  8 bits.

     

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to COMPACT

    WRT Patent Advice, it will be just General Outline(s) of the Patenting Process. Like they say on TV, paraphrasing, " I am a patent Atty, BUT do Not play one on this Blog."

    However, I would have to know what Legal Jurisdiction(s) [Nation] you guys are in? Luckily the Patent Laws of the US were just harmonized w/ European/English-Speaking Countries, via the USA AIA (America Invents Act) of 2011. Luckily, we are Not talking Drug Patents or Patent Law in (say) India or China. WRT I can only say WTF?

     

    uscdadnyc (ny ny usa)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 10 years ago in reply to uscdadnyc

    Compact's in Australia.

    In addition to a standard patent we have a local thing called an Innovation Patent that lasts a maximum of 8 years.

    These patents are supposedly granted without examination however these patents are only legally enforceable after examination and certification. (As you said WTF?)

    We've also got an alternative process called Provisional Application which is designed supposedly to allow the applicant up to 12 months to get the Patent application lodged.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to COMPACT

    Compact wrote>>...

    We've also got an alternative process called Provisional Application which is designed supposedly to allow the applicant up to 12 months to get the Patent application lodged.

    ELY Reply>> Same as in the U.S. Being such, I assume that the (required) Specification [detail description of the invention] will support the "Claims" later drafted w/i 12 months, in order to turn the Provisional into a Regular Australian Patent Application. Like the famous WWII US General MacArthur said "the Corps. The Corps. The Corps,

    so it is in Patent Law, "The Claims. The Claims. The Claims.".

    Compact wrote>>...

    In addition to a standard patent we have a local thing called an Innovation Patent that lasts a maximum of 8 years.

    These patents are supposedly granted without examination however these patents are only legally enforceable after examination and certification. (As you said WTF?)

    ELY Reply>> Interesting this "Innovation Patent(s)", I suppose it is the Australian Patent Office attempt to spur the pace of Innovation. I guess the holder of an Innovation Patent Application, can use it as a Sword under the rubric of: "Patent Pending". Another words, any possible Infringers are on Notice as of the date of filing of the Innovation Patent Application. And Damage can start from that point in Time.

    Thx for the Input. Like I said b/f , it is always interesting to converse w/ you

     

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to uscdadnyc

    To ALL:

    We all get product placement Ads (if we allow Cookies. And I do). One product intrigues me. It is a SMPS by Tenma # 72-9470, 13.8Vdc. Why 13.8Vdc? What is so special about 13.8Volts.? I know I am not very current (no pun intended) on Pwr Supplies, but can somebody help me here?

    Good Thing I am not Superstitious, but the Tenma Part # has the elements of my Street Address. Weird, You can't make these things up.

     

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to uscdadnyc

    It's an old-school thing, an anachronism. Due to the chemistry of lead acid batteries, they are conveniently chargeable at around 13.8V for a 12V nominal lead acid battery. So old school chargers were literally just a resistor and a 13.8V supply. Today trickle charging can still just be done with a (higher value) resistor, but back in time the accepted approach for normal charging was to use a 13.8V supply. Nowadays this would not be done, there are constant voltage and constant current phases that are observed, and they vary for different battery chemistries.

    But in earlier times that would have been expensive to implement.

     

    So, a lot of radio gear (radio being nearly synonymous with all electronics hobbyist activity) at that time could handle 13.8V. The supplies are still made, and any 12V automotive electronics will be able to run off that supply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to shabaz

    Way back when we had systems out in the country, they used Lead Acid batteries, and 13.8v was the 'desired' voltage to recharge them.

    The comment was something along the lines of recharging at the fastest rate without causing undue stress ....

     

    The trouble was many of these systems stayed at near full capacity, so all the 13.8v did was boil off the electolyte and the battery would be dry everytime we checked it.

     

    We reduced the voltage to 13.4v and never had an issue or dry battery.

    I've always used 13.4v every since.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to mcb1

    For those who did NOT sign-up for the first (of 5) courses In "Intro to Power Electronics" hosted at www.coursera.org. Professors are from Univ of Colorado [USA], the course is pretty Good. They even give you a Link to get a copy of "Ltspice". IDK how fully functional is this copy is, but it is worth getting Nevertheless. For my professional needs this Ltspice and my Paid Student Copy of MatLab/Simulink are more than adequate to give me a handle on current technology in electronics. I am always looking out for what will possibly become Prior Art.

     

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to mcb1

    For those who did NOT sign-up for the first (of 5) courses In "Intro to Power Electronics" hosted at www.coursera.org. Professors are from Univ of Colorado [USA], the course is pretty Good. They even give you a Link to get a copy of "Ltspice". IDK how fully functional is this copy is, but it is worth getting Nevertheless. For my professional needs this Ltspice and my Paid Student Copy of MatLab/Simulink are more than adequate to give me a handle on current technology in electronics. I am always looking out for what will possibly become Prior Art.

     

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 10 years ago in reply to uscdadnyc

    LT Spice is free to anyone - if you get  chance then go to one of the Linear Technology lectures about it, delivered by Mike Engelhardt, I went to one in Edinburgh (part of the 2014 LTspice World Circuit ) and it was one of the best lectures of its kind I've ever attended.

     

    Sorry about the random font changes - blame the E14 editor !!

     

    MK

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 10 years ago in reply to michaelkellett

    Click on the HTML icon and remove the unwanted tags!

     

    LT Spice is free to anyone - if you get  chance then go to one of the Linear Technology lectures about it, delivered by Mike Engelhardt, I went to one in Edinburgh (part of the 2014 LTspice World Circuit ) and it was one of the best lectures of its kind I've ever attended.

     

    Sorry about the random font changes - blame the E14 editor !!

     

    MK