Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Power Supply for Home lab?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 136 replies
  • Subscribers 345 subscribers
  • Views 20582 views
  • Users 0 members are here
  • diy_power_supply
  • function_generator
  • power_supplies
  • diy
  • voltage/current
  • power_supply
  • power_meter
  • variable_power_supply
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Power Supply for Home lab?

mudz
mudz over 10 years ago

Hi,
I am starting this year with different projects. Indeed, I need a power supply which I felt for so long is the main missing component in my small home lab. Currently, I am using PC SMPS, Transformers, and different adaptors to power up different projects and kits.
Many times I felt need of a variable power source but I did that with two different power supplies, but it is time consuming. And many more things to say but its just a waste of time to write and for yourself to read...... Now Its too much and I'm going to build one good power supply. Previously I'm fulfilling my power supply needs by using a adaptor and then using a voltage regulator(7805, 7809, 7812, LM317..) afterward for my projects.
So, what do you suggest?

Also I'm going to include few more additions to it like function generator, power consumption meter.
So what do you suggest what will be the best thing to make a good power supply?

An IC?

A Microcontroller? like PIC

Just build a box consisting a transformer/adaptor with voltage regulator and few pots?

Do tell me which will be better to use? A microcontroller or IC available in market for specific task for example Function generator IC? I'm confused should I go with a microcontroller and make my own program to do these tasks or should I buy an IC for individual task and then using a controller to control all?

 

 

mudz

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    I know this is self promoting but I am in the middle of a set of tutorials on building a LAB / Bench power supply and accessories I start with the basic building blocks, explaining in practical terms what…
  • michaelkellett
    michaelkellett over 10 years ago +2
    There is no best - it depends what you are doing - I have loads of different power supplies (it's my work not just a hobby so they can be paid for if needed.) My favorite general purpose supply is a rather…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to mudz +2
    I would suggest starting with a basic naalog design (As I have shown in my series), understand its operation, then it should be a simple extension to add DAC and ADC monitoring this way it seperates the…
Parents
  • mudz
    mudz over 10 years ago

    One more question: Linear Power Supply or Switch Mode Power Supply?
    Depends? I may consider doing some business with it as well?
    My plans are to make it:
    1) less bulky/weight
    2) Compact

    3) portable

    4) Stablility with accuracy

    5) much Cheaper than market solutions

     

    mudz

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 10 years ago in reply to mudz

    As mentioned in one of my previous reply (in a joking way) - Linear Power supplies dissipate excess energy as heat and if there's a large difference between the input and output there's also lots of heat generated.

    Since DC Linear Power supplies generally work on a DC input and don't use a capacitor or inductor to store a self generated oscillating energy field thus they are much quieter than switching power supplies but usually contain huge and heavy stepping AC transformers to get the input voltages to a suitable level.

     

    The Apple ][ was one of the first personal computers to use a SMPS.  This was to reduce its weight by not needing a heavy step down AC transformer.

    It looked quite impressive, professional and very safe in its cadmium plated steel escutcheon.

     

    SMPSs are quite complex and bad things can happen when things go awry!

    That's one reason why there's such a variety of them and not just a single design to cater for all circumstances.

    One could view an SMPS as a radio transmitter that converts its outputs as a set of DC voltages. (by way of suitable filtering!)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • COMPACT
    COMPACT over 10 years ago in reply to mudz

    As mentioned in one of my previous reply (in a joking way) - Linear Power supplies dissipate excess energy as heat and if there's a large difference between the input and output there's also lots of heat generated.

    Since DC Linear Power supplies generally work on a DC input and don't use a capacitor or inductor to store a self generated oscillating energy field thus they are much quieter than switching power supplies but usually contain huge and heavy stepping AC transformers to get the input voltages to a suitable level.

     

    The Apple ][ was one of the first personal computers to use a SMPS.  This was to reduce its weight by not needing a heavy step down AC transformer.

    It looked quite impressive, professional and very safe in its cadmium plated steel escutcheon.

     

    SMPSs are quite complex and bad things can happen when things go awry!

    That's one reason why there's such a variety of them and not just a single design to cater for all circumstances.

    One could view an SMPS as a radio transmitter that converts its outputs as a set of DC voltages. (by way of suitable filtering!)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to COMPACT

    If we were all to use SMPS, what would we do w/ those "heavy stepping AC transformers"?

    Answer(s): Use them to Drown Minions. (only Kidding!) Use them to Drown Kittens (half-Heartedly) Kidding!BTW I still have a Transformer from an S-100 Imsai Computer (circa 1976?). It is about 3/4 the size of a (bread/bagel) Electric Toaster. Think of all the Kittens that will be in danger. Heck, forget the Kittens. The Transformer is so heavy, I am thinking Cats.

     

    ELY aka USCDADNYC

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 10 years ago in reply to uscdadnyc

    Did you build your S100 computer in the 1970's?

    And how about the really thick copper wires and giant filter capacitors that are larger than kittens for the +8V lines for the S100 bus!

    My S100 computer was internet connected, is yours?