Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Freescale KINETIS expert online next monday
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 308 subscribers
  • Views 1770 views
  • Users 0 members are here
  • freescale
  • kinetis
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Freescale KINETIS expert online next monday

PBrunner
PBrunner over 15 years ago

Gordon Padkin is our resident element14 expert on KINETIS and will be available online to answer any questions you may have on this product.

  • Sign in to reply
  • Cancel
Parents
  • PBrunner
    PBrunner over 15 years ago

    Hi Gordon, Can you explain more about the Low Power capabilities of this new MCU range and why it is suitable for use in my portable application? Thank you !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • PBrunner
    PBrunner over 15 years ago

    Hi Gordon, Can you explain more about the Low Power capabilities of this new MCU range and why it is suitable for use in my portable application? Thank you !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • GPADKIN
    GPADKIN over 15 years ago in reply to PBrunner

    Well there are several improvements and new features that Kinetis brings to market.

     

    Firstly as this family is based on a 90nm Thin Film Storage manufacturing process which can reduced the dynamic run current consumption by up to as much as 1/3 or previous manufacturing technologies.  the new Kinetis MCU family consumes as little as 200uA/MHz in run mode with clocks to CPU and all peripherals active.  In addition with the new features of the ARM Cortex M4 Core, specifically the MAC unit, SIMD unit and enhanced DSP instructions, help reduce further the number of cycles needed to process complex algorithms futher reducing the run current consumption.

     

    The other major benefit of the Kinetis range is the range of 10 flexible modes of operation, enabling designs to select the most appropriate mode to optimize the power consumption at any given moment.  The modes of operation are the standard Run, Wait & Stop modes. Plus you have the ability to scale the CPU and peripheral clocks down to 2MHz and enter into Very Low Power Run (VLPR) & Wait Modes (VLPW) and as an extension to these modes there is a Very Low Power Stop Mode.  Then with the additional of the NEW Low Leakage Wake-up Unit LLWU there are a range of modes where by the logic is completely shut down to further reduce leakage and overall power consumption. There are Low Leakage Stop (LLS) & Very Low Leakage Stop 1, 2 & 3 (VLLS1, VLLS2, VLL3). Each offering a different levels of functionality. In the lowest power mode, VLLS3 the Kinetis family will consume as little of 500nA.  The family also supports an extremely fast wake up time of 4uS.

     

    Other features of the Kinetis family include

         - Clock gating, to turn of clocks to unused moduels.

         - Indepent &  secure RTC with a dedicated 32KHz OSC and separate power system

         - Low Voltage Detect

     

    Hope this answers questions.

     

    Best Regards,

    Gordon