Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Design suggestion for a bus
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 33 replies
  • Subscribers 343 subscribers
  • Views 3893 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Design suggestion for a bus

amgalbu
amgalbu over 10 years ago

Hello

I need to develop a custom board (hardware + software) to drive a set pneumatic valves. The requirements are

  • the boards can be stacked (up to 18 boards can be stacked, but I expect this number to be increased in the future)
  • the boards must be configuration-free (no dip-switches to set the board address)
  • the bus must be fault-tolerant: if a board in the stack breaks, the other boards should continue to work properly
  • pneumatic valves are "digital", so the bus must convey only on/off commands

An external board communicates with the stacked boards through the bus and drives each pneumatic valve indivudually

 

The only solution I can think of is to have two serial buses: the first one is an in-out bus used only to configure the address of each board in the stack and is used only when the system is switched on. The second bus connects all the boards in parallel, thus providing the required fault-tolerance

 

However, this solution is far from being elegant... Does somebody have a better idea?

 

Cheers

Ambrogio

  • Sign in to reply
  • Cancel

Top Replies

  • crjeder
    crjeder over 10 years ago in reply to Robert Peter Oakes +1
    I2C adressability is an issue. E. g. a suitable device could be TPS22993 Quad Channel Load Switch with GPIO and I2C Control but it features only 3 adress pins for a max of 8 devices. But each can operate…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1
    Then by that measure, using a device like a 23017 http://ww1.microchip.com/downloads/en/DeviceDoc/21952b.pdf would give 16 valves on a board and re duce the count of boards considerably and only needs…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    Then by that measure, using a device like a 23017  http://ww1.microchip.com/downloads/en/DeviceDoc/21952b.pdf  would give 16 valves on a board and reduce the count of boards considerably and only needs a couple of OCTAL Driver chips to interface to relays / Solenoids

     

    I suspect this is compacting the control too much though but this is not known as your description does not provide too much of the operational details and is quite vague

     

    If you can provide more details of how this will be configured and what it is controling we can advise better

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • amgalbu
    amgalbu over 10 years ago in reply to Robert Peter Oakes

    Hi Peter

    I will try to explain the problem

    I have pneumatic valves that can be placed side-by-side as shown in this picture. You can (currently) have up to 38 valves

     

    image

    I need a board that controls these valves using a serial bus. There are two requirements:

    1. If (let's say) the central board does not switch on, all the remaining valves must continue to work normally

    2. The board must be "plug-and-play": when a board breaks down, the maintenance person take a spare part from the box, replace it and that's all

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to amgalbu

    The obvious way to do this is to use Devicenet

     

    https://www.google.co.uk/search?q=device+net+idc&ie=utf-8&oe=utf-8&gws_rd=cr&ei=8mO0VvPDI4fEOvCvgsAO

     

    If actual Devicenet is too expensive you could trawl the extensive literature for ideas.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • amgalbu
    amgalbu over 10 years ago in reply to michaelkellett

    Hi Michael

    The obvious way to do this is to use Devicenet

    Not sure why this is the obvious choice, since the devices will require a commissioning phase before installation and there are tens of industrial buses out there that are more widely used than DeviceNet

     

    If actual Devicenet is too expensive you could trawl the extensive literature for ideas.

    Yes, of course there is Google out there that can provide all the answers, but may be this community could provide suggestions based on hands-on experiences

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • amgalbu
    amgalbu over 10 years ago in reply to michaelkellett

    Hi Michael

    The obvious way to do this is to use Devicenet

    Not sure why this is the obvious choice, since the devices will require a commissioning phase before installation and there are tens of industrial buses out there that are more widely used than DeviceNet

     

    If actual Devicenet is too expensive you could trawl the extensive literature for ideas.

    Yes, of course there is Google out there that can provide all the answers, but may be this community could provide suggestions based on hands-on experiences

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 10 years ago in reply to amgalbu

    Well because Devicenet exists, uses low cost wiring, is simple enough that you might make the nodes small enough so that you could have one per valve.

     

    If you MUST have each node knowing its address without programming it must be plugged in to  a particular slot in the network (star connected) or be able to determine its position in  a daisy chained network.

     

    Both methods are quite high risk - being very susceptible to mis-plugging in the field.

     

    I'm sure that a position discovering daisy chain scheme could be devised but it's hard to imagine one that would be very reliable (all the obvious ways of doing it require nodes to actively process all messages that pass through them).

     

    My hands on experience of building machines and control electronics says use star wiring, design a reliable hardware driver and replace the whole board if it fails.

     

    If you can't get good enough reliability like that (and it wouldn't be good enough for some applications) then you are into a different realm alltogether and without very detailed information about the system I couldn't make any suggestions.

     

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • amgalbu
    amgalbu over 10 years ago in reply to michaelkellett

    Hi michael

    Which information do you need?