Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum 10,500mAh, 1.5V????
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 340 subscribers
  • Views 583 views
  • Users 0 members are here
  • 10
  • 1.5v
  • 500mah
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

10,500mAh, 1.5V????

e14 Contributor
e14 Contributor over 14 years ago

I am looking for a power solution that results in approx. 10,500mAh, 1.5V. The solution would ideally be as small as possible.

Any suggestions/advise would be much appreciated. Many thanks

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    what do you mean exactly?

    mAh is the unit of batteries, so 4 x AAA alcaline could do the job...

    or are you looking for a power source that replaces the battery?

    in this case you would need to generate 1.5V @ ILOAD from an input (solar, grid, another battery, etc...)

    KR

    Vincenzo

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to e14 Contributor

    mAh is Milliamp Hours, a unit for measuring electric power over time. It is commonly used to describe the amount of charge a battery can hold. The higher the mAh, the longer the battery will last.

     

    Unfortunately I don't believe there are any 1.5v batteries that can hold 10,500 mAh. Most I can think of would be a rechargeable AA with around 2500mAh.

    Smallest battery I have seen with up to 10k mAh was 6v, which was a lawnmower battery.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    I agree with Cory, you will be hard pressed to find one at that capacity

     

    you may be better off with a higher voltage battery and an efficient buck converter right at the place where the load is, this will eliminate allot of losses due to potentially inadequate cables and connectors (The buck converter will loose less than those)

     

    Regards

     

    Peter