Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum expert opinion needed on Raspberry Pi power issue
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 341 subscribers
  • Views 5048 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

expert opinion needed on Raspberry Pi power issue

e14 Contributor
e14 Contributor over 14 years ago

The Raspberry Pi has an LDO voltage regulator to produce 1.8v. 

However, a thermal image of the board, see post #6 on this thread:

http://www.element14.com/community/thread/18991

shows that this regulator, RG1, (the largest blue rectangle in the

upper-left quadrant) to be cool, while the hottest chip is the LAN chip

(SMSC LAN9512).  It turns out that the LAN chip has an internal

1.8v regulator, which user jamodio noticed is apparently connected

to the 1.8v power plane where it normally would be connected

only to decoupling capacitors, not the power plane.  User selsinork

verified that if RG1 is removed completely from the board, the

board still works, apparently drawing all its 1.8v power through

the LAN chip.  User beetem, who first noticed the cool RG1,

has commented on possible problems with having two LDO

regulators operating in parallel like this.

 

So is this really a problem?  If so, how serious?  Is there an

explanation for why some boards run significantly hotter than

others?  How to get element14's attention?

 

The latest thread is here:

http://www.element14.com/community/thread/19236?start=15&tstart=0

 

SMSC datasheet, showing VDD18CORE connected to decoupling

capacitors in Figure 2.2, page 16:

http://www.smsc.com/media/Downloads_Public/Data_Sheets/9512.pdf

 

Raspberry Pi Schematic 1.0, where top left of page 3 of 5 shows VDD18CORE

connected to +1.8v in addition to decoupling capacitors.

http://www.element14.com/community/solutions/5952

 

jamodio's original 10 June 2010 report (post #137)

http://www.element14.com/community/message/53280

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

     

    Mike Powell pinged me this thread directly and asked if I could respond, first apologies dropping of the radar (is it really that long!).  I have been looking at board bugs and this one is on my list, notes in my lab so more tomorrow.

     

    All - it would be really helpful if you could call out your serial numbers, it would allow me to find one in my stash with (hopefully) the same batch of parts, then we can get test aligned.

    Pete

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Pete,

     

    Serial number from the SoC or the label on the back of the board ?  The one I started modifying is labelled FN120711618 & SoC serial 000000001395836f not sure which number is more useful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Selsinork

     

    The FN number is the one, unfortunately my stash of boards runs out at FN120651352 so if the serial number are 'really' sequential you are 60K boards later than mine. [In reality we get a hole when the month changes so it's hard to predict exactly.] I'll call in some more testing samples from our partners.

     

    The warmest SMSC I have is 54C at T-ambient of 29C which is a deal cooler than the 61C reported.  There must be a corner case where RG1 is regulating low and the SMSC regulating high (as already suggested).  Time to ping off RG1 on a few more boards and see if I can kill one or get it to misbehave.

     

    On the case....

     

    Cheers

     

    Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    If it helps, my warm board with the elevated 1.8v is FN120744907

    Removing RG1 did seem to make it quite a bit hotter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Troy - thanks for that

     

    Do you have any way of measuring this - I would also be interested in the 1V8 voltage with RG1 off.

     

    Cheers

     

    Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Troy - thanks for that

     

    Do you have any way of measuring this - I would also be interested in the 1V8 voltage with RG1 off.

     

    Cheers

     

    Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    This particular board which was noticeably warmer than my others but not exceptionally hot was measuring 1837mV before and after (compared to 1793mV on another board). Measurement was taken across the RG1 common and output pads. Sorry, I don't have a way of accurately measuring temperature, only my finger.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Troy

     

    After years of soldering, I sort of got used to holding on to parts even though I knew they were burning my fingers as I would only need to resolder it again.  The advent of lead free has elevated the pain barrier again!

     

    So to be sure - you are saying that with RG1 out of the circuit and the SMSC providing all the power, the voltage was 1837mV and the same with RG1 reconnected?

     

    If any of the other 'hot runners' reading this thread could just measure the 1V8 that would be great, in fact anyone who could report, hot or warm and the voltage would be tremendously useful. {Don't forget serial numbers from the white label on the underside]

     

    Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Yes, I measured 1837mV before and after removing RG1, however it did get quite a bit hotter with RG1 off. Just to clarify what I said in the other thread, this is the second board I have taken to with the iron. The first one was fine (aside from a little instability, which is probably software related and me expecting too much) and I couldn't get it really hot even without RG1. The only modification made to this one was removing and replacing RG1.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Pete,

      It's good to see you back in this forum. 

     

    I'm curious if you have enough data to tell if the temperature

    distribution between different boards is normal (bell curve) or

    bi-modal (hot boards and merely warm boards, but not much

    between).

     

    I'm also curious if you think the 80mA current that Mackay measured

    at RG1 during startup would be enough to account for the observed

    temperature differences.

     

    followups can go to the other thread.