Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Need help, maybe need a circuit design?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 303 subscribers
  • Views 652 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Need help, maybe need a circuit design?

Former Member
Former Member over 13 years ago

Hello all, I'm here on a suggestion from a friend to hopefully get this problem sorted out. 

 

I currently have a function generator that just isn't cutting it anymore.  What I need is to pulse DC current, probably 12+ volts through a solution at about 20 amps.  I need to be able to control the frequency from 100 hz to like 500 khz, I currently do that by running 2 12 VDC power sources in series with a solid state relay on the negative side before the solution.  The SSR is controlled by the function generator, but it occured to me recently that the SSR can't function that fast so I need a new method.  Maybe a circuit?  Some specialized relay? 

 

As you can tell I'm pretty newbish at this, but am a fast learned since this is a very necessary piece of equipment at the moment

 

I look forward to any advice that you all can offer, Thank you

 

-Nathan

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 13 years ago

    Do you really mean 500kHz ?

    It can be done but it's way outside Solid State Relay territory.

    It's a serious design project - do you have  a budget to buy something or are you hoping for  a DIY solution >

     

    Michael Kellett

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to michaelkellett

    Its possible I'll only need up to about 300khz but i guess 500khz was too much wiggle room lol

     

    A DIY solution would be nice, but I've got to get it all set relatively soon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billpenner
    billpenner over 13 years ago in reply to Former Member

    By a solution do you mean a liquid? If not, is the load inductive? You might consider one or multiple power MOSFET(s).

     

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to billpenner

    Yeah its about 75% water.  Pretty darn conductive.  I was suggested MOSFETS and was told to buy a certain 6, 3 of each kind, but no one has been able to instruct me on how to wire everything up after that.  I can do basic circuits if I have a design, but mostly I'm quite helpless

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billpenner
    billpenner over 13 years ago in reply to Former Member

    Do you need to reverse the polarity? that is in effect, use an alterneting current or just pulse it off and on. Is the duty cycle 50% or does the pulse width change? Sounds like you are electroplating and/or polishing.

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • billpenner
    billpenner over 13 years ago in reply to Former Member

    Do you need to reverse the polarity? that is in effect, use an alterneting current or just pulse it off and on. Is the duty cycle 50% or does the pulse width change? Sounds like you are electroplating and/or polishing.

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 13 years ago in reply to billpenner

    The last time I wanted to do something a bit like this I bought a big audio power amplifier (1450W per channel 2900W bridged into 8 R) for about £200.  Currently CPC (a Farnell company) have a Behringer EP4000 listed which will do 4000W into 4R bridged.

    Now thats about 32A RMS or 44A peak so it should be OK with your 20A. Put a big resistor in series to limit the current (4R rated at 1000W min) and you are there - except that the amp may not like putting out pulses of the same polarity all the time. You could probably get round this by putting  a big diode in series with your load and providing  a path for current in the other direction with another big diode and a second power resistor.

     

    If you could provide a bit more detail about the waveforms you would like to achieve it would be easier to help. If it is for electroplating I assume that you know that you could just buy a suitable supply designed for the job.

     

    Michael Kellett