Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Distributing battery power to multiple components
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 338 subscribers
  • Views 3525 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Distributing battery power to multiple components

skjohnson
skjohnson over 12 years ago

Hello all,

 

I'm hoping to get some help with a problem that I'm not remotely qualified to figure out myself. It calls for an electrical engineering type, while I'm a physicist. Unfortunately, I'm all there is, so here I find myself.

 

I have a robot platform powered by a 24V 20Ah battery. The platform includes three set onboard power options:

  • 24V/5A
  • 12V/5A
  • 5V/5A

 

My requirements are actually the following:

  • 2x computer @12V/5A

 

Then the other items use a variable amount of current:

  • 3x DSLR @8.1V
  • 3x camera lights @7.2 to 8.4V (according to the specs, "9.6
  • 1x stepper motor @11V+ and current somewhere in the neighbourhood of 2 to 4A

 

I'm not really good with power, but from my limited understanding, I should ideally have some sort of circuitry to regulate the power and avoid any sort of spikes. The robot has just this sort of solution, as shown below:

 

image

image

I'd like to keep the computers running from the above convenient rail, but I'm wondering what a solution might look like, to power the other components that have variable current requirements. Should I be focusing on getting the specific voltage correct to each of the components and then letting the battery supply the appropriate current, or am I supposed to keep both in mind?

 

If I don't have to design anything from scratch, it would make life easier, but I'm game for anything, really.

  • Sign in to reply
  • Cancel
  • D_Hersey
    D_Hersey over 12 years ago

    "I think the computers are PCs (the clue was in "Operating the Intense PC ......", so I reckon he'll be running a full blown OS."

    Why tax my intuition when the horse is at hand?

    "BTW - how many microprocessors/micro-controllers aren't CMOS ?"

    You know what I meant:  Something intended to be an embedded platform, thus probably less consumptive than a desktop MB.  SS harddrives might be a step on the road to less power consumption in this mysterious application.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • skjohnson
    skjohnson over 12 years ago in reply to jw0752

    Don, other than the robotic base, this is almost entirely put together from off the shelf parts, as it's just a prototype. I'll definitely keep your suggestion in mind for a possible next version, although one of the PCs is Windows-based, while the other is linux. The power savings are attractive, but this is definitely beyond my current scope.

     

    John, thanks for the link to the part. It turns out it's a generic Chinese part that various companies rebrand, so I was able to source the same part from Amazon (amusingly here and here, with the same picture) so I'll keep everyone posted, once it arrives and I get it installed. You've all been a great help, so I'm very much obliged and appreciative!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 12 years ago in reply to skjohnson

    Glad we could be of help. I look forward to hearing how your project turns out.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • skjohnson
    skjohnson over 12 years ago in reply to jw0752

    John, et al.

     

    I just wanted to give a warm thanks for the assistance. I was able to get everything working, using the helpful information I received in this thread. Cheers and thanks again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<