Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Booting Linux on iMX6q Sabre Lite.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 305 subscribers
  • Views 525 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Booting Linux on iMX6q Sabre Lite.

Former Member
Former Member over 11 years ago

Hi,

 

I have one of the iMX6 quad boards (built to Sabre Lite). The pre-built MicroSD card boots and works fine but I want to build my own image. I did the following on my host:

 

      sudo apt-get install gawk wget git-core diffstat unzip texinfo chrpath

      sudo apt-get install build-essential libsdl1.2-dev xterm curl

     mkdir ~/bin

     cd ~/bin

     curl http://commondatastorage.googleapis.com/git-repo-dwonloads/repo > repo

     chmod a+x repo

      mkdir ~/fsl

      cd ~/fsl

      repo init -u https://github.com/Freescale/fsl-community-bsp-platform -b dizzy

      repo sync

      source setup-environment build

    

Edit conf/local.conf and change MACHINE to "imx6qsabrelite"

    

     bitbake core-image-minimal

 

Insert 4G MicroSDCard (device /dev/sdb)


     cd tmp/deploy/image/imx6qsabrelite

     sudo dd if=core-image-minimal-imx6qsabrelite.sdcard of=/dev/sdb bs=1M

     sync

 

Put SDCard into my board and power on.

In the terminal, I get:

 

U-Boot 2009.08 (Aug 16 2012 - 10:06:42)

CPU:   Freescale i.MX 6 family 0.0V at 792 MHz
Temperature:   43 C, calibration data 0x5784bd7d
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock     : 66000000Hz
ipg per clock : 66000000Hz
uart clock    : 80000000Hz
cspi clock    : 60000000Hz
ahb clock     : 132000000Hz
axi clock   : 264000000Hz
emi_slow clock: 29333333Hz
ddr clock     : 528000000Hz
usdhc1 clock  : 200000000Hz
usdhc2 clock  : 200000000Hz
usdhc3 clock  : 200000000Hz
usdhc4 clock  : 200000000Hz
nfc clock     : 24000000Hz
Board: MX6Q-SABRELITE:[ POR]
Boot Device: I2C
I2C:   ready
DRAM:   1 GB
MMC:   FSL_USDHC: 0,FSL_USDHC: 1
JEDEC ID: 0xbf:0x25:0x41
Reading SPI NOR flash 0xc0000 [0x2000 bytes] -> ram 0x276009b8
SUCCESS

*** Warning - bad CRC, using default environment

In:    serial
Out:   serial
Err:   serial
Net:   got MAC address from IIM: 00:00:00:00:00:00
FEC0 [PRIME]
Hit any key to stop autoboot:  0
Card did not respond to voltage select!
mmc0(part 0) is current device
MMC: block number 0x1 exceeds max(0x0)
** Can't read from device 0 **

** Unable to use mmc 0:1 for fatload **
** Bad partition 1 **
mmc1 is current device
reading /6q_bootscript

** Unable to read "/6q_bootscript" from mmc 1:1 **
Loading file "/6q_bootscript" from mmc device 1:1 (xxb1)
Failed to mount ext2 filesystem...
** Bad ext2 partition or disk - mmc 1:1 **
MX6Q SABRELITE U-Boot >

 

Since this is all fairly new to me, I'm at a loss as to what to do next. I was hoping the Yocto build would produce a working SDCard image for me. Have I missed some vital step?

 

I looked on the SDCard and there was a 6x_bootscript. I renamed this to 6q_bootscript and now have the following:

 

U-Boot 2009.08 (Aug 16 2012 - 10:06:42)

CPU:   Freescale i.MX 6 family 0.0V at 792 MHz
Temperature:   43 C, calibration data 0x5784bd7d
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock     : 66000000Hz
ipg per clock : 66000000Hz
uart clock    : 80000000Hz
cspi clock    : 60000000Hz
ahb clock     : 132000000Hz
axi clock   : 264000000Hz
emi_slow clock: 29333333Hz
ddr clock     : 528000000Hz
usdhc1 clock  : 200000000Hz
usdhc2 clock  : 200000000Hz
usdhc3 clock  : 200000000Hz
usdhc4 clock  : 200000000Hz
nfc clock     : 24000000Hz
Board: MX6Q-SABRELITE:[ POR]
Boot Device: I2C
I2C:   ready
DRAM:   1 GB
MMC:   FSL_USDHC: 0,FSL_USDHC: 1
JEDEC ID: 0xbf:0x25:0x41
Reading SPI NOR flash 0xc0000 [0x2000 bytes] -> ram 0x276009b8
SUCCESS

In:    serial
Out:   serial
Err:   serial
Net:   got MAC address from IIM: 00:00:00:00:00:00
FEC0 [PRIME]
Hit any key to stop autoboot:  0
MMC: block number 0x1 exceeds max(0x0)
** Can't read from device 1 **

** Unable to use mmc 1:1 for fatload **
Wrong Image Format for bootm command
ERROR: can't get kernel image!
MX6Q SABRELITE U-Boot >

 

Can somebody point me in the right direction please?

 

TIA,

 

Richard.