Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Why use bitwise OR / AND
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 317 subscribers
  • Views 563 views
  • Users 0 members are here
  • coding
  • computer
  • programming
  • bitwise
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Why use bitwise OR / AND

Former Member
Former Member over 11 years ago

I have been programming for over an year now. I still don't get why bitwise OR and AND operators are used. They seem to return random numbers.

What mathematical purpose do they have?

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    It can seem this way if your looking at the values as decimal or hex These operations are a binary operation so it works on ones and zeroes For example the decimal number 15 is 0F in hex or 00001111 in…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    It can seem this way if your looking at the values as decimal or hex

     

    These operations are a binary operation so it works on ones and zeroes

     

    For example the decimal number 15 is 0F in hex or 00001111 in binary

     

    If I and 16 with 4 I will get 4, why well consider the binary value

     

    0000 1111 <-- 16

     

    0000 0100 <-- 4

     

    Only where the ones align will you have a 1 left in the answer, therefor you get 00000100 or 4

     

    It can appear random if your looking at the number in decimal

     

    Now the opersit is more confusing

     

    Given

     

    01010011 <-- 83 anded  with

     

    10010101 <-- 149 results in

     

    00010001 <-- 17

     

    Looking at this in decimal would be really confusing but looking at it in binary it makes perfect sense. So again only where the ones match are you left with a one. With the OR operator it wirks that you get a one where ever there is a one on either or both sides (But no carry)

     

    So

     

    10101010 OR

     

    01010101 =

     

    11111111

     

     

     

    Then again

     

    11110000 OR

     

    00000000 =

     

    11110000

     

    Hope that clarifies the issue

     

    Also the binary notation has values like this

     

    128, 64, 32, 16, 8, 4, 2, 1 and to get to the decimal just add up where each bit has a one aligned with it

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago

    In low-level programming, you often use an integer to represent a collection of single bit fields, or fields that are only a few bits wide.  The bit-wise operators are useful for checking the values of those fields or changing individual bits.  A good example in GNU/Linux is the "file mode" field that represents permissions as a bit vector, often shown in octal.  For example, "0664" = 110.110.100 means that the file is readable and writable by its owner and its group, but to the world it's read-only.

     

    Data communications protocols often use individual bits and short fields in headers for various control purposes.

     

    Bit-wise AND and OR are often used for device registers, where individual bits may represent the values of GPIO inputs or outputs.

     

    Bit-wise XOR is often used for making linear-feedback shift registers, which may be used as pseudo-random number generators.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago

    Thanks guys. You have been very helpful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 11 years ago

    Sometimes one operand word is data and the other is a mask.  Let's say that three separate binary events in I/O land are required to draw a conclusion.  By using the mask we can check the conditions in parallel, rather than sequentially.  Saves time.

    Easier to modify.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 11 years ago

    Sometimes, when working with this, it is better to have your numbers represented as hexadecimal.  Then your numerals correspond to four-bit groups.  Makes it easier to reckon in.