Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum John Wiltrout, I was remiss in under-correcting you the other day!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 338 subscribers
  • Views 2293 views
  • Users 0 members are here
  • resistors
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

John Wiltrout, I was remiss in under-correcting you the other day!

D_Hersey
D_Hersey over 11 years ago

In a thread you stated that the only way to compare two resistors was to put them in a string, put a potential across said string and measure and compare the drops of the two loads.  I won't go digging up the thread, because I am far too much of a gentleman for something as crass as that.  Please take the essence of my rendition as accurate.

 

image

At the time I noted that you had overlooked the Norton alternative.  But as my head hit the pillow tonight, the ghosts of ETs past implored me in both ears:  SOMEONE IS WRONG ON THE INTERNET!  Our doppelgänger del Norte, JWT!  You are guilty of dissimulating John's degree of wrongness, Don!  Get up and type!

 

Consider:

 

image

Imagine that the first two circuits have a dashed rectangles around them, sparing the terminals.  They are 'black boxes.'  For concreteness, let's imagine that each resistor is one ohm/Siemens.  The black boxes would measure out to be one ohm/Siemens.

Pretend that the horizontal line in the second diagram is a jumper.  How much current flows through this wire?  None, ever.  Whether the jumper is attached will be known only to the 'inside the box' community.

So, the (bipolar) ammeter in the third diagram reads zero if Ra=Rb.  Else it will indicate which resistor is larger/smaller.  Remember, the galvanic meter is highly sensitive, although passive.  This circuit arrangement is called a "Whetstone Bridge."

 

Whetstone is a place in England where people like to balance things.

 

So there we have it, friend.

  • Sign in to reply
  • Cancel
  • D_Hersey
    D_Hersey over 11 years ago

    A little about the Norton amp, filtered by the decades.  With a Norton amp or an op-amp that is configured in the negative-feedback mode there is no theoretical limit on input voltage.  LM3900 holds its inputs at IIRC about a diode-drop up from BoS.  The op-amp input will sit at the reference level.  In real life the input resistor should be qualified for HV, split, and equipped with Zener-like diodes at the tap.  I'm  not suggesting anyone play with HV, I'm tryin' to illustrate the concept.

     

    Audio guys who are averse to shot noise embraced the LM3900.  I've heard the new device, the third link in my prior list is really the bomb.  I know you know this, MK, but for any innocent lurkers, shot noise describes an issue when HiFi audio is represented with low levels of current.  Not enough electrons analogises to limited sampling resolution in digital.  The audio guys also have to deal with the electrons jiggling, which they refer to as thermal noise.  The op amp can be rather susceptible to (shot noise) this, due to its naturally high Zin.

     

    Some golden-ears find shot noise to be more dystopic than thermal noise.  They would embrace this schema.

     

    ==========

    I find it dystopic that the spell-checker is unaware of the word dystopic.  It's just dystopic.

     

    John, in the normal case you have to provide your own input resistors to limit current when using a Norton amp.  This is not the case with op-amps, typically.  With op-amps there can be input resistors to balance the dissipation on both sides of the input mirror.  This minimises an additional offset and an additional offset drift term, but they are far less fundamental than the input resistors of a Norton amp.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 11 years ago

    John, although the Wheatstone bridge was invented a long time ago, it is timeless:

     

    Analog Devices : Analog Dialogue : Weigh Scale Design

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 11 years ago

    We can rustle around out back and come back with a SQUID:

     

    SQUID - Wikipedia, the free encyclopedia

     

    http://hyperphysics.phy-astr.gsu.edu/hbase/solids/squid.html

     

    First-order Hall effect is linear:

     

    Hall effect - Wikipedia, the free encyclopedia

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<