Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Problem getting CW10.6 to connect to test board but P&E Multilink works fine.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 302 subscribers
  • Views 460 views
  • Users 0 members are here
  • multilink;
  • kinetis
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Problem getting CW10.6 to connect to test board but P&E Multilink works fine.

astrayelmgod
astrayelmgod over 10 years ago

Hi --

 

I have CW 10.6.4 for a MK64FX512 project and a P&E Multilink Universal FX connected to our target board.  My code just waves two  port B lines up and down, nothing else.

 

If I use the P&E PROGACMP Programmer directly, it works just fine.  It can connect to the board, display memory, clear and program the memory.  Powering the board down overnight, then retesting the next day shows the same memory contents as before.  So, I am pretty sure the hardware is OK.

 

CW compiles the code, then crashes at about the point where it tries to download the code.  Doesn't matter if I choose Run or Debug.  Doesn't matter what speed I choose (Multilink runs at 12.5MHz).  Doesn't matter if I add a delay after reset.  Doesn't matter how many times I refresh/retry.  The dialog box says:

 

P&E Connection Assistant

 

An error occurred while connecting to the interface hardware or target

specified in the Launch Configuration Dialog.  for this launch, you may

retry/re-specify the connection with the following parameters:

 

All of the visible settings are identical to the ones in PROGACMP.  But it won't connect.

 

Any suggestions?

  • Sign in to reply
  • Cancel
  • astrayelmgod
    astrayelmgod over 10 years ago

    I fixed it.  I had the SWD box checked when it shouldn't have been.