Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Battery Charging using DC Motor
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 30 replies
  • Answers 12 answers
  • Subscribers 346 subscribers
  • Views 19887 views
  • Users 0 members are here
  • battery_charge
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Battery Charging using DC Motor

e14 Contributor
e14 Contributor over 11 years ago

I have been trying to wrap this idea around my head that I can successfully charge a battery by using a DC motor.  Here is the example:  You have let's say a 16,000mAh 6S Lipo Battery.  This battery is your primary energy source.  This battery will power a brush-less DC motor.  When the DC motor is creating high RPM's, this energy would be used to recharge the primary battery, while also powering other components within the device.  In this example, the device housing these components would be a cooling fan for a motor design I am working on. 

 

Is this possible?

 

If it is, one thing I concern myself with, is that the battery designs of today, mostly only have one connection, which is used to plug into the charger or to plug into the device you wish to operate.  If this is in fact possible, I would like to speak further with you on perhaps helping me develop a solution.  Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +4 suggested
    Hi Dan, shabaz is correct. If you make a motor spin with a battery the energy comes from the battery and is converted to mechanical energy and heat in the motor. In order to charge a battery with a motor…
  • jw0752
    jw0752 over 11 years ago in reply to mrsyfy +4 suggested
    Hi Douglas, Thinking outside the box is good. shabaz did a good job of summarizing and expanding my post. Certainly some energy can be recovered if there is a need for the energy and if it is economically…
  • michaelkellett
    michaelkellett over 9 years ago in reply to empresario +4 suggested
    I am quite sure that you have NOT seen any such thing but it may be that some freak circumstances or clever tricks have deceived you. If you could describe what you have seen and better still offer pictures…
Parents
  • shabaz
    0 shabaz over 11 years ago

    Sounds like those mythical 'free energy' ideas. If the battery is powering the motor, then a certain amount of energy is needed to do this. That energy came from the battery (due to a chemical reaction).

    If you wish to use the motor to charge the battery then that energy comes from.. that's right, the battery itself.

    So the answer is yes, it is possible (with a complex circuit since you're using a brushless motor) to charge a battery but won't result in anything useful since work is being done to put energy back into the battery (and that energy originally was supplied from the battery) and you have conversion losses at all stages. There are probably hundreds of such discussions on the Internet - for some reason it seems a popular thought. See here for some more discussion on it: https://www.physicsforums.com/threads/how-to-use-an-electric-motor-to-recharge-a-battery.535694/

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to shabaz

    This is the second principle of the thermodynamics.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to balearicdynamics

    Hi Enrico,

    Sorry I was still typing my post when you mentioned the second law of Thermodynamics so I didn't see that you had already mentioned it until after my post.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to jw0752

    Repetita juvant friend ! But this seems having no effect on a lot of free energy inventors image

     

    My general question is - how is it possible that someone tried to propose energy solutions, ANY kind of energy solution, without knowing the minimal, essential, laws that roles our part of universe? This is the real mystery ...

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to balearicdynamics

    how is it possible that someone tried to propose energy solutions

    What amazes me more is that it wasn't thought of before .... image

    Enrico ....Didn't you know you can find all the answers on the internet...they might not be right, but because they are there they must be. image

     

    I think the fundamental understanding about energy is that it is always converted into something ...it's never lost just converted.

    Because there are no free lunches ... some is always lost ... usually to heat, hence nothing will ever be 100% efficient, there will always be losses.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to mcb1

    I think that we should make an Arduino project demonstrating the Carnot cycle image with sensors it's not difficult to see the disperse entropy and why adiabatics are not straight lines ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to mcb1

    I think that we should make an Arduino project demonstrating the Carnot cycle image with sensors it's not difficult to see the disperse entropy and why adiabatics are not straight lines ...