Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Battery Charging using DC Motor
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 30 replies
  • Answers 12 answers
  • Subscribers 346 subscribers
  • Views 19887 views
  • Users 0 members are here
  • battery_charge
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Battery Charging using DC Motor

e14 Contributor
e14 Contributor over 11 years ago

I have been trying to wrap this idea around my head that I can successfully charge a battery by using a DC motor.  Here is the example:  You have let's say a 16,000mAh 6S Lipo Battery.  This battery is your primary energy source.  This battery will power a brush-less DC motor.  When the DC motor is creating high RPM's, this energy would be used to recharge the primary battery, while also powering other components within the device.  In this example, the device housing these components would be a cooling fan for a motor design I am working on. 

 

Is this possible?

 

If it is, one thing I concern myself with, is that the battery designs of today, mostly only have one connection, which is used to plug into the charger or to plug into the device you wish to operate.  If this is in fact possible, I would like to speak further with you on perhaps helping me develop a solution.  Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +4 suggested
    Hi Dan, shabaz is correct. If you make a motor spin with a battery the energy comes from the battery and is converted to mechanical energy and heat in the motor. In order to charge a battery with a motor…
  • jw0752
    jw0752 over 11 years ago in reply to mrsyfy +4 suggested
    Hi Douglas, Thinking outside the box is good. shabaz did a good job of summarizing and expanding my post. Certainly some energy can be recovered if there is a need for the energy and if it is economically…
  • michaelkellett
    michaelkellett over 9 years ago in reply to empresario +4 suggested
    I am quite sure that you have NOT seen any such thing but it may be that some freak circumstances or clever tricks have deceived you. If you could describe what you have seen and better still offer pictures…
Parents
  • Capper
    0 Capper over 11 years ago

    Of course you can charge a battery from a dc motor, that's how generators work.  You just can't do it at the same time you're powering the motor.

    Look up regenerative brake "https://en.wikipedia.org/wiki/Regenerative_brake"

    Keep thinking,

    Scott

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Capper
    0 Capper over 11 years ago

    Of course you can charge a battery from a dc motor, that's how generators work.  You just can't do it at the same time you're powering the motor.

    Look up regenerative brake "https://en.wikipedia.org/wiki/Regenerative_brake"

    Keep thinking,

    Scott

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • empresario
    0 empresario over 9 years ago in reply to Capper

    it is possible and i have seen such

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to empresario

    I am quite sure that you have NOT seen any such thing but it may be that some freak circumstances or clever tricks have deceived you.

     

    If you could describe what you have seen and better still offer pictures or links I'm sure that plenty of E14 people will be very happy to explain what you might have seen - and why it doesn't do what it seems.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • pettitda
    0 pettitda over 9 years ago in reply to michaelkellett

    I suppose if you had two sets of armature coils you could technically "charge" the battery from one set of coils and discharge the battery from the other set of coils.  Although arguably you couldn't say you were charging the battery because the net flow of current would be out of the battery not into it.  It would be more of a Rube Goldberg experiment than anything else.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 9 years ago in reply to Capper

    Look up regenerative brake

    But the power from regenerative braking comes from slowing down the vehicle. It takes much more energy to get that vehicle moving than you get out of regen braking. Except when going down a hill, but eventually you'll have to get back up that hill.