Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum weight change sensor for arduino?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 303 subscribers
  • Views 1137 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

weight change sensor for arduino?

Former Member
Former Member over 10 years ago

Hello everyone,

 

I am a newbie, but I have done a fair bit of reading and researching about Arduino programming and motor controlling and I think with some help from you I am ready to start my project which is basically an electric fishing reel to be used for automatic jigging.

 

The idea is based on programming the motor to let the fishing line drop down to the bottom then start hauling it in cycles at different speeds and distances, and when fish strikes, it hauls the line all the way up to the boat !

 

my question is, is there a sensor that can sense the weight change on the line to trigger the hauling process?

For example, if I program the sensor for the normal operating weight on the line to be between 0.5kg and 0.75kg, and anything above that will be considered as a catch and will start the hauling process.

 

There are few automatic jigging machines in the market which I got the idea from, but way too expensive "over $3000", and also on a commercial fishing scale which is not my field.

And they work the same way I explained above "sensing the extra weight on the line", so I am confident that there is a sensor of that kind, but unfortunately I failed to find it so far !

 

It would be great to get an answer so I can go ahead and start the project.

 

I still have some more questions about the project, but I thought I would start with this one, and then take it from there.

 

Thank you in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +1
    Maybe all you need is a spring - when it stretches far enough it closes a switch.
Parents
  • dougw
    0 dougw over 10 years ago

    Maybe all you need is a spring - when it stretches far enough it closes a switch.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to dougw

    Douglas,

    That's definitely a great simple idea, but the problem here will be the sea condition as it is sometimes rough and the boat will be rocking up and down which will cause extra tension on the line and as a result the spring will be stretched and will haul the line thinking it is a fish, and also if I decide to change the sinker to a heavier one it will stretch the spring and I will be forced to keep changing springs from lighter to heavier and vice versa !

     

    I was thinking about a current sensor and using "if" logic to program it to stay in normal operating condition if the current on the motor is between two numbers "allowing for different conditions", and if the current goes beyond the programmed number, then a hauling process starts.

    This way it will be a matter of software programming trials and errors as opposed to hardware replacements !

     

    Another thing I thought about was a load cell attached to a pulley with the line going through it and program it to stay normal between two number and when it goes beyond that with the line tension it will start hauling !

     

    Please have a look at video in my pervious reply above, that might make it clearer as my English is not that good.

     

    The challenge for me as a beginner will be writing the script to program the motor to do what I want it to, but I am sure you guys will help.

     

    Cheers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to Former Member

    If you can put the work into development the load cell approach will ultimately give better results because you can measure line tension much more directly. Measuring motor current is cheaper and easier but may not be sensitive enough  because of mechanical losses in the coupling between the motor and the line tension. Why not try some measurements of motor current and see what happens.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to Former Member

    If you can put the work into development the load cell approach will ultimately give better results because you can measure line tension much more directly. Measuring motor current is cheaper and easier but may not be sensitive enough  because of mechanical losses in the coupling between the motor and the line tension. Why not try some measurements of motor current and see what happens.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 10 years ago in reply to michaelkellett

    Michael,

     

    you are absolutely right, but using the load cell will make the machine more exposed to environmental elements "heat, humidity, salt, corrosion, etc..." as it will have to be mechanically attached to the line, where in the current sensor everything can be housed in a sealed box and the only exposed part will be the motor pin which will be driving the reel, and everything else will be safe inside the housing and communicating with the motor internally (that's the theory anyway).

     

    I don't need it to be super sensitive anyway, for example lets say I have current values from 1minimum  to 10maximum and if I can program the motor to operate normally between "current value1 and current value4" so the variation in water condition and boat movement will be allowed for, and anything above current value4 will tell the motor to haul the line all the way up to the boat.

     

    as I said, I am still a beginner and working my way around programming and choosing the right stuff for my project which I think is a bit too advanced for my limited knowledge, but with some help and expert ideas I will get there in the end image

     

    please feel free to correct me any time and any suggestion is most welcomed.

     

    Cheers.