Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum weight change sensor for arduino?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 303 subscribers
  • Views 1129 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

weight change sensor for arduino?

Former Member
Former Member over 10 years ago

Hello everyone,

 

I am a newbie, but I have done a fair bit of reading and researching about Arduino programming and motor controlling and I think with some help from you I am ready to start my project which is basically an electric fishing reel to be used for automatic jigging.

 

The idea is based on programming the motor to let the fishing line drop down to the bottom then start hauling it in cycles at different speeds and distances, and when fish strikes, it hauls the line all the way up to the boat !

 

my question is, is there a sensor that can sense the weight change on the line to trigger the hauling process?

For example, if I program the sensor for the normal operating weight on the line to be between 0.5kg and 0.75kg, and anything above that will be considered as a catch and will start the hauling process.

 

There are few automatic jigging machines in the market which I got the idea from, but way too expensive "over $3000", and also on a commercial fishing scale which is not my field.

And they work the same way I explained above "sensing the extra weight on the line", so I am confident that there is a sensor of that kind, but unfortunately I failed to find it so far !

 

It would be great to get an answer so I can go ahead and start the project.

 

I still have some more questions about the project, but I thought I would start with this one, and then take it from there.

 

Thank you in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +1
    Maybe all you need is a spring - when it stretches far enough it closes a switch.
Parents
  • clem57
    0 clem57 over 10 years ago

    So is this what you are looking for Fishamatic, ice Fishamatic tackle - fishing rod hook setters?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    So is this what you are looking for Fishamatic, ice Fishamatic tackle - fishing rod hook setters?