Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Raspberry Compute Module IO Board
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 342 subscribers
  • Views 1908 views
  • Users 0 members are here
  • board
  • io
  • raspberry-pi
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Raspberry Compute Module IO Board

e14 Contributor
e14 Contributor over 11 years ago

I am currently working on a IO board development and would like to know if a LAN7500 chip can take place of the LAN9512 from the Model B/B+? My reasoning is that I would like to have a product that can support 10/100/1000 internet speeds where it is available. Any help is greatly appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to bobalexander +2
    Since I couldn't remember off the top of my head I had to go back through the datasheets and it appears that it can only handle up to 480 Mbps at the High end. So it would appear that using the LAN7500…
Parents
  • screamingtiger
    0 screamingtiger over 11 years ago

    I question if the Raspberry Pi could handle 1000MBS, it may not have enough CPU power to keep up.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to screamingtiger

    screamingtiger

         Actually it would be 1000 million bit per second theoretically which comes to a bit more than 100 million bytes per second which overwhelms USB's 480Mbit/s. I would say the problem comes when using external USB disk like SSD which could saturate the interface.

    C

    Edit corrected statement.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago in reply to screamingtiger

    screamingtiger

         Actually it would be 1000 million bit per second theoretically which comes to a bit more than 100 million bytes per second which overwhelms USB's 480Mbit/s. I would say the problem comes when using external USB disk like SSD which could saturate the interface.

    C

    Edit corrected statement.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to clem57

    Well actually it would be  a bit like having  a switch between two computers where one uses 100Mbit Ethernet and the other uses 1Gbit. In this case the LANxxx chip will be buffering the data but the OP won't gain any great advanatge (if any) in throughput and will have the disadvantage of cutting himself off from any community support for the existing and normal solution. It sounds  a bad plan to me.

     

    @Cody  - it looks to me as if you have neither experience or test gear - in which case your only chance of making the the high speed stuff work is to copy exactly the RPIi breakout board for the tracking of high speed signals. (ie - if they use 0..5 oz copper tracks 0.2mm wide, 0.5mm apart separated from a ground plane by xmm of FR4 board then you must too.) The problem you will find is that they don't give you a step by step guide. You may get lucky but this is more a case of trying to fly before you can walk !

     

    Why are you using the compute board at all - isn't there any easier way of getting where you want be ?

     

    MK