Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Raspberry Compute Module IO Board
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 342 subscribers
  • Views 1915 views
  • Users 0 members are here
  • board
  • io
  • raspberry-pi
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Raspberry Compute Module IO Board

e14 Contributor
e14 Contributor over 11 years ago

I am currently working on a IO board development and would like to know if a LAN7500 chip can take place of the LAN9512 from the Model B/B+? My reasoning is that I would like to have a product that can support 10/100/1000 internet speeds where it is available. Any help is greatly appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to bobalexander +2
    Since I couldn't remember off the top of my head I had to go back through the datasheets and it appears that it can only handle up to 480 Mbps at the High end. So it would appear that using the LAN7500…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    A point to take note of

     

    The physical layer is the part that is 10, 100 or 1000 Mbits, nothing above that even really cares and it is only relevent between the two directly connected devices (Pi and a HUB for instance). if any other devices are not compatable at the same speed when the connection is established then the two connected devices agree on a common speed, often with modern chips also compensating for non MX cables too if needed. if a PI connected to a hub is 100Mbit and on the hub is the PC at 1GBit, the HUB will buffer and speed shift between the two

     

    The TCP/IP layer is completly seperate and it often has a bigger impact as it decides the packet size, typically 1500bytes per packet but this can again be over-ridden if desired and you know what your doing

     

    USB is as correctly stated a 480MBit bus so the PI irrespective of its performance will never get to exceed that, meaning it will never be able to make full use of a 1GBit LAN but can participate on one, the higher speed will mean it gets its data out of the chip and on its way quicker and therefor will free up the LAN quicker. If the PI was uprated to USB3 then of course things improve quite a bit, or a LAN chip is more directly connected to the chip / CPU bus.

     

    So does a faster LAN chip have benefits... yes. will the app get its data out quicker if everything else is the same, probably not or only marginally so is it really worth it, you can judge that yourself

     

    as far as designing a board to be faster for networking and USB, have you looked at this :- Meet MinnowBoard MAX | minnowboard.org or this ODROID | Hardkernel, basically the job your trying to do has been done and for a good price too so unless your doing it purly for the intelectual excersize, your trying to replicate whats been done already

     

    And thats OK, I just want you to understand what your facing

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    A point to take note of

     

    The physical layer is the part that is 10, 100 or 1000 Mbits, nothing above that even really cares and it is only relevent between the two directly connected devices (Pi and a HUB for instance). if any other devices are not compatable at the same speed when the connection is established then the two connected devices agree on a common speed, often with modern chips also compensating for non MX cables too if needed. if a PI connected to a hub is 100Mbit and on the hub is the PC at 1GBit, the HUB will buffer and speed shift between the two

     

    The TCP/IP layer is completly seperate and it often has a bigger impact as it decides the packet size, typically 1500bytes per packet but this can again be over-ridden if desired and you know what your doing

     

    USB is as correctly stated a 480MBit bus so the PI irrespective of its performance will never get to exceed that, meaning it will never be able to make full use of a 1GBit LAN but can participate on one, the higher speed will mean it gets its data out of the chip and on its way quicker and therefor will free up the LAN quicker. If the PI was uprated to USB3 then of course things improve quite a bit, or a LAN chip is more directly connected to the chip / CPU bus.

     

    So does a faster LAN chip have benefits... yes. will the app get its data out quicker if everything else is the same, probably not or only marginally so is it really worth it, you can judge that yourself

     

    as far as designing a board to be faster for networking and USB, have you looked at this :- Meet MinnowBoard MAX | minnowboard.org or this ODROID | Hardkernel, basically the job your trying to do has been done and for a good price too so unless your doing it purly for the intelectual excersize, your trying to replicate whats been done already

     

    And thats OK, I just want you to understand what your facing