Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Which board to use for outdoor lighting controller?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 318 subscribers
  • Views 727 views
  • Users 0 members are here
  • lighting
  • landscape
  • sbc
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Which board to use for outdoor lighting controller?

ksmiller99
ksmiller99 over 10 years ago

Hello All,

With the plethora of available boards, I'm having trouble deciding what board(s) to use for a one-off outdoor lighting controller for personal use. The lighting is just a few addressable RGB LED strips. What I imagine is a board that has an Arduino-like side for real-time control of the LEDs and a Linux-like side that has WiFi and runs a small web server to allow a user to select which lighting program to run. I'd like to avoid having extra functionality that won't be used such as Ethernet and video, which adds to the cost and is an additional point of failure. Cost is a factor, and I could use two boards and/or add-on boards, but because it will be outdoors, I think the connections should be soldered because of humidity and other weather issues.

 

Do you have any board or design suggestions?

 

Thanks,

Kevin

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1 suggested
    If you want to stick with the Arduino side of things then the board that pretty much exactly matches your requirements is the Arduino Yun All the details are here: https://www.arduino.cc/en/Main/ArduinoBoardYun…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to clem57 +1
    Talk about great minds think alike , I was saying the exact same thing at the same time as you lol
Parents
  • clem57
    0 clem57 over 10 years ago

    Yun fits the bill very nice with arduino interfacing and wireless access from the net. Included is remote API controllable from the web to turn on or off pins.

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to clem57

    Talk about great minds think alike image, I was saying the exact same thing at the same time as you lol

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to clem57

    Talk about great minds think alike image, I was saying the exact same thing at the same time as you lol