Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Reuse of blu ray drive with raspberry pi?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 339 subscribers
  • Views 1652 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Reuse of blu ray drive with raspberry pi?

e14 Contributor
e14 Contributor over 10 years ago

Hello,

 

I have an old standalone blu ray player laying around and want to use it as a housing for my pi as a media player.

My initial plan was to only keep the case and power supply, but I am wondering if there is any chance of using the built in blu ray tray with the pi...

Powering the tray should be no problem but is the data connection of these trays of any standard or proprietary?

(To be more precise, its a Philips BDP3300, if this is of any help image)

 

Any clues?

Thanks a lot!

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago +2
    Hi, If you meant to use it to play discs, then the answer is no, the RPI has no video inputs and so it cannot connect to the blu ray player video outputs. Some internal connections will be standards based…
  • COMPACT
    COMPACT over 10 years ago +1
    Of course you can and even retain its original functionality. A simple idea you can use is have the GPIO to control the buttons of or as an IR Feed to the Blu-Ray player. You can use a video multiplexer…
Parents
  • shabaz
    0 shabaz over 10 years ago

    Hi,

    If you meant to use it to play discs, then the answer is no, the RPI has no video inputs and so it cannot connect to the blu ray player video outputs.

    Some internal connections will be standards based signals, but those that the RPI does not interface to, or cannot use for any benefit.

     

    If you meant to just power the tray (i.e. only a mechanical motion) then that is possible - the tray is controlled by a motor.

    I don't know what kind of motor is powering the tray (and pretty sure Sony won't tell you either) so some examination and experimentation

    will be needed, general instructions for controlling a motor are here (PDF).

    If you want to explore further then you may want to check out these electronics book recommendations that explain how to control many things with

    circuitry and micro-controllers.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    Thanks for the quick response and the links!

     

    I was hoping to use it to play discs with some kind of adapter or converter, such as the ones used in external drives. Say, converting SATA zu USB...

    That's probably kind of optimistic, but maybe it's possible image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    Thanks for the quick response and the links!

     

    I was hoping to use it to play discs with some kind of adapter or converter, such as the ones used in external drives. Say, converting SATA zu USB...

    That's probably kind of optimistic, but maybe it's possible image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 10 years ago in reply to e14 Contributor

    No problem, I hope it helps!

    No chance to do this conversion I'm afraid. There is no SATA interface (or any other PC compatible data interface) inside a Blu-Ray video player.

    They make them with integrated circuits designed for one task (video playing). The manufacturers won't waste silicon (hence money) implementing SATA in this case.