Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How could I install a new 12 volt backlight?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 51 replies
  • Answers 5 answers
  • Subscribers 343 subscribers
  • Views 10092 views
  • Users 0 members are here
  • monitor
  • power
  • backlighting
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How could I install a new 12 volt backlight?

bwarren97
bwarren97 over 10 years ago

I have a 1080p monitor that I really really liked, until its backlight started being a butthead. So, I decided to take out the old backlight, and stick in an aftermarket one. I thought it would be nice and simple, until I realized that the LED driver ran on 12 volts and there was no 12 volt output anywhere on the monitor (the original LED was driven by 80 volts).
I have confirmed that the backlight works by jump-wiring it to a PC power supply, but I need a somewhat space-saving method of driving it within the monitor case using its own power supply so that it turns on and off with the monitor. I would like to just solder a 12 volt regulator directly onto the 80 volt output, but I don't know if there is a small chip capable of providing sufficient power or stepping down that much voltage. Any ideas?

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 10 years ago in reply to bwarren97 +2 suggested
    An optocoupler (as you discovered when you seardhed it) provides isolation between sides (LED) and the other (Transistor/Tirac/SCR). They come in various forms and some are much more sensitive than others…
  • shabaz
    shabaz over 10 years ago +1
    You can apply ohm's law and the power equation and see immediately you have a very high amount of power to dissipate as cmay77 mentions - heatsinks and fan time basically. So, theoretically possible with…
  • shabaz
    shabaz over 10 years ago in reply to bwarren97 +1
    By connecting to a 80V supply, even if your backlight draws just 0.3A (4W), your heatsink will need to dissipate more than 20W - that's a huge heatsink. Furthermore, the supply you measured is probably…
Parents
  • shabaz
    0 shabaz over 10 years ago

    You can apply ohm's law and the power equation and see immediately you have a very high amount of power to dissipate as cmay77 mentions - heatsinks and fan time basically. So, theoretically possible with a linear voltage regulator, but realistically the answer is no.

    There are DC-DC converters available to do the conversion with less heat, but expect to pay around $60 for any semi-decent one - don't expect a cheap ebay one to work here, the 80V is a constraint. So basically half the cost of a new monitor - and it still may not give great results, since your monitor probably needs serious levels of calibration in your OS, due to the change in LEDs. It may not even work - I've no idea how much power the previous LEDs were consuming and that is what the 80V supply is probably designed for.


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 10 years ago

    You can apply ohm's law and the power equation and see immediately you have a very high amount of power to dissipate as cmay77 mentions - heatsinks and fan time basically. So, theoretically possible with a linear voltage regulator, but realistically the answer is no.

    There are DC-DC converters available to do the conversion with less heat, but expect to pay around $60 for any semi-decent one - don't expect a cheap ebay one to work here, the 80V is a constraint. So basically half the cost of a new monitor - and it still may not give great results, since your monitor probably needs serious levels of calibration in your OS, due to the change in LEDs. It may not even work - I've no idea how much power the previous LEDs were consuming and that is what the 80V supply is probably designed for.


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Problemchild
    0 Problemchild over 10 years ago in reply to shabaz

    Indeed if he had a 48-60 V LED chain rather than a 80V one he could of used one of the HV cheapo regulators at £2 or less  all of a sudden the 80 V reduces the choices somewhat  image !