Anyone got a link to a TENMA 72-264572-2645 Power Supply Review
A User's Guide would be very appreciated too.
Thanks.
Be sure to click 'more' and select 'suggest as answer'!
If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!
Anyone got a link to a TENMA 72-264572-2645 Power Supply Review
A User's Guide would be very appreciated too.
Thanks.
I've just got a Tenma 72-255072-2550
Is it any good ?
MK
G'day MK
It seems to do what it's meant to. The constant current mode is a bit of an oddball in my eyes.
Constant Current mode works when the current limit is reached.
It's great for testing LEDs.
Just dial up the wind down the current output to zero and wind up the voltage to match the LED's forward voltage.
Connect the LED, enable the PS output and wind up the current knob to the current desired.
This model is a programmable model and is controllable via a PC with special software.
It was a Connect Special.
I'd really like one of those new fangled Keithley Multimeters (with giant buffer) to check its output stability over time!
Manufacturer: KEITHLEY
With the dropping Ozzie Peso I'll have to win the lottery to get one.
VC
Do you need special software to drive the Tenma or can you use general purpose programming languages.
One issue I think you have with the Tenma is that it doesn't specify if it can cope in battery charging type applications where the output may be connected to a voltage source.
You could try it (with a suitable current limiting resistor
).
I have a DMM7510DMM7510 currently using it to make noise measurements on the analogue front end for CO2 sensors I'd swap the huge buffer for faster data transfer via Ethernet then the computer's disk is the buffer
The fast (1Ms/s) data acquisition is the good bit (but it's not 71/2 digits at that speed !!)
MK
Do you need special software to drive the Tenma or can you use general purpose programming languages.
One issue I think you have with the Tenma is that it doesn't specify if it can cope in battery charging type applications where the output may be connected to a voltage source.
You could try it (with a suitable current limiting resistor
).
I have a DMM7510DMM7510 currently using it to make noise measurements on the analogue front end for CO2 sensors I'd swap the huge buffer for faster data transfer via Ethernet then the computer's disk is the buffer
The fast (1Ms/s) data acquisition is the good bit (but it's not 71/2 digits at that speed !!)
MK