Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum mic29502wt
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 21 replies
  • Answers 3 answers
  • Subscribers 321 subscribers
  • Views 3273 views
  • Users 0 members are here
  • help
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

mic29502wt

skal
skal over 10 years ago

Hi

 

i don't really know much about this device ,but i would like to use it in a regulated vacuum tube filament supply  , output voltage should be able to move from min voltage to about 10vdc ,6.3v @ 3A max load.

 

I have played with the lm317 and the 5A version  to that device and i could never get them to regulated properly and  they very easy to damage , 

 

My luck with SS parts , are a joke maybe it is ,the lack of knowledge in this area , which is stopping me from understanding how these reg work and @ £ 7 a pop i need to be pretty sure

about what resistors and capacitors are needed for the project before i  buy  a single Ldo

 

cheers

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago in reply to skal +1
    So you're paralleling up valve filaments.. I'm guessing the adjustable nature is so that it is possible to control the precise current through the filament? If so then an adjustable supply is not much…
Parents
  • shabaz
    0 shabaz over 10 years ago

    Hi Denis,

     

    3A is very high, this would be > 18W at 6.3V (P=Voltage x Current). The reason this becomes important is that

    regulators dissipate power as heat in order to perform their function.

    So if (say) your source was a 12V supply and you're regulating to 6.3V with a load taking 3A, then the power dissipated

    as heat by the regulator is approx (12-6.3)*3 = approx 18W again, i.e. the little regulator needs to dissipate 18W which needs

    a very large heatsink (without that, it will heat up rapidly and then possibly get damaged. This is regardless of if it is rated for 5A, it will need an external heatsink to achieve that.

    You didn't mention if you have a heatsink, or the input voltage, but these are the areas to focus on if they are getting damaged.

    The 317 is a very common part, there will be circuit diagrams to show how to add a variable resistor.

    The Micrel part has a similar method, where you can replace one of the resistors with a variable one, and the output voltage will be based on the formula you found. But 3A is approaching the limit for what is practical with a linear supply (which is what the LM317 and the Micrel part are) due to heatsink size eventually becoming impractical as you go beyond a few amps (depends on your input voltage as mentioned)

    and then other (more complex) circuit topologies are preferred.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • skal
    0 skal over 10 years ago in reply to shabaz

    This is pre design

     

     

    so if you included a pre resistor to drop the voltage at input of the reg to abut 7.3vdc, would that help with the dissipation of the  reg?

     

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to skal

    The resistor will also generate heat too...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • skal
    0 skal over 10 years ago in reply to clem57

    yes, but the reg would only be dropping 1vdc , and that would help with dissipation ? or iam i missing something

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to skal

    Does that mean the input VDC is 8.3? You can take the above assumption shabaz

    explanation of 12 VDC and replace with yours to see what wattage needs to dissipate. Lower the better.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • skal
    0 skal over 10 years ago in reply to clem57

    Yes,  input VDC is 8.3 (8.3-6.3)*3A = approx. 6W  ,  will this regulate  don't know my self ,and a heat sink help with dissipation?

     

    how do would 1 determine the size of the heat sink for this reg

     

    cheers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to skal

    Hi Dennis,

     

    The same power equation is used if you have a resistor, in other words the problem just moves to the resistor and then that will need heatsinking.

    The calculated 6W will need a heatsink too.

    Will you vary the input when you need 10V for the filament supply? If your input supply is adjustable, you don't need to use 8.3V as the input.

    You should set it just slightly higher than the dropout voltage. For the Micrel part, the datasheet says 600mV (0.6V) so if you set your input to just a bit higher then

    you'll dissipate less energy as heat. So if you have your input at 7.3V then you've halved it to 3W, which can be easily handled by bolting it to the chassis.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 10 years ago in reply to skal

    Hi Dennis,

     

    The same power equation is used if you have a resistor, in other words the problem just moves to the resistor and then that will need heatsinking.

    The calculated 6W will need a heatsink too.

    Will you vary the input when you need 10V for the filament supply? If your input supply is adjustable, you don't need to use 8.3V as the input.

    You should set it just slightly higher than the dropout voltage. For the Micrel part, the datasheet says 600mV (0.6V) so if you set your input to just a bit higher then

    you'll dissipate less energy as heat. So if you have your input at 7.3V then you've halved it to 3W, which can be easily handled by bolting it to the chassis.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data