Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum mic29502wt
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 21 replies
  • Answers 3 answers
  • Subscribers 340 subscribers
  • Views 3737 views
  • Users 0 members are here
  • help
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

mic29502wt

skal
skal over 10 years ago

Hi

 

i don't really know much about this device ,but i would like to use it in a regulated vacuum tube filament supply  , output voltage should be able to move from min voltage to about 10vdc ,6.3v @ 3A max load.

 

I have played with the lm317 and the 5A version  to that device and i could never get them to regulated properly and  they very easy to damage , 

 

My luck with SS parts , are a joke maybe it is ,the lack of knowledge in this area , which is stopping me from understanding how these reg work and @ £ 7 a pop i need to be pretty sure

about what resistors and capacitors are needed for the project before i  buy  a single Ldo

 

cheers

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago in reply to skal +1
    So you're paralleling up valve filaments.. I'm guessing the adjustable nature is so that it is possible to control the precise current through the filament? If so then an adjustable supply is not much…
Parents
  • jc2048
    0 jc2048 over 10 years ago

    If you are managing to blow up LM137s you need to be very cautious before using the MIC29502 If it were me I'd try and understand why the LM317s were dying before doing anything else(Are you sure you are killing them They have an internal temperature monitor and will shut down and refuse to operate if they get too hot Most LM317s are rated at 1.5A for normal use the current limit will be higher than that but you don't know exactly where it will cut in and you don't want to be operating close under it

     

    Given how cheap the LM317s are compared to the MIC29502 couldn't you use a pair of them with each one running 4 filaments(4 x 300mA 1.2A[For the cost of the MIC29502 you could give each filament its own LM317

     

    If you do want to try a MIC29502, here's how it would look

     

    image

     

    The calculation of the resistors works differently to the LM317. The LM317 is a floating regulator and its control loop compares the voltage between the ADJ pin and the output pin with the internal reference to control the pass element (the internal transistor that adjusts the current to the output). The MIC29502 is ground referenced and is comparing the voltage at the ADJ pin relative to GND with the reference voltage.

     

    Here's how I got the values on the drawing.

     

    I started with the potentiometer. They come in far fewer different values than fixed resistors, typically in a 1,2,5 sequence. You wanted an adjustment range of about 1.5V. A 200 ohm pot seemed like a good start. With 1.5V across it, that would mean a current of 1.5/200 = 7.5mA (the current flows from the output down through R1, VR1, and R2 to ground) which is reasonable. The regulator tries to hold the ADJ pin at 1.24V, so resistor R2 would be 1.24V/7.5mA = 165 ohms. Here we have a choice - 150 and 180 are standard values - and I chose 180 ohms; that compromises your adjustment range a little but I reckoned it would still be acceptable (you can rework the values if it's not). Now the current isn't 7.5mA any longer, instead the regulator will maintain a current of 1.24V / 180ohms = 6.88mA which I'll use for the rest of the calculations. We have two of the values, we just need a value for R1. Let's say we have the pot at the halfway point.  The resistance will be 100 ohms. We want that to correspond to 6.3V. The total resistance (R1+VR1+R2) is 6.3V / 6.88mA = 916 ohms. So, R1 = 916 - (180 + 100) = 636 ohms. Nearest value is 620.

     

    With the pot set to zero, the output voltage will be 5.5V.

     

    With the pot set to 200ohms, the output will be 6.88V.

     

    If you want to check that I've got it right, take the output voltages above and the R2 value and plug them into the formula on the datasheet and see what value it comes up with for R1 in each case. If it matches R1 + VR1 then we're there.

     

    One additional thing to note is that the part has a minimum current of 10mA and the current I've chosen is less than that. It won't matter once you get your filaments connected, but if you want to test it first before you connect them put a small load on the output (1K will do) otherwise it may not regulate properly. Alternatively you could scale all the resistor values so that the current through the chain is more than the 10mA.

     

    Couple of other observations

     

    1/ don't forget the diode drops in the bridge when calculating the transformer voltage you'll need (2 x 0.9V = 1.8V at 3A)

     

    2/ the ripple on 20000uF at 50Hz is about 1.5V at 3A and 1.2V at 2.4A

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • skal
    0 skal over 10 years ago in reply to jc2048

    Thank you ,this is what i needed the method of working out the values, i can go away now and plugin some values to see what i get..

     

    cheers

     

    Den

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • skal
    0 skal over 10 years ago in reply to jc2048

    Thank you ,this is what i needed the method of working out the values, i can go away now and plugin some values to see what i get..

     

    cheers

     

    Den

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • skal
    0 skal over 10 years ago in reply to skal

    i was also looking at these diodes for the rectification stage (SB540-E3/54 - VISHAY - Rectifier Diode, Single, 40 V, 5 A, DO-201AD, 2, 480 mV | Farnell element14  ), should the job, times 4 and 3 times 27000uf two filtering the ac ripple  and one after the reg. (http://uk.farnell.com/multicomp/mchpr16v279m30x31/cap-alu-elec-27000uf-16v-snap/dp/1903174 )

     

    do think these should do the job.

     

    Den

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to skal

    You might do better using a ready built bridge rectifier rather than 4 diodes - I like this style because they are easy to heat sink and attach thick wires - this was the cheapest I found quickly at Farnell  CM1508 - MULTICOMP - Bridge Rectifier Diode, Single, 800 V, 15 A, 1.2 V, 4 | Farnell element14 if you want you can get a pcb mounting part even more cheaply. In fact they are so cheap you can easily afford to over specify on current and voltage which will make you design more robust.

    There is no point in putting a huge capacitor after the regulator - the values in the data sheet will be sufficient - and it cautions you against using  a very low ESR part so don't stick a big ceramic in ! 47uF should be OK. The output impedance of the regulator will be of the order of 0.01ohms up to a few hundred Hz (check the graphs on the data sheet) so putting  big cap there won't help. (At 100Hz you need 159,000 uF to get down to 0.01R !!).

    The type of capacitors you've chosen should be OK (did you mean them to be pcb mounted ?).

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • skal
    0 skal over 10 years ago in reply to michaelkellett

    yes i need pcb mounted capacitor , do i need a bleeder resistors for the capacitors,and   also is there any need for a 0.1uf film in the input and out of the reg , i have used them before with the lm317reg.

     

    cheers

     

    Den

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to skal

    The data sheet says you only need small caps near the regulator if you have long leads but putting some 0805 surface mount footprints on the board won't hurt - you don't need to fit them unless they are needed. Ceramic caps are much better than film for this and surface mount much better than ones with wires. Choose parts with X7R or X5R dielectric and generous over voltage rating, especially on the input side. Farnell 2320827 at about £0.04 each look good.

    Bleeder resistors are only needed if it matters that the caps hold charge for a long time after power off. With 54000uF you'll be down to about 10% of the operating voltage after about 11 seconds with a 100R resistor. At 9V across the resistor when the power is on you'll be dissipating 0.81 W so use  a 3W resistor so it doesn't get too hot - but don't bother unless you really need it. (if the load is always connected the voltage across the caps will drop much faster.)

     

    MK