Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum mic29502wt
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 21 replies
  • Answers 3 answers
  • Subscribers 340 subscribers
  • Views 3732 views
  • Users 0 members are here
  • help
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

mic29502wt

skal
skal over 10 years ago

Hi

 

i don't really know much about this device ,but i would like to use it in a regulated vacuum tube filament supply  , output voltage should be able to move from min voltage to about 10vdc ,6.3v @ 3A max load.

 

I have played with the lm317 and the 5A version  to that device and i could never get them to regulated properly and  they very easy to damage , 

 

My luck with SS parts , are a joke maybe it is ,the lack of knowledge in this area , which is stopping me from understanding how these reg work and @ £ 7 a pop i need to be pretty sure

about what resistors and capacitors are needed for the project before i  buy  a single Ldo

 

cheers

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago in reply to skal +1
    So you're paralleling up valve filaments.. I'm guessing the adjustable nature is so that it is possible to control the precise current through the filament? If so then an adjustable supply is not much…
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to skal

    The data sheet says you only need small caps near the regulator if you have long leads but putting some 0805 surface mount footprints on the board won't hurt - you don't need to fit them unless they are needed. Ceramic caps are much better than film for this and surface mount much better than ones with wires. Choose parts with X7R or X5R dielectric and generous over voltage rating, especially on the input side. Farnell 2320827 at about £0.04 each look good.

    Bleeder resistors are only needed if it matters that the caps hold charge for a long time after power off. With 54000uF you'll be down to about 10% of the operating voltage after about 11 seconds with a 100R resistor. At 9V across the resistor when the power is on you'll be dissipating 0.81 W so use  a 3W resistor so it doesn't get too hot - but don't bother unless you really need it. (if the load is always connected the voltage across the caps will drop much faster.)

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<