Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How to run HDMI and Official Raspberry Pi Display (DSI) simultaneously?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 25 replies
  • Answers 6 answers
  • Subscribers 344 subscribers
  • Views 15714 views
  • Users 0 members are here
  • dual head
  • dsi
  • hdmi
  • frame_buffer
  • raspberry pi
  • rpi
  • official display
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How to run HDMI and Official Raspberry Pi Display (DSI) simultaneously?

e14 Contributor
e14 Contributor over 10 years ago

Hallo  to all RPi lovers,

I've been trying for a while to clone the video from Official Raspberry Pi Display (connects through DSI) to the HDMI display. Both work fine when alone but not together.

I am pretty much sure, that it is possible from hardware side, as the omxplayer can play video, on HDMI display, while DSI Display is on and functioning.

Looking deeper in the problem I am able to state following:

1. Raspberry Pi doesn't create a framebuffer for second device, there is only /dev/fb0, no matter how many monitors are plugged

2. As the consequence of first, fbcp and other tools, that can play with framebuffer around, won't work.

3. As far as I understood the module bcm2708_fb is in charge of HDMI framebuffer however here is the lsmod:

Module             Size  Used by
cfg80211         419759  0
rfkill            16659  2 cfg80211
bcm2835_gpiomem    3023  0
evdev             10226  6
joydev             9047  0
snd_bcm2835       19739  3
snd_pcm           74833  1 snd_bcm2835
r8712u           167991  0
snd_timer         18164  1 snd_pcm
snd               52116  9 snd_bcm2835,snd_timer,snd_pcm
uio_pdrv_genirq    2966  0
rpi_ft5406         2826  0
uio                8228  1 uio_pdrv_genirq
rpi_backlight      1988  0
i2c_dev            6040  0
fuse              81721  3
ipv6             341380  30

 

and modprobe  bcm2708_fb gives in dmsg following error:

 

[ 3597.206111] bcm2708_fb soc:fb: Unknown ioctl 0x40187a22

[ 3721.217242] bcm2708_fb soc:fb: Unknown ioctl 0x40187a22

[ 3757.719256] bcm2708_fb soc:fb: Unknown ioctl 0x40187a22

[ 3881.152850] bcm2708_fb soc:fb: Unknown ioctl 0x40187a22

Just to imagine here is a part of config that defines the device:

 

Section "Device"

        Identifier      "Allwinner A10/A13 FBDEV"

        Driver          "fbturbo"

        Option          "fbdev" "/dev/fb0"

 

        Option          "SwapbuffersWait" "true"

EndSection

 

But Xorg configuration is the least of the Problem.

 

Would be happy to get any advices or questions and thanking for them in advance.

 

 

PS. To use built-in RCA, GPIO-VGA adapter, USB external graphic cards is not an option. Aim is stable and clear - to clone HDMI and DSI

The Device is Raspberry Pi 2, (Jessy and Wheezy)

 

PPS. Is there is the way to input code here as code with no highlighting?

  • Sign in to reply
  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 9 years ago in reply to shabaz +2
    Hi Shabaz! You put more light on this interesting problem. The dual HDMI-VGA remain, in my opinion a good idea for a lot of applications. What I know instead - but it is interesting your citation (from…
  • shabaz
    shabaz over 10 years ago +1 suggested
    I'm pretty sure that would require GPU firmware effort, see here for some discussion not entirely unrelated: https://www.raspberrypi.org/forums/viewtopic.php?f=63&t=120541 The discussion there is concerned…
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to shabaz +1 suggested
    Shabaz are you sure that it is not possible changing the X11 Linux settings? I think - not yet tried - that the HDMI screen can be saw as a second display... If possible it will be great, don't you think…
Parents
  • geeviz
    0 geeviz over 6 years ago

    i am struggling more the less with the same problem with two monitor setup which won't work yet... for the pi 3 with and 7 inch usb touch displaylink and normal standard hdmi (my hdmi keeps blank screen with the underscore left above in corner.. )

    i cannot get them to work simultaneously..

     

    Section "Device"

    Identifier "DisplayLinkDevice"

    driver "fbdev"

    Option "fbdev" "/dev/fb1"

    Option "ShadowFB" "off"

    EndSection

     

     

    Section "Monitor"

    Identifier "monitor"

    Option "DPMS"

    EndSection

     

     

    Section "Screen"

    Identifier "screen"

    Device "DisplayLinkDevice"

    Monitor "monitor"

    EndSection

     

     

    Section "ServerLayout"

    Identifier "default"

    Screen 0 "screen" 0 0

    screen 1 "bigscreen" RightOf "screen"

    InputDevice "touchscreen" "CorePointer"

    Option "BlankTime" "0"

    Option "StandbyTime" "0"

    Option "SuspendTime" "0"

    Option "OffTime" "0"

    EndSection

     

     

    Section "InputDevice"

    Identifier "touchscreen"

    Driver "evdev"

    Option "Device" "/dev/input/by-id/usb-e2i_Technology__Inc._USB_Touchpanel"

    Option "DeviceName" "touchscreen"

    Option "ReportingMode" "Raw"

    Option "SendCoreEvents" "On"

    Option "Calibrate" "1"

    Option "MinX" "1754"

    Option "MaxX" "64067"

    Option "MinY" "62314"

    Option "MaxY" "1240"

    Option "SwapAxes" "1"

    Option "TransformationMatrix" "1 0 0 0 -1 1 0 0 1"

    EndSection

     

     

    Section "InputClass"

    Identifier "calibration"

    MatchProduct "e2i Technology, Inc. USB Touchpanel"

    Option "Calibration" "1754 64067 62314 1240"

    Option "SwapAxes" "1"

    Option "InvertY" "true"

    Option "TransformationMatrix" "1 0 0 0 -1 1 0 0 1"

    EndSection

     

     

    Section "Device"

    Identifier "default"

    driver "Modesetting"

    Option "kmsdev" "/dev/dri/card0"

    EndSection

     

     

    Section "Monitor"

    Identifier "default"

    EndSection

     

     

    Section "Screen"

    Identifier "bigscreen"

    device "default"

    monitor "default"

    EndSection

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • geeviz
    0 geeviz over 6 years ago

    i am struggling more the less with the same problem with two monitor setup which won't work yet... for the pi 3 with and 7 inch usb touch displaylink and normal standard hdmi (my hdmi keeps blank screen with the underscore left above in corner.. )

    i cannot get them to work simultaneously..

     

    Section "Device"

    Identifier "DisplayLinkDevice"

    driver "fbdev"

    Option "fbdev" "/dev/fb1"

    Option "ShadowFB" "off"

    EndSection

     

     

    Section "Monitor"

    Identifier "monitor"

    Option "DPMS"

    EndSection

     

     

    Section "Screen"

    Identifier "screen"

    Device "DisplayLinkDevice"

    Monitor "monitor"

    EndSection

     

     

    Section "ServerLayout"

    Identifier "default"

    Screen 0 "screen" 0 0

    screen 1 "bigscreen" RightOf "screen"

    InputDevice "touchscreen" "CorePointer"

    Option "BlankTime" "0"

    Option "StandbyTime" "0"

    Option "SuspendTime" "0"

    Option "OffTime" "0"

    EndSection

     

     

    Section "InputDevice"

    Identifier "touchscreen"

    Driver "evdev"

    Option "Device" "/dev/input/by-id/usb-e2i_Technology__Inc._USB_Touchpanel"

    Option "DeviceName" "touchscreen"

    Option "ReportingMode" "Raw"

    Option "SendCoreEvents" "On"

    Option "Calibrate" "1"

    Option "MinX" "1754"

    Option "MaxX" "64067"

    Option "MinY" "62314"

    Option "MaxY" "1240"

    Option "SwapAxes" "1"

    Option "TransformationMatrix" "1 0 0 0 -1 1 0 0 1"

    EndSection

     

     

    Section "InputClass"

    Identifier "calibration"

    MatchProduct "e2i Technology, Inc. USB Touchpanel"

    Option "Calibration" "1754 64067 62314 1240"

    Option "SwapAxes" "1"

    Option "InvertY" "true"

    Option "TransformationMatrix" "1 0 0 0 -1 1 0 0 1"

    EndSection

     

     

    Section "Device"

    Identifier "default"

    driver "Modesetting"

    Option "kmsdev" "/dev/dri/card0"

    EndSection

     

     

    Section "Monitor"

    Identifier "default"

    EndSection

     

     

    Section "Screen"

    Identifier "bigscreen"

    device "default"

    monitor "default"

    EndSection